Is it mandatory to send calibration command (SCAL) on power up? or it's better to put the C22500 in sleep mode after power up?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it mandatory to send calibration command (SCAL) on power up? or it's better to put the C22500 in sleep mode after power up?
The SCAL command can be sent at any time when the radio is not in low power mode. You can put the radio to sleep immediately after power up if you like. I would suggest doing as much configuration as possible initially first then putting it to sleep. No real requirement to do this just personal preference as part of an initialization procedure.
Jim Noxon