Other Parts Discussed in Thread: OMAP-L138, DA8XX
Hello
I modifed ramdisk by reference to below link:
http://processors.wiki.ti.com/index.php/Creating_a_RAMDISK
Thogh I could size up my ramdisk.gz from 4M to 5M.
when over 5M, booting is failed.
Is this concerned in DRAM size for operating
and not to recommend over 4M ramdisk?
|
OMAP-L138 initialization passed!
I2C: ready Hit any key to stop autoboot: 0 Environment size: 441/131068 bytes NAND read: device 0 offset 0x400000, size 0x600000 Loading from NAND 512MiB 3,3V 8-bit, offset 0x200000 Starting kernel ... Uncompressing Linux... done, booting the kernel. Backtrace: |
Thank you for reading.