Part Number: DRA829V
Hello,
Can we use FT2232HQ for multiplexing both MAIN and MCU UART.
1. Will this impacts the binary loading ?
2. We are planning to use single usb port with FT2232 device multiplexing MAIN and MCU UART.
BR,
Arun M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRA829V
Hello,
Can we use FT2232HQ for multiplexing both MAIN and MCU UART.
1. Will this impacts the binary loading ?
2. We are planning to use single usb port with FT2232 device multiplexing MAIN and MCU UART.
BR,
Arun M
Arun,
Yes you can use FT2232H to multiplex between different UART ports. This is currently done on the EVM. For more information and design recommendation, please reference the EVM schematic and user guide here:
https://www.ti.com/tool/J721EXSOMXEVM
https://www.ti.com/lit/ug/spruis4b/spruis4b.pdf
Best Regards,
Shiou Mei
Hi Shiou,
Thanks. I understood that in EVM it is multiplexed, but we are planning to multiplex both MCU_UART0 And MAIN_UART0 which is not done in the EVM. Could you please confirm this
Arun
A single FT2232H can be used to support MCU_UART0 and MAIN_UART0. Depending on how the VDDSHV IO rails are powered, you may need to add buffer/isolation between Processor/FT2232H (especially if supporting MCU-only or similar modes). Not clear on question regarding binary impact. The EVM support UARTs for both MCU_UART0 and MAIN_UART0. It sounds like this design will be same - so no impact.
Hi Robert,
Binary impact i asked is loading the images
1. tiboot.bin - MCU UART0
2. sysfw.itb - MCU UART0
3. tispl.bin - MAIN UART0
4.uboot.img - MAIN UART0
Will there be impact if MAIN UART0 and MCU UART0 is multiplexed !!
We are not using MCU only mode. We are utilizing both the domains
-Arun
I'm not clear on meaning of MAIN UART0 and MCU UART0 being multiplexed - can you explain? The FT2232H supports dual UARTs, so is the plan to support these two UARTs on the FT2232H - or do these UARTs share a single port on the FT2232H?
Hello Robert,
In the EVM, MCU_UART0 and WKUP_UART0 are multiplexed through FT2232 and is connected to J43(MCU Domain UART) and similarly another quad device is used to multiplex UART0(Main domain) and is connected to J44 (Main UART).
We are planning to use a dual port FT2232 and implement MCU_UART0 and UART0 (main domain) in that single chip and connect to a single USB port.
I would like to know whether this is possible as i see for quad and dual device, the power domains are different.
In another sense, It will be similar as Dual port FTDI, but Instead of WKUP_UART0 we will use UART0.
Thanks,
Arun M