This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vpss.ko modprobe hangs

Guru 10685 points


I've built syslink including the kernel module, then built my kernel and its modules against syslink. I boot up my board and manually run the steps of the TI init script "S50load-firmware.sh". This is what happens:

# PATH=$PATH:/usr/share/ti/ti-hdvpss-display-utils
# modprobe syslink
SysLink module created on Date:Mar 29 2011 Time:14:15:57
Entered KnlUtilsDrv_initializeModule
traceMask value: 0x0
Leaving KnlUtilsDrv_initializeModule 0x0
# procmgrapp.exe 2 /usr/share/ti/ti-hdvpss-display-utils/ti816x_hdvpss.xem3 &
# ProcMgrApp sample application
Entered ProcMgrApp_startup
ProcMgr_attach status: [0x0]
After attach: ProcMgr_getState
    state [0x1]
ProcMgr_load status: [0x3046000]
After load: ProcMgr_getState
    state [0x3]
ProcMgr_start passed [0x6a85000]

# modprobe vpss mode=hdmi:1080p-60,dvo2:1080p-60 debug=1

and then it hangs. I can't use Ctrl-C or anything else. The same happens without the debug argument and also with just "modprobe vpss". 

I don't know if it's relevant or not but occasionally ProcMgrApp fails with this:

ProcMgrApp sample application
Entered ProcMgrApp_startup
ProcMgr_attach status: [0x0]
After attach: ProcMgr_getState
    state [0x1]
Error in ProcMgr_load [0x83046005]
Leaving ProcMgrApp_startup
Press enter to continue and perform shutdown ...

Assertion at Line no: 127 in /home/user/ezsdk/ti-ezsdk_c6a816x-evm_5_00_00_56/s
yslink_02_00_00_56/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/
utils/hlos/Memory.c: (size > 0) : failed
Entered ProcMgrApp_shutdown
Assertion at Line no: 261 in /home/
user/ezsdk/ti-ezsdk_c6a816x-evm_5_00_00_56/s
yslink_02_00_00_56/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/
utils/hlos/knl/osal/Linux/MemoryOS.c: (size > 0) : failed
Assertion at Line no: 304 in /home/
user/ezsdk/ti-ezsdk_c6a816x-evm_5_00_00_56/s
yslink_02_00_00_56/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/
ipc/hlos/knl/Linux/IpcDrv.c: (status >= 0) : failed
Ipc_control Ipc_CONTROLCMD_STOPCALLBACK status: [0xffffffff]
ProcMgr_stop status: [0x6a85000]
After stop: ProcMgr_getState
    state [0x2]
ProcMgr_unload status: [0x8485f003]
After unload: ProcMgr_getState
    state [0x2]
ProcMgr_detach status: [0x0]
After detach: ProcMgr_getState
    state [0x0]
ProcMgr_close status: [0x0]
Leaving ProcMgrApp_shutdown

If I just load VPSS without loading syslink and running ProcMgrApp first it seems to load the module but with this error message:

# modprobe vpss mode=hdmi:1080p-60,dvo2:1080p-60 debug=1
SysLink module created on Date:Mar 29 2011 Time:14:15:57
Entered KnlUtilsDrv_initializeModule
traceMask value: 0x0
Leaving KnlUtilsDrv_initializeModule 0x0
VPSS_FVID2: Failed to send version command to M3 0xfffffff9.
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22

So, does anyone know why my VPSS module is failing to load?

Thanks,
Ralph