This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

evm5515 - cc3.3 dsp/bios 5 - GPIO and HWI interrupts

 folks,

I need to declere my gpio as an input interrupt and I'm not sure if by using the configuration tool of the BIOS I'm defining everything I need.

should I use the CSL  first in order to define the GPIO as input interrupt (raising or falling) and then use the BIOS in order to declered the ISR routine ? or I can define everything with the BIOS?

BR

Talmor