This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM64X: Using SD card to boot

Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: AM6442

Hi,

I'm trying to use the SD booting on the AM6442 with the boot image included in the MCU-PLUS-SDK-AM64X_08.00.00.21.
I followed the manual and the SOC Initialization Using SD BOOT procedure to create an SD card.
After boot, the watchdog is still active and the TISCI communiaction seems to not work.

I tried booting using the OSPI boot which works fine, but I need to program larger parts of OSPI flash so SD boot is needed.


I've read that the SD booting was not supported from the beginning, is it still not supported or is this a different issue?

Best regards,

Robert