Part Number: PROCESSOR-SDK-AM57X
Other Parts Discussed in Thread: AM5718, AM5728, DRA722, TPD12S015
Hi all,
I am using
Board Name : AM5718 IDK
Processor SDK version :ti-processor-sdk-linux-am57xx-evm-06.03.00.106
Linux version : linux-4.19.94+gitAUTOINC+be5389fd85-gbe5389fd85
U-boot Version : u-boot-2019.01+gitAUTOINC+333c3e72d3-g333c3e72d3
i am working on Bringing up a custom board using SD card .
i tried in IDK board it worked.
for custom board i changed code eeprom read data in ti/sdk/board-support/u-boot-2019.01+gitAUTOINC+333c3e72d3-g333c3e72d3/board/ti/common/board_detect.c after this u-boot is booted but kernel code is hanged
could you please help me to fix this issue
boot -log
U-Boot 2019.01-g323d51410c-dirty (Jul 23 2021 - 14:47:34 +0530)
CPU : DRA722-GP ES2.0
Model: TI AM5728 IDK
Board: AM571x IDK REV 14
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... OK
unable to get I2C bus. ret 1
unable to get I2C bus. ret 1
unable to get I2C bus. ret 1
i2c_write: error waiting for data ACK (status=0x116)
cdce9xx_reg_write: failed for addr:5, ret:-121
Net: eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
1529 bytes read in 2 ms (746.1 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
Running uenvcmd ...
1 bytes read in 3 ms (0 Bytes/s)
Already setup.
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4506112 bytes read in 201 ms (21.4 MiB/s)
128480 bytes read in 8 ms (15.3 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffdd000, end 8ffff5df ... OK
## Transferring control to Linux (at address 82000000)...
Starting kernel ...
[ 0.000000] Ritesh Test --> Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.94-gbe5389fd85 (ritesh@ritesh-pc) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #4 SMP PREEMPT Thu Jul 22 16:26:10 IST 2021
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM5718 IDK
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] OF: reserved mem: initialized node ipu2-memory@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] OF: reserved mem: initialized node dsp1-memory@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node ipu1-memory@9d000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to (ptrval) for dram barrier
[ 0.000000] Hit pending asynchronous external abort (FSR=0x00001211) during first unmask, this is most likely caused by a firmware/bootloader bug.
[ 0.000000] On node 0 totalpages: 203776
[ 0.000000] DMA zone: 1728 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 139008 pages, LIFO batch:31
[ 0.000000] HighMem zone: 64768 pages, LIFO batch:15
[ 0.000000] DRA722 ES2.0
[ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x468 with crng_init=0
[ 0.000000] percpu: Embedded 15 pages/cpu s32396 r8192 d20852 u61440
[ 0.000000] pcpu-alloc: s32396 r8192 d20852 u61440 alloc=15*4096
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 202048
[ 0.000000] Kernel command line: console=ttyS2,115200n8 root=PARTUUID=3c5d1d1b-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 643940K/815104K available (8192K kernel code, 335K rwdata, 2804K rodata, 2048K init, 267K bss, 23708K reserved, 147456K cma-reserved, 234496K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (10208 kB)
[ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (2048 kB)
[ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 336 kB)
[ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 268 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000006] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000017] Switching to timer-based delay loop, resolution 162ns
[ 0.000257] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000265] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000699] Console: colour dummy device 80x30
[ 0.000715] Test Print: Consol Init success.........
[ 0.000744] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000762] pid_max: default: 32768 minimum: 301
[ 0.000869] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000882] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001362] CPU: Testing write buffer coherency: ok
[ 0.001395] CPU0: Spectre v2: using ICIALLU workaround
[ 0.001593] /cpus/cpu@0 missing clock-frequency property
[ 0.001605] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.059874] Setting up static identity map for 0x80200000 - 0x80200060
[ 0.079874] rcu: Hierarchical SRCU implementation.
[ 0.100037] EFI services will not be available.
[ 0.119912] smp: Bringing up secondary CPUs ...
[ 0.119922] smp: Brought up 1 node, 1 CPU
[ 0.119931] SMP: Total of 1 processors activated (12.29 BogoMIPS).
[ 0.119938] CPU: All CPU(s) started in HYP mode.
[ 0.119944] CPU: Virtualization extensions available.
[ 0.120312] devtmpfs: initialized
[ 0.140055] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.140295] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.140311] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 0.142962] pinctrl core: initialized pinctrl subsystem
[ 0.143424] DMI not present or invalid.
[ 0.143682] NET: Registered protocol family 16
[ 0.150802] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.151608] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.324015] cpuidle: using governor ladder
[ 0.324044] cpuidle: using governor menu
[ 0.332178] gpio gpiochip0: (gpio-0-31): added GPIO chardev (254:0)
[ 0.332235] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0 (gpio-0-31)
[ 0.332276] OMAP GPIO hardware version 0.1
[ 0.332781] gpio gpiochip1: (gpio-32-63): added GPIO chardev (254:1)
[ 0.332835] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip1 (gpio-32-63)
[ 0.333349] gpio gpiochip2: (gpio-64-95): added GPIO chardev (254:2)
[ 0.333407] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip2 (gpio-64-95)
[ 0.333900] gpio gpiochip3: (gpio-96-127): added GPIO chardev (254:3)
[ 0.333953] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochip3 (gpio-96-127)
[ 0.334445] gpio gpiochip4: (gpio-128-159): added GPIO chardev (254:4)
[ 0.334499] gpiochip_setup_dev: registered GPIOs 128 to 159 on device: gpiochip4 (gpio-128-159)
[ 0.334995] gpio gpiochip5: (gpio-160-191): added GPIO chardev (254:5)
[ 0.335047] gpiochip_setup_dev: registered GPIOs 160 to 191 on device: gpiochip5 (gpio-160-191)
[ 0.335550] gpio gpiochip6: (gpio-192-223): added GPIO chardev (254:6)
[ 0.335608] gpiochip_setup_dev: registered GPIOs 192 to 223 on device: gpiochip6 (gpio-192-223)
[ 0.336103] gpio gpiochip7: (gpio-224-255): added GPIO chardev (254:7)
[ 0.336160] gpiochip_setup_dev: registered GPIOs 224 to 255 on device: gpiochip7 (gpio-224-255)
[ 0.350600] No ATAGs?
[ 0.350640] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.350654] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.351421] OMAP DMA hardware revision 0.0
[ 0.382096] edma 43300000.edma: memcpy is disabled
[ 0.384761] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.390475] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.390951] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-vmain[0]'
[ 0.391167] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-v3_3d[0]'
[ 0.391357] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-vtt[0]'
[ 0.393565] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.393711] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.393904] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.394089] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.394392] iommu: Adding device 58820000.ipu to group 1
[ 0.394458] iommu: Adding device 55020000.ipu to group 2
[ 0.394564] iommu: Adding device 40800000.dsp to group 0
[ 0.395743] SCSI subsystem initialized
[ 0.396717] palmas 0-0058: Irq flag is 0x00000004
[ 0.420384] palmas 0-0058: POLARITY_CTRL update failed: -121
[ 0.420671] palmas: probe of 0-0058 failed with error -121
[ 0.420865] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.421038] media: Linux media interface: v0.10
[ 0.421068] videodev: Linux video capture interface: v2.00
[ 0.421132] pps_core: LinuxPPS API ver. 1 registered
[ 0.421140] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.421157] PTP clock support registered
[ 0.421184] EDAC MC: Ver: 3.0.0
[ 0.430878] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.431020] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.440501] Advanced Linux Sound Architecture Driver Initialized.
[ 0.441186] clocksource: Switched to clocksource arch_sys_counter
[ 0.447435] NET: Registered protocol family 2
[ 0.447936] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
[ 0.447963] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.448023] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.448148] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.448217] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.448248] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.448359] NET: Registered protocol family 1
[ 0.478757] RPC: Registered named UNIX socket transport module.
[ 0.478767] RPC: Registered udp transport module.
[ 0.478775] RPC: Registered tcp transport module.
[ 0.478782] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.478792] PCI: CLS 0 bytes, default 64
[ 0.479790] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.480561] Initialise system trusted keyrings
[ 0.480695] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.484953] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.495390] NFS: Registering the id_resolver key type
[ 0.495412] Key type id_resolver registered
[ 0.495421] Key type id_legacy registered
[ 0.495452] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.497023] Key type asymmetric registered
[ 0.497034] Asymmetric key parser 'x509' registered
[ 0.497082] bounce: pool size: 64 pages
[ 0.497112] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.497121] io scheduler noop registered
[ 0.497129] io scheduler deadline registered
[ 0.497216] io scheduler cfq registered (default)
[ 0.497225] io scheduler mq-deadline registered
[ 0.497233] io scheduler kyber registered
[ 0.502027] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
[ 0.502158] pinctrl-single 4a002e8c.pinmux: please update dts to use #pinctrl-cells = <1>
[ 0.502205] pinctrl-single 4a002e8c.pinmux: initialized with no interrupts
[ 0.502215] pinctrl-single 4a002e8c.pinmux: 1 pins, size 4
[ 0.525519] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.1
[ 0.525640] dra7-pcie 51000000.pcie: GPIO lookup for consumer (null)
[ 0.525650] dra7-pcie 51000000.pcie: using device tree for GPIO lookup
[ 0.525685] of_get_named_gpiod_flags: parsed 'gpios' property of node '/ocp/axi@0/pcie@51000000[0]' - status (0)
[ 0.525720] gpio gpiochip4: Persistence not supported for GPIO 18
[ 0.525875] dra7-pcie 51000000.pcie: host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 0.525910] dra7-pcie 51000000.pcie: IO 0x20003000..0x20012fff -> 0x00000000
[ 0.525932] dra7-pcie 51000000.pcie: MEM 0x20013000..0x2fffffff -> 0x20013000
[ 1.526132] dra7-pcie 51000000.pcie: Phy link never came up
[ 1.526244] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 1.526256] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.526266] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.526275] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 1.526306] pci 0000:00:00.0: [104c:8888] type 01 class 0x060400
[ 1.526337] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff 64bit]
[ 1.526392] pci 0000:00:00.0: supports D1
[ 1.526401] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 1.531821] PCI: bus0: Fast back to back transfers disabled
[ 1.536871] PCI: bus1: Fast back to back transfers enabled
[ 1.536908] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit]
[ 1.536925] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 1.537198] pcieport 0000:00:00.0: Signaling PME with IRQ 167
[ 1.537300] pcieport 0000:00:00.0: AER enabled with IRQ 167
[ 1.574643] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 1.577592] console [ttyS2] disabled
[ 1.577646] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 45, base_baud = 3000000) is a 8250
[ 2.785818] console [ttyS2] enabled
[ 2.791135] omap_rng 48090000.rng: Random Number Generator ver. 20
[ 2.797478] random: fast init done
[ 2.801016] random: crng init done
[ 2.805927] tpd12s015 encoder@0: GPIO lookup for consumer (null)
[ 2.812423] tpd12s015 encoder@0: using device tree for GPIO lookup
[ 2.818639] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/encoder@0[0]'
[ 2.827010] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/encoder@0[0]'
[ 2.835236] tpd12s015 encoder@0: using lookup tables for GPIO lookup
[ 2.841628] tpd12s015 encoder@0: No GPIO consumer (null) found
[ 2.847486] tpd12s015 encoder@0: GPIO lookup for consumer (null)
[ 2.853526] tpd12s015 encoder@0: using device tree for GPIO lookup
[ 2.859737] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/encoder@0[1]'
[ 2.868050] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/encoder@0[1]'
[ 2.876272] tpd12s015 encoder@0: using lookup tables for GPIO lookup
[ 2.882661] tpd12s015 encoder@0: No GPIO consumer (null) found
[ 2.888518] tpd12s015 encoder@0: GPIO lookup for consumer (null)
[ 2.894559] tpd12s015 encoder@0: using device tree for GPIO lookup
[ 2.900781] of_get_named_gpiod_flags: parsed 'gpios' property of node '/encoder@0[2]' - status (0)
[ 2.909817] gpio gpiochip6: Persistence not supported for GPIO 12
[ 2.916628] connector-hdmi connector@0: GPIO lookup for consumer hpd
[ 2.923050] connector-hdmi connector@0: using device tree for GPIO lookup
[ 2.929873] of_get_named_gpiod_flags: can't parse 'hpd-gpios' property of node '/connector@0[0]'
[ 2.938732] of_get_named_gpiod_flags: can't parse 'hpd-gpio' property of node '/connector@0[0]'
[ 2.947506] connector-hdmi connector@0: using lookup tables for GPIO lookup
[ 2.954526] connector-hdmi connector@0: No GPIO consumer hpd found
[ 2.970233] brd: module loaded
[ 2.978835] loop: module loaded
[ 2.986503] m25p80 spi0.0: s25fl256s1 (32768 Kbytes)
[ 2.991618] 7 fixed-partitions partitions found on MTD device spi0.0
[ 2.997998] Creating 7 MTD partitions on "spi0.0":
[ 3.002824] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 3.008573] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 3.014562] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 3.021111] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 3.027422] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 3.034427] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 3.040360] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 3.047214] mdio_bus fixed-0: GPIO lookup for consumer reset
[ 3.052917] mdio_bus fixed-0: using lookup tables for GPIO lookup
[ 3.059037] mdio_bus fixed-0: No GPIO consumer reset found
[ 3.064569] libphy: Fixed MDIO Bus: probed
[ 3.071724] mdio_bus 48485000.mdio: GPIO lookup for consumer reset
[ 3.077933] mdio_bus 48485000.mdio: using device tree for GPIO lookup
[ 3.084443] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/ethernet@48484000/mdio@48485000[0]'
[ 3.095550] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/ethernet@48484000/mdio@48485000[0]'
[ 3.106564] mdio_bus 48485000.mdio: using lookup tables for GPIO lookup
[ 3.113216] mdio_bus 48485000.mdio: No GPIO consumer reset found
[ 3.171237] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 3.178927] davinci_mdio 48485000.mdio: detected phy mask fffffffe
[ 3.187595] libphy: 48485000.mdio: probed
[ 3.191675] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver Micrel KSZ9031 Gigabit PHY
[ 3.202029] cpsw 48484000.ethernet: Detected MACID = 40:06:a0:ab:9a:2e
[ 3.208638] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[ 3.215072] cpsw 48484000.ethernet: ALE Table size 1024
[ 3.220363] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[ 3.228261] cpsw 48484000.ethernet: cpsw: Detected MACID = 40:06:a0:ab:9a:2f
[ 3.236396] i2c /dev entries driver
[ 3.244539] sdhci: Secure Digital Host Controller Interface driver
[ 3.250747] sdhci: Copyright(c) Pierre Ossman
[ 3.255890] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.262288] sdhci-omap 4809c000.mmc: GPIO lookup for consumer cd
[ 3.268320] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.274910] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@4809c000[0]' - status (0)
[ 3.284821] gpio gpiochip5: Persistence not supported for GPIO 27
[ 3.290945] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.299969] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.304620] sdhci-omap 4809c000.mmc: GPIO lookup for consumer wp
[ 3.310650] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.317220] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@4809c000[0]'
[ 3.326405] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@4809c000[0]'
[ 3.335500] sdhci-omap 4809c000.mmc: using lookup tables for GPIO lookup
[ 3.342238] sdhci-omap 4809c000.mmc: No GPIO consumer wp found
[ 3.348230] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.4
[ 3.355002] sdhci-omap 4809c000.mmc: failed to set system capabilities
[ 3.361628] sdhci-omap 4809c000.mmc: Dropping the link to regulator.4
[ 3.368381] sdhci-omap 480b4000.mmc: GPIO lookup for consumer wp
[ 3.374450] sdhci-omap 480b4000.mmc: using device tree for GPIO lookup
[ 3.381013] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@480b4000[0]'
[ 3.390235] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@480b4000[0]'
[ 3.399350] sdhci-omap 480b4000.mmc: using lookup tables for GPIO lookup
[ 3.406105] sdhci-omap 480b4000.mmc: No GPIO consumer wp found
[ 3.412071] sdhci-omap 480b4000.mmc: failed to set system capabilities
[ 3.418984] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/cpu0-led[0]' - status (0)
[ 3.428369] gpio gpiochip1: Persistence not supported for GPIO 25
[ 3.434497] no flags found for gpios
[ 3.438171] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/usr0-led[0]' - status (0)
[ 3.447533] gpio gpiochip1: Persistence not supported for GPIO 26
[ 3.453658] no flags found for gpios
[ 3.457308] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/heartbeat-led[0]' - status (0)
[ 3.467104] gpio gpiochip1: Persistence not supported for GPIO 27
[ 3.473231] no flags found for gpios
[ 3.476884] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/usr1-led[0]' - status (0)
[ 3.486245] gpio gpiochip1: Persistence not supported for GPIO 28
[ 3.492371] no flags found for gpios
[ 3.496024] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/usr2-led[0]' - status (0)
[ 3.505386] gpio gpiochip1: Persistence not supported for GPIO 21
[ 3.511512] no flags found for gpios
[ 3.515161] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/mmc0-led[0]' - status (0)
[ 3.524523] gpio gpiochip1: Persistence not supported for GPIO 19
[ 3.530639] no flags found for gpios
[ 3.534612] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.544950] NET: Registered protocol family 10
[ 3.560241] Segment Routing with IPv6
[ 3.564027] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.570370] NET: Registered protocol family 17
[ 3.575051] Key type dns_resolver registered
[ 3.579455] Registering SWP/SWPB emulation handler
[ 3.584285] omap_voltage_late_init: Voltage driver support not added
[ 3.590664] Power Management for TI OMAP4+ devices.
[ 3.596157] Loading compiled-in X.509 certificates
[ 3.623872] dmm 4e000000.dmm: workaround for errata i878 in use
[ 3.631488] dmm 4e000000.dmm: initialized all PAT entries
[ 3.637952] tpd12s015 encoder@0: GPIO lookup for consumer (null)
[ 3.644028] tpd12s015 encoder@0: using device tree for GPIO lookup
[ 3.650245] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/encoder@0[0]'
[ 3.658561] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/encoder@0[0]'
[ 3.666784] tpd12s015 encoder@0: using lookup tables for GPIO lookup
[ 3.673176] tpd12s015 encoder@0: No GPIO consumer (null) found
[ 3.679033] tpd12s015 encoder@0: GPIO lookup for consumer (null)
[ 3.685073] tpd12s015 encoder@0: using device tree for GPIO lookup
[ 3.691293] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/encoder@0[1]'
[ 3.699596] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/encoder@0[1]'
[ 3.707818] tpd12s015 encoder@0: using lookup tables for GPIO lookup
[ 3.714208] tpd12s015 encoder@0: No GPIO consumer (null) found
[ 3.720065] tpd12s015 encoder@0: GPIO lookup for consumer (null)
[ 3.726104] tpd12s015 encoder@0: using device tree for GPIO lookup
[ 3.732336] of_get_named_gpiod_flags: parsed 'gpios' property of node '/encoder@0[2]' - status (0)
[ 3.741387] gpio gpiochip6: Persistence not supported for GPIO 12
[ 3.748197] sdhci-omap 4809c000.mmc: GPIO lookup for consumer cd
[ 3.754256] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.760826] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@4809c000[0]' - status (0)
[ 3.770738] gpio gpiochip5: Persistence not supported for GPIO 27
[ 3.776873] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.785704] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.790341] sdhci-omap 4809c000.mmc: GPIO lookup for consumer wp
[ 3.796381] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.802951] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@4809c000[0]'
[ 3.812137] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@4809c000[0]'
[ 3.821230] sdhci-omap 4809c000.mmc: using lookup tables for GPIO lookup
[ 3.827959] sdhci-omap 4809c000.mmc: No GPIO consumer wp found
[ 3.833980] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.4
[ 3.840745] sdhci-omap 4809c000.mmc: failed to set system capabilities
[ 3.847386] sdhci-omap 4809c000.mmc: Dropping the link to regulator.4
[ 3.854379] sdhci-omap 480b4000.mmc: GPIO lookup for consumer wp
[ 3.860411] sdhci-omap 480b4000.mmc: using device tree for GPIO lookup
[ 3.867018] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@480b4000[0]'
[ 3.876229] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@480b4000[0]'
[ 3.885326] sdhci-omap 480b4000.mmc: using lookup tables for GPIO lookup
[ 3.892065] sdhci-omap 480b4000.mmc: No GPIO consumer wp found
[ 3.898037] sdhci-omap 480b4000.mmc: failed to set system capabilities
[ 3.905435] sdhci-omap 4809c000.mmc: GPIO lookup for consumer cd
[ 3.911483] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.918059] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@4809c000[0]' - status (0)
[ 3.927944] gpio gpiochip5: Persistence not supported for GPIO 27
[ 3.934077] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.942912] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.947549] sdhci-omap 4809c000.mmc: GPIO lookup for consumer wp
[ 3.953590] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.960149] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@4809c000[0]'
[ 3.969336] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@4809c000[0]'
[ 3.978430] sdhci-omap 4809c000.mmc: using lookup tables for GPIO lookup
[ 3.985167] sdhci-omap 4809c000.mmc: No GPIO consumer wp found
[ 3.991123] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.4
[ 3.997896] sdhci-omap 4809c000.mmc: failed to set system capabilities
[ 4.004518] sdhci-omap 4809c000.mmc: Dropping the link to regulator.4
[ 4.011444] sdhci-omap 480b4000.mmc: GPIO lookup for consumer wp
[ 4.017476] sdhci-omap 480b4000.mmc: using device tree for GPIO lookup
[ 4.024071] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@480b4000[0]'
[ 4.033278] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@480b4000[0]'
[ 4.042375] sdhci-omap 480b4000.mmc: using lookup tables for GPIO lookup
[ 4.049105] sdhci-omap 480b4000.mmc: No GPIO consumer wp found
[ 4.055064] sdhci-omap 480b4000.mmc: failed to set system capabilities
[ 4.062398] hctosys: unable to open rtc device (rtc0)
[ 4.068236] ALSA device list:
[ 4.072396] No soundcards found.
[ 4.076548] Waiting for root device PARTUUID=3c5d1d1b-02...
[ 34.401227] pbias_mmc_omap5: disabling
thanks and regards
chandana