Part Number: AM3359
Other Parts Discussed in Thread: SYSCONFIG
Dear TI Support Team,
We are trying to configure the GPMC in AM3359 processor using DTS, our GPMC is communicating with end device(ARTIX 7 FPGA) on Chip Select "3".
I am referring to the Documentation provided with the Linux source code.
Path: Documentation/devicetree/bindings/memory-controllers/omap-gpmc.txt
Still we are facing challenge with configuring GPMC_SYSCONFIG, GPMC_IRQENABLE, GPMC_STATUS and CONFIG 7 using DTS.
can you please provide some information as how or which field we can configure in DTS.
We have attached our required GPMC registers value and read back value below.
-----expected-----
mwr 0x50000010 0x00000008
mwr 0x5000001C 0x00000200
mwr 0x50000054 0x00000000
mwr 0x50000108 0x00000f50
----Received-----
root@RCU:~# mrd 0x50000010 0x1
0x00000011
root@RCU:~# mrd 0x5000001C 0x1
0x00000000
root@RCU:~# mrd 0x50000054 0x1
0x00000301
root@RCU:~# mrd 0x50000108 0x1
0x00000F43
Also, we have attached the DTS node for GPMC below
&gpmc {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&mygpmc1_pins_default>;
#address-cells = <2>;
#size-cells = <1>;
ranges = < 0 0 0x08000000 0x01000000 /*CD0: 256MB for NAND 0x1000000 */
3 0 0x03000000 0x01000000>; /*CS3: configuration memory
mapping 127KB for FPGA GPMC */
r4_gpmc: r4_gpmc@50000000 {
compatible = "ti,omap-gpmc";
reg = <3 0 0x01000000>; /* CS3, offset 0, IO size 4*/
interrupt-parent = <&gpmc>;
interrupt-controller;
interrupts = <2 IRQ_TYPE_EDGE_FALLING>, /* GPMC Wait0 active low*/
<3 IRQ_TYPE_EDGE_FALLING>; /* GPMC Wait1 active low*/
#interrupts-cells = <2>;
gpmc,num-cs = <6>;
gpmc,num-waitpins = <2>;
gpmc,sync-clk-ps = <10000>;
/*GPMC Config 2 details*/
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <290>;
gpmc,cs-wr-off-ns = <90>;
/*GPMC Config 3 details*/
gpmc,adv-on-ns = <0>;
gpmc,adv-rd-off-ns = <10>;
gpmc,adv-wr-off-ns = <10>;
gpmc,we-on-ns = <20>;
gpmc,we-off-ns = <80>;
gpmc,adv-aad-mux-on-ns = <0>;
gpmc,adv-aad-mux-rd-off-ns = <0>;
gpmc,adv-aad-mux-wr-off-ns = <0>;
/*GPMC Config 4 details*/
gpmc,oe-on-ns = <30>;
gpmc,oe-off-ns = <290>;
gpmc,oe-aad-mux-on-ns = <0>;
/*GPMC Config 5,6 wait-monitoring-ns details*/
gpmc,page-burst-access-ns = <10>;
gpmc,access-ns = <80>;
gpmc,rd-cycle-ns = <310>;
gpmc,wr-cycle-ns = <310>;
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <20>;
gpmc,clk-activation-ns = <10>;
gpmc,wait-monitoring-ns = <10>;
/*GPMC Boolean timing parameters*/
gpmc,cycle2cycle-diffcsen = "true";
gpmc,cycle2cycle-samecsen = "true";
/*GPMC OMAP3+ & AM335x parameters*/
gpmc,wr-access-ns = <20>;
gpmc,wr-data-mux-bus-ns = <30>;
/*GPMC chip select settings*/
gpmc,burst-read = <0>;
gpmc,burst-write = <0>;
gpmc,burst-wrap = <0>;
gpmc,device-width = <2>; /*1 for 8 & 2 for 16 bit*/
gpmc,mux-add-data = <2>;
gpmc,sync-read = <1>;
gpmc,sync-write = <1>;
gpmc,wait-pin = <1>;
gpmc,wait-on-read = <1>;
gpmc,wait-on-write = <1>;
gpmc,device-nand = "false";
};
};
Best Regards,
Rishabh Mishra