Part Number: AM3358
I have the same or similar issue as described in
The kernel 5.4.106 from the SDK 07.03.00.005 works as expected, there are no issues with the GPU, kmscube and qt eglfs examples work.
I tried the following setup:
- ti linux kernel 5.10.41 (repo: git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git, branch: ti-linux-5.10.y, tag: 08.00.00.004)
- sgx kernel module 1.17.4948957 (repo: git://git.ti.com/graphics/omap5-sgx-ddk-linux.git, branch: ti-img-sgx/1.17.4948957/k5.10)
- (repo: git://git.ti.com/processor-firmware/ti-amx3-cm3-pm-firmware.git, branch: ti-v4.1.y, tag: 08.00.00.004)
with the following result:
- the sgx kernel module logs errors about some timeouts and transitions failed etc.
- after a reboot weston starts up but and keeps running but there is no display output (compared to running the 5.4.106 ti-kernel)
- after killing weston and running "kmscube -f RG16" I get one rendered frame with the cube once. after CTRL-C and restart of kmscube
- stop and restart of rc.pvr.service gives me this output:
root@am335x-evm:~# rmmod pvrsrvkm [13110.997961] PVR_K:(Error): PollForValueKM: Timeout. Expected 0x8 but found 0x0 (mask 0x8). [13111.006286] PVR_K:(Error): SGXPrePowerState: Wait for SGX ukernel power transition failed. [13111.015341] PVR_K: SGX debug (SGX_DDK sgxddk 1.17@4948957) [13111.021185] PVR_K: Host Ctl flags= 00000006 [13111.025477] PVR_K: SGX Host control: [13111.029499] PVR_K: (HC-0) 0x00000001 0x0000002C 0x00000000 0x00000000 [13111.036060] PVR_K: (HC-10) 0x00000000 0x00000000 0x00000014 0x00030D40 [13111.043113] PVR_K: (HC-20) 0x00000000 0x00000004 0x00000006 0x00000000 [13111.050017] PVR_K: (HC-30) 0x00000000 0x00C7A1AB 0xEFC7C740 0x00000000 [13111.056675] PVR_K: (HC-40) 0x00000000 0x00000000 0x00000080 0x00000000 [13111.063779] PVR_K: SGX TA/3D control: [13111.067463] PVR_K: (T3C-0) 0x0F003000 0x0F003140 0x0F002000 0x00000000 [13111.074529] PVR_K: (T3C-10) 0x00000000 0x00000001 0x00000002 0x00000001 [13111.081508] PVR_K: (T3C-20) 0x0F00AEA0 0x00000000 0x00000000 0x00000000 [13111.088508] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.095250] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.102373] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.109339] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.116074] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.123172] PVR_K: (T3C-80) 0x00000000 0x00000000 0x00000000 0x0F000000 [13111.130126] PVR_K: (T3C-90) 0x83C07000 0x0F08C000 0x00000000 0x0F09E840 [13111.136861] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x0F09E840 0x00000000 [13111.144010] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.150989] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.157724] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000 [13111.164840] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x00000000 0x00000000 [13111.171801] PVR_K: (T3C-F0) 0x00000000 0x000003AD 0x000003AD 0x00000000 [13111.178771] PVR_K: (T3C-100) 0x00000003 0x00000000 0x00000000 0x00000000 [13111.185604] PVR_K: (T3C-110) 0x00000000 0x00000000 0x00000000 0x00000000 [13111.192778] PVR_K: (T3C-120) 0x0F00AEA0 0x0F08C000 0x00000000 0x00000000 [13111.199844] PVR_K: SGX Kernel CCB WO:0x42 RO:0x42 [13111.204570] PVR_K: Active syncs root@am335x-evm:~# root@am335x-evm:~# root@am335x-evm:~# systemctl start rc.pvr.service [13128.615818] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1 [13128.661992] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ] [13129.667980] PVR_K:(Error): PollForValueKM: Timeout. Expected 0x1 but found 0x0 (mask 0x1). [13129.676305] PVR_K:(Error): SGXInitialise: Wait for uKernel initialisation failed [13129.684356] PVR_K: SGX debug (SGX_DDK sgxddk 1.17@4948957) [13129.690201] PVR_K: Host Ctl flags= 00000006 [13129.694495] PVR_K: SGX Host control: [13129.698479] PVR_K: (HC-0) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.705041] PVR_K: (HC-10) 0x00000000 0x00000000 0x00000014 0x00030D40 [13129.712089] PVR_K: (HC-20) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.719062] PVR_K: (HC-30) 0x00000000 0x00000000 0xFCA5D120 0x00000000 [13129.725721] PVR_K: (HC-40) 0x00000000 0x00000000 0x00000000 0x00030012 [13129.732772] PVR_K: SGX TA/3D control: [13129.736458] PVR_K: (T3C-0) 0x0F003000 0x0F003140 0x0F002000 0x00000000 [13129.743498] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000 [13129.750541] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.757277] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.764410] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.771395] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.778408] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.785142] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.792250] PVR_K: (T3C-80) 0x00000000 0x00000000 0x00000000 0x0F000000 [13129.799278] PVR_K: (T3C-90) 0x83F3C000 0x00000000 0x00000000 0x00000000 [13129.806014] PVR_K: (T3C-A0) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.813134] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.820120] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.826856] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000 [13129.833948] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x00000000 0x00000000 [13129.840914] PVR_K: (T3C-F0) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.847648] PVR_K: (T3C-100) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.854832] PVR_K: (T3C-110) 0x00000000 0x00000000 0x00000000 0x00000000 [13129.861882] PVR_K: (T3C-120) 0x00000000 0x00000000 0x000003C0 0x00030012 [13129.868937] PVR_K: SGX Kernel CCB WO:0x0 RO:0x0 [13129.873488] PVR_K: Active syncs [13129.876645] PVR_K:(Error): SGXPostPowerState: SGXInitialise failed [13129.883386] PVR_K:(Error): PVRSRVSetDevicePowerStateKM : Transition to 0 FAILED 0x18 [13129.891423] PVR_K:(Error): SGXScheduleCCBCommandKM failed to power up device - ui32CallerID:-1 eError:24 [13129.901178] PVR_K:(Error): SGXGetMiscInfoUkernel: SGXScheduleCCBCommandKM failed. [13129.908925] PVR_K: (FAIL) SGXInit: Unable to validate hardware core revision [13129.916010] PVR_K:(Error): PVRSRVFinaliseSystem: Failed PVRSRVDevInitCompatCheck call (device index: 0) [13129.925964] PVR_K:(Error): BridgedDispatchKM: Initialisation failed. Driver unusable. root@am335x-evm:~#
question: what is your plan with regards to releasing the ti kernel 5.10.y and/or SDK 08.00.00.00x?
lsmod:
Module Size Used by pru_rproc 24576 0 icss_iep 24576 0 irq_pruss_intc 16384 0 ti_am335x_adc 16384 0 ti_am335x_tsc 16384 0 snd_soc_simple_card 20480 0 snd_soc_simple_card_utils 24576 1 snd_soc_simple_card omap_aes_driver 24576 0 omap_crypto 16384 1 omap_aes_driver libaes 16384 1 omap_aes_driver pruss 16384 1 pru_rproc pm33xx 16384 0 omap_sham 28672 0 crypto_engine 16384 2 omap_aes_driver,omap_sham ti_emif_sram 16384 1 pm33xx pvrsrvkm 405504 2 musb_dsps 20480 0 musb_hdrc 110592 1 musb_dsps udc_core 28672 1 musb_hdrc phy_am335x 16384 2 usbcore 241664 1 musb_hdrc phy_generic 16384 1 phy_am335x usb_common 16384 5 phy_am335x,udc_core,musb_hdrc,musb_dsps,usbcore wkup_m3_ipc 16384 1 pm33xx phy_am335x_control 16384 1 phy_am335x at24 20480 0 rtc_omap 20480 4 pm33xx omap_wdt 16384 0 ti_am335x_tscadc 16384 2 ti_am335x_adc,ti_am335x_tsc wkup_m3_rproc 16384 1 sch_fq_codel 20480 1
dmesg:
[ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.10.41 (eric_koch@LinuxDev) (arm-none-linux-gnueabihf-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 PREEMPT Wed Jul 28 16:11:36 AWST 2021 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black with LCD4 cape [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x9c800000 [ 0.000000] Zone ranges: [ 0.000000] Normal [mem 0x0000000080000000-0x000000009fefffff] [ 0.000000] HighMem empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009fefffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000009fefffff] [ 0.000000] On node 0 totalpages: 130816 [ 0.000000] Normal zone: 1150 pages used for memmap [ 0.000000] Normal zone: 0 pages reserved [ 0.000000] Normal zone: 130816 pages, LIFO batch:31 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.0 (sgx neon) [ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 [ 0.000000] pcpu-alloc: [0] 0 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129666 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=62c62eef-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 453392K/523264K available (9216K kernel code, 692K rwdata, 3316K rodata, 1024K init, 281K bss, 20720K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] random: get_random_bytes called from start_kernel+0x324/0x4e0 with crng_init=0 [ 0.000000] TI gptimer clocksource: always-on /ocp/interconnect@44c00000/segment@200000/target-module@31000 [ 0.000010] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000027] clocksource: dmtimer: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000331] TI gptimer clockevent: 24000000 Hz at /ocp/interconnect@48000000/segment@0/target-module@40000 [ 0.001253] Console: colour dummy device 80x30 [ 0.001292] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.001300] This ensures that you still see kernel messages. Please [ 0.001306] update your kernel commandline. [ 0.001357] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736) [ 0.090401] pid_max: default: 32768 minimum: 301 [ 0.090559] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.090575] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.091415] CPU: Testing write buffer coherency: ok [ 0.091487] CPU0: Spectre v2: using BPIALL workaround [ 0.092288] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.092428] rcu: Hierarchical SRCU implementation. [ 0.092515] EFI services will not be available. [ 0.092871] devtmpfs: initialized [ 0.102873] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.103125] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.103148] futex hash table entries: 256 (order: -1, 3072 bytes, linear) [ 0.106523] pinctrl core: initialized pinctrl subsystem [ 0.107421] DMI not present or invalid. [ 0.107859] NET: Registered protocol family 16 [ 0.110008] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.127596] l3-aon-clkctrl:0000:0: failed to disable [ 0.128757] thermal_sys: Registered thermal governor 'fair_share' [ 0.128768] thermal_sys: Registered thermal governor 'bang_bang' [ 0.128782] thermal_sys: Registered thermal governor 'step_wise' [ 0.128789] thermal_sys: Registered thermal governor 'user_space' [ 0.129133] cpuidle: using governor ladder [ 0.129167] cpuidle: using governor menu [ 1.208377] No ATAGs? [ 1.208406] hw-breakpoint: debug architecture 0x4 unsupported. [ 1.231618] reg-fixed-voltage fixedregulator0: GPIO lookup for consumer (null) [ 1.231634] reg-fixed-voltage fixedregulator0: using device tree for GPIO lookup [ 1.231669] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator0[0]' [ 1.231687] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator0[0]' [ 1.231698] reg-fixed-voltage fixedregulator0: using lookup tables for GPIO lookup [ 1.231707] reg-fixed-voltage fixedregulator0: No GPIO consumer (null) found [ 1.232709] iommu: Default domain type: Translated [ 1.234742] SCSI subsystem initialized [ 1.235204] mc: Linux media interface: v0.10 [ 1.235244] videodev: Linux video capture interface: v2.00 [ 1.235350] pps_core: LinuxPPS API ver. 1 registered [ 1.235360] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 1.235382] PTP clock support registered [ 1.235442] EDAC MC: Ver: 3.0.0 [ 1.236660] Advanced Linux Sound Architecture Driver Initialized. [ 1.237930] clocksource: Switched to clocksource dmtimer [ 1.245084] NET: Registered protocol family 2 [ 1.245299] IP idents hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 1.246257] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear) [ 1.246309] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear) [ 1.246350] TCP bind hash table entries: 4096 (order: 2, 16384 bytes, linear) [ 1.246389] TCP: Hash tables configured (established 4096 bind 4096) [ 1.246498] UDP hash table entries: 256 (order: 0, 4096 bytes, linear) [ 1.246519] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear) [ 1.246657] NET: Registered protocol family 1 [ 1.247192] RPC: Registered named UNIX socket transport module. [ 1.247208] RPC: Registered udp transport module. [ 1.247215] RPC: Registered tcp transport module. [ 1.247221] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.247240] PCI: CLS 0 bytes, default 64 [ 1.248522] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 1.249756] Initialise system trusted keyrings [ 1.250108] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 1.253650] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 1.254422] NFS: Registering the id_resolver key type [ 1.254474] Key type id_resolver registered [ 1.254483] Key type id_legacy registered [ 1.254527] ntfs: driver 2.1.32 [Flags: R/O]. [ 1.255107] Key type asymmetric registered [ 1.255125] Asymmetric key parser 'x509' registered [ 1.255173] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 1.255185] io scheduler mq-deadline registered [ 1.255194] io scheduler kyber registered [ 1.635559] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 1.753444] debugfs: Directory '49000000.dma' with parent 'dmaengine' already present! [ 1.753489] edma 49000000.dma: TI EDMA DMA engine driver [ 1.773285] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 1.776916] pwm-backlight backlight: GPIO lookup for consumer enable [ 1.776936] pwm-backlight backlight: using device tree for GPIO lookup [ 1.776971] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]' [ 1.776989] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]' [ 1.777001] pwm-backlight backlight: using lookup tables for GPIO lookup [ 1.777010] pwm-backlight backlight: No GPIO consumer enable found [ 1.777034] pwm-backlight backlight: supply power not found, using dummy regulator [ 1.778802] gpio-clk clk_mcasp0: GPIO lookup for consumer enable [ 1.778819] gpio-clk clk_mcasp0: using device tree for GPIO lookup [ 1.778843] gpio-clk clk_mcasp0: No GPIO consumer enable found [ 1.824699] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 1.829152] omap8250 44e09000.serial: GPIO lookup for consumer rs485-term [ 1.829171] omap8250 44e09000.serial: using device tree for GPIO lookup [ 1.829212] of_get_named_gpiod_flags: can't parse 'rs485-term-gpios' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@9000/serial@0[0]' [ 1.829235] of_get_named_gpiod_flags: can't parse 'rs485-term-gpio' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@9000/serial@0[0]' [ 1.829249] omap8250 44e09000.serial: using lookup tables for GPIO lookup [ 1.829258] omap8250 44e09000.serial: No GPIO consumer rs485-term found [ 1.829304] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 20, base_baud = 3000000) is a 8250 [ 2.490918] printk: console [ttyS0] enabled [ 2.498145] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 2.506160] tilcdc-panel panel: GPIO lookup for consumer enable [ 2.506174] tilcdc-panel panel: using device tree for GPIO lookup [ 2.506205] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/panel[0]' [ 2.506222] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/panel[0]' [ 2.506234] tilcdc-panel panel: using lookup tables for GPIO lookup [ 2.506242] tilcdc-panel panel: No GPIO consumer enable found [ 2.507411] random: fast init done [ 2.511218] random: crng init done [ 2.516202] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on minor 0 [ 2.567470] Console: switching to colour frame buffer device 60x34 [ 2.591608] tilcdc 4830e000.lcdc: [drm] fb0: tilcdcdrmfb frame buffer device [ 2.614254] brd: module loaded [ 2.624132] loop: module loaded [ 2.631888] mdio_bus fixed-0: GPIO lookup for consumer reset [ 2.631906] mdio_bus fixed-0: using lookup tables for GPIO lookup [ 2.631915] mdio_bus fixed-0: No GPIO consumer reset found [ 2.631945] libphy: Fixed MDIO Bus: probed [ 2.639504] i2c /dev entries driver [ 2.645563] cpuidle: enable-method property 'ti,am3352' found operations [ 2.653049] sdhci: Secure Digital Host Controller Interface driver [ 2.659322] sdhci: Copyright(c) Pierre Ossman [ 2.664708] sdhci-pltfm: SDHCI platform and OF driver helper [ 2.671956] sdhci-omap 48060000.mmc: GPIO lookup for consumer cd [ 2.671971] sdhci-omap 48060000.mmc: using device tree for GPIO lookup [ 2.671998] sdhci-omap 48060000.mmc: No GPIO consumer cd found [ 2.672567] sdhci-omap 481d8000.mmc: GPIO lookup for consumer wp [ 2.672578] sdhci-omap 481d8000.mmc: using device tree for GPIO lookup [ 2.672619] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@48000000/segment@100000/target-module@d8000/mmc@0[0]' [ 2.672642] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@48000000/segment@100000/target-module@d8000/mmc@0[0]' [ 2.672653] sdhci-omap 481d8000.mmc: using lookup tables for GPIO lookup [ 2.672661] sdhci-omap 481d8000.mmc: No GPIO consumer wp found [ 2.672819] sdhci-omap 481d8000.mmc: supply vqmmc not found, using dummy regulator [ 2.681587] ledtrig-cpu: registered to indicate activity on CPUs [ 2.701875] davinci-mcasp 48038000.mcasp: IRQ common not found [ 2.719453] NET: Registered protocol family 10 [ 2.724920] Segment Routing with IPv6 [ 2.734953] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 2.748626] NET: Registered protocol family 17 [ 2.753471] Key type dns_resolver registered [ 2.767960] omap_voltage_late_init: Voltage driver support not added [ 2.778069] Loading compiled-in X.509 certificates [ 2.800993] gpio gpiochip0: (gpio-0-31): created GPIO range 0->7 ==> 44e10800.pinmux PIN 82->89 [ 2.801020] gpio gpiochip0: (gpio-0-31): created GPIO range 8->11 ==> 44e10800.pinmux PIN 52->55 [ 2.801032] gpio gpiochip0: (gpio-0-31): created GPIO range 12->15 ==> 44e10800.pinmux PIN 94->97 [ 2.801044] gpio gpiochip0: (gpio-0-31): created GPIO range 16->17 ==> 44e10800.pinmux PIN 71->72 [ 2.801055] gpio gpiochip0: (gpio-0-31): created GPIO range 18->18 ==> 44e10800.pinmux PIN 135->135 [ 2.801066] gpio gpiochip0: (gpio-0-31): created GPIO range 19->20 ==> 44e10800.pinmux PIN 108->109 [ 2.801078] gpio gpiochip0: (gpio-0-31): created GPIO range 21->21 ==> 44e10800.pinmux PIN 73->73 [ 2.801090] gpio gpiochip0: (gpio-0-31): created GPIO range 22->23 ==> 44e10800.pinmux PIN 8->9 [ 2.801101] gpio gpiochip0: (gpio-0-31): created GPIO range 26->27 ==> 44e10800.pinmux PIN 10->11 [ 2.801118] gpio gpiochip0: (gpio-0-31): created GPIO range 28->28 ==> 44e10800.pinmux PIN 74->74 [ 2.801131] gpio gpiochip0: (gpio-0-31): created GPIO range 29->29 ==> 44e10800.pinmux PIN 81->81 [ 2.801157] gpio gpiochip0: (gpio-0-31): created GPIO range 30->31 ==> 44e10800.pinmux PIN 28->29 [ 2.801496] gpio gpiochip0: (gpio-0-31): added GPIO chardev (254:0) [ 2.801593] gpio gpiochip0: registered GPIOs 0 to 31 on gpio-0-31 [ 2.801646] OMAP GPIO hardware version 0.1 [ 2.806836] i2c i2c-0: GPIO lookup for consumer scl [ 2.806851] i2c i2c-0: using device tree for GPIO lookup [ 2.806887] of_get_named_gpiod_flags: can't parse 'scl-gpios' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@b000/i2c@0[0]' [ 2.806908] of_get_named_gpiod_flags: can't parse 'scl-gpio' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@b000/i2c@0[0]' [ 2.806922] i2c i2c-0: using lookup tables for GPIO lookup [ 2.806929] i2c i2c-0: No GPIO consumer scl found [ 2.806949] i2c i2c-0: GPIO lookup for consumer sda [ 2.806955] i2c i2c-0: using device tree for GPIO lookup [ 2.806976] of_get_named_gpiod_flags: can't parse 'sda-gpios' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@b000/i2c@0[0]' [ 2.806996] of_get_named_gpiod_flags: can't parse 'sda-gpio' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@b000/i2c@0[0]' [ 2.807005] i2c i2c-0: using lookup tables for GPIO lookup [ 2.807012] i2c i2c-0: No GPIO consumer sda found [ 2.818000] mmc1: SDHCI controller on 481d8000.mmc [481d8000.mmc] using External DMA [ 2.838440] tps65217-pmic: Failed to locate of_node [id: -1] [ 2.850451] tps65217-bl: Failed to locate of_node [id: -1] [ 2.858948] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.864867] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.871130] gpio gpiochip1: (gpio-32-63): created GPIO range 0->7 ==> 44e10800.pinmux PIN 0->7 [ 2.871149] gpio gpiochip1: (gpio-32-63): created GPIO range 8->11 ==> 44e10800.pinmux PIN 90->93 [ 2.871161] gpio gpiochip1: (gpio-32-63): created GPIO range 12->27 ==> 44e10800.pinmux PIN 12->27 [ 2.871173] gpio gpiochip1: (gpio-32-63): created GPIO range 28->31 ==> 44e10800.pinmux PIN 30->33 [ 2.871474] gpio gpiochip1: (gpio-32-63): added GPIO chardev (254:1) [ 2.871560] gpio gpiochip1: registered GPIOs 32 to 63 on gpio-32-63 [ 2.872874] i2c i2c-2: GPIO lookup for consumer scl [ 2.872890] i2c i2c-2: using device tree for GPIO lookup [ 2.872924] of_get_named_gpiod_flags: can't parse 'scl-gpios' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0[0]' [ 2.872946] of_get_named_gpiod_flags: can't parse 'scl-gpio' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0[0]' [ 2.872959] i2c i2c-2: using lookup tables for GPIO lookup [ 2.872967] i2c i2c-2: No GPIO consumer scl found [ 2.872986] i2c i2c-2: GPIO lookup for consumer sda [ 2.872992] i2c i2c-2: using device tree for GPIO lookup [ 2.873013] of_get_named_gpiod_flags: can't parse 'sda-gpios' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0[0]' [ 2.873034] of_get_named_gpiod_flags: can't parse 'sda-gpio' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0[0]' [ 2.873042] i2c i2c-2: using lookup tables for GPIO lookup [ 2.873049] i2c i2c-2: No GPIO consumer sda found [ 2.873964] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz [ 2.880112] gpio gpiochip2: (gpio-64-95): created GPIO range 0->17 ==> 44e10800.pinmux PIN 34->51 [ 2.880129] gpio gpiochip2: (gpio-64-95): created GPIO range 18->21 ==> 44e10800.pinmux PIN 77->80 [ 2.880141] gpio gpiochip2: (gpio-64-95): created GPIO range 22->31 ==> 44e10800.pinmux PIN 56->65 [ 2.880417] gpio gpiochip2: (gpio-64-95): added GPIO chardev (254:2) [ 2.880493] gpio gpiochip2: registered GPIOs 64 to 95 on gpio-64-95 [ 2.880854] gpio gpiochip3: (gpio-96-127): created GPIO range 0->4 ==> 44e10800.pinmux PIN 66->70 [ 2.880869] gpio gpiochip3: (gpio-96-127): created GPIO range 5->6 ==> 44e10800.pinmux PIN 98->99 [ 2.880880] gpio gpiochip3: (gpio-96-127): created GPIO range 7->8 ==> 44e10800.pinmux PIN 75->76 [ 2.880891] gpio gpiochip3: (gpio-96-127): created GPIO range 13->13 ==> 44e10800.pinmux PIN 141->141 [ 2.880902] gpio gpiochip3: (gpio-96-127): created GPIO range 14->21 ==> 44e10800.pinmux PIN 100->107 [ 2.881122] gpio gpiochip3: (gpio-96-127): added GPIO chardev (254:3) [ 2.881203] gpio gpiochip3: registered GPIOs 96 to 127 on gpio-96-127 [ 2.884257] gpio-clk clk_mcasp0: GPIO lookup for consumer enable [ 2.884275] gpio-clk clk_mcasp0: using device tree for GPIO lookup [ 2.884325] of_get_named_gpiod_flags: parsed 'enable-gpios' property of node '/clk_mcasp0[0]' - status (0) [ 2.884409] gpio gpiochip1: Persistence not supported for GPIO 27 [ 2.887869] sdhci-omap 48060000.mmc: GPIO lookup for consumer cd [ 2.887888] sdhci-omap 48060000.mmc: using device tree for GPIO lookup [ 2.888036] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]' - status (0) [ 2.888115] gpio gpiochip0: Persistence not supported for GPIO 6 [ 2.888144] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22) [ 2.896916] sdhci-omap 48060000.mmc: Got CD GPIO [ 2.902406] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led2[0]' - status (0) [ 2.902436] gpio gpiochip1: Persistence not supported for GPIO 21 [ 2.902443] gpio-53 (?): no flags found for gpios [ 2.902737] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led3[0]' - status (0) [ 2.902755] gpio gpiochip1: Persistence not supported for GPIO 22 [ 2.902762] gpio-54 (?): no flags found for gpios [ 2.902866] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led4[0]' - status (0) [ 2.902879] gpio gpiochip1: Persistence not supported for GPIO 23 [ 2.902886] gpio-55 (?): no flags found for gpios [ 2.902985] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led5[0]' - status (0) [ 2.902997] gpio gpiochip1: Persistence not supported for GPIO 24 [ 2.903003] gpio-56 (?): no flags found for gpios [ 2.903900] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio-leds-cape-lcd/lcd-led0[0]' - status (0) [ 2.903928] gpio gpiochip1: Persistence not supported for GPIO 28 [ 2.903935] gpio-60 (?): no flags found for gpios [ 2.906147] ALSA device list: [ 2.909367] No soundcards found. [ 2.912892] mmc1: new high speed MMC card at address 0001 [ 2.919509] sdhci-omap 48060000.mmc: GPIO lookup for consumer wp [ 2.919524] sdhci-omap 48060000.mmc: using device tree for GPIO lookup [ 2.919574] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]' [ 2.919596] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]' [ 2.919611] sdhci-omap 48060000.mmc: using lookup tables for GPIO lookup [ 2.919620] sdhci-omap 48060000.mmc: No GPIO consumer wp found [ 2.919815] sdhci-omap 48060000.mmc: supply vqmmc not found, using dummy regulator [ 2.928474] mmcblk1: mmc1:0001 MMC02G 1.79 GiB [ 2.933296] mmcblk1boot0: mmc1:0001 MMC02G partition 1 1.00 MiB [ 2.948270] mmcblk1boot1: mmc1:0001 MMC02G partition 2 1.00 MiB [ 2.954444] mmcblk1rpmb: mmc1:0001 MMC02G partition 3 128 KiB, chardev (243:0) [ 3.034327] mmc0: SDHCI controller on 48060000.mmc [48060000.mmc] using External DMA [ 3.044303] Waiting for root device PARTUUID=62c62eef-02... [ 3.083484] mmc0: new high speed SDHC card at address 0007 [ 3.090779] mmcblk0: mmc0:0007 SD16G 14.9 GiB [ 3.100071] mmcblk0: p1 p2 [ 16.591539] EXT4-fs (mmcblk0p2): recovery complete [ 16.599899] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 16.608202] VFS: Mounted root (ext4 filesystem) on device 179:50. [ 16.624430] devtmpfs: mounted [ 16.629347] Freeing unused kernel memory: 1024K [ 16.634498] Run /sbin/init as init process [ 16.638645] with arguments: [ 16.638652] /sbin/init [ 16.638657] with environment: [ 16.638662] HOME=/ [ 16.638666] TERM=linux [ 17.073439] systemd[1]: System time before build time, advancing clock. [ 17.118564] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 17.141349] systemd[1]: Detected architecture arm. [ 17.200715] systemd[1]: Set hostname to <am335x-evm>. [ 18.166178] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 18.178857] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 18.193216] systemd[1]: Created slice system-getty.slice. [ 18.230729] systemd[1]: Created slice system-serial\x2dgetty.slice. [ 18.272744] systemd[1]: Created slice User and Session Slice. [ 18.309680] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ 18.348774] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ 18.389682] systemd[1]: Reached target Paths. [ 18.428874] systemd[1]: Reached target Remote File Systems. [ 18.468387] systemd[1]: Reached target Slices. [ 18.480794] systemd[1]: Reached target Swap. [ 18.536082] systemd[1]: Listening on RPCbind Server Activation Socket. [ 18.580388] systemd[1]: Reached target RPC Port Mapper. [ 18.634604] systemd[1]: Listening on Process Core Dump Socket. [ 18.668927] systemd[1]: Listening on initctl Compatibility Named Pipe. [ 18.777481] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. [ 18.789379] systemd[1]: Listening on Journal Socket (/dev/log). [ 18.832414] systemd[1]: Listening on Journal Socket. [ 18.869775] systemd[1]: Listening on Network Service Netlink Socket. [ 18.910908] systemd[1]: Listening on udev Control Socket. [ 18.949046] systemd[1]: Listening on udev Kernel Socket. [ 18.990416] systemd[1]: Condition check resulted in Huge Pages File System being skipped. [ 19.009341] systemd[1]: Mounting POSIX Message Queue File System... [ 19.038571] systemd[1]: Mounting Kernel Debug File System... [ 19.072891] systemd[1]: Mounting Temporary Directory (/tmp)... [ 19.126312] systemd[1]: Starting Create list of static device nodes for the current kernel... [ 19.187051] systemd[1]: Starting Start psplash boot splash screen... [ 19.253494] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon. [ 19.313733] systemd[1]: Starting RPC Bind... [ 19.334660] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 19.398784] systemd[1]: Starting Journal Service... [ 19.454223] systemd[1]: Starting Load Kernel Modules... [ 19.504432] systemd[1]: Starting Remount Root and Kernel File Systems... [ 19.574580] systemd[1]: Starting udev Coldplug all Devices... [ 19.587451] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) [ 19.687483] systemd[1]: Started Start psplash boot splash screen. [ 19.762453] systemd[1]: Started RPC Bind. [ 19.780004] systemd[1]: Mounted POSIX Message Queue File System. [ 19.828778] systemd[1]: Mounted Kernel Debug File System. [ 19.859375] systemd[1]: Mounted Temporary Directory (/tmp). [ 19.908434] systemd[1]: Started Create list of static device nodes for the current kernel. [ 19.958312] systemd[1]: Started Load Kernel Modules. [ 20.002395] systemd[1]: Started Remount Root and Kernel File Systems. [ 20.070075] systemd[1]: Condition check resulted in FUSE Control File System being skipped. [ 20.129278] systemd[1]: Mounting Kernel Configuration File System... [ 20.182181] systemd[1]: Started Start psplash-systemd progress communication helper. [ 20.252582] systemd[1]: Condition check resulted in Rebuild Hardware Database being skipped. [ 20.282494] systemd[1]: Starting Apply Kernel Variables... [ 20.328477] systemd[1]: Condition check resulted in Create System Users being skipped. [ 20.374535] systemd[1]: Starting Create Static Device Nodes in /dev... [ 20.413558] systemd[1]: Started Journal Service. [ 20.901228] systemd-journald[86]: Received client request to flush runtime journal. [ 23.863476] remoteproc remoteproc0: wkup_m3 is available [ 24.603297] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 24.680900] omap_rtc 44e3e000.rtc: char device (252:0) [ 24.680938] omap_rtc 44e3e000.rtc: registered as rtc0 [ 24.686097] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01T00:00:00 UTC (946684800) [ 24.948209] omap_rtc 44e3e000.rtc: GPIO lookup for consumer wp [ 24.948229] omap_rtc 44e3e000.rtc: using device tree for GPIO lookup [ 24.948293] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@3e000/rtc@0[0]' [ 24.948318] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@3e000/rtc@0[0]' [ 24.948335] omap_rtc 44e3e000.rtc: using lookup tables for GPIO lookup [ 24.948344] omap_rtc 44e3e000.rtc: No GPIO consumer wp found [ 25.256887] at24 0-0050: supply vcc not found, using dummy regulator [ 25.303844] remoteproc remoteproc0: powering up wkup_m3 [ 25.364372] at24 0-0050: GPIO lookup for consumer wp [ 25.364391] at24 0-0050: using device tree for GPIO lookup [ 25.364443] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@b000/i2c@0/baseboard_eeprom@50[0]' [ 25.364468] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@44c00000/segment@200000/target-module@b000/i2c@0/baseboard_eeprom@50[0]' [ 25.364484] at24 0-0050: using lookup tables for GPIO lookup [ 25.364493] at24 0-0050: No GPIO consumer wp found [ 25.388945] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write [ 25.430903] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217148 [ 25.570435] at24 2-0054: supply vcc not found, using dummy regulator [ 25.577133] at24 2-0054: GPIO lookup for consumer wp [ 25.577143] at24 2-0054: using device tree for GPIO lookup [ 25.577185] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom0@54[0]' [ 25.577210] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom0@54[0]' [ 25.577225] at24 2-0054: using lookup tables for GPIO lookup [ 25.577234] at24 2-0054: No GPIO consumer wp found [ 25.579311] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 25.579336] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192 [ 25.698733] at24 2-0054: 32768 byte 24c256 EEPROM, writable, 1 bytes/write [ 25.769097] at24 2-0055: supply vcc not found, using dummy regulator [ 25.861383] at24 2-0055: GPIO lookup for consumer wp [ 25.861403] at24 2-0055: using device tree for GPIO lookup [ 25.861449] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom1@55[0]' [ 25.861474] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom1@55[0]' [ 25.861490] at24 2-0055: using lookup tables for GPIO lookup [ 25.861498] at24 2-0055: No GPIO consumer wp found [ 25.890777] at24 2-0056: supply vcc not found, using dummy regulator [ 25.897465] at24 2-0056: GPIO lookup for consumer wp [ 25.897476] at24 2-0056: using device tree for GPIO lookup [ 25.897515] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom2@56[0]' [ 25.897540] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom2@56[0]' [ 25.897554] at24 2-0056: using lookup tables for GPIO lookup [ 25.897562] at24 2-0056: No GPIO consumer wp found [ 25.973468] at24 2-0057: supply vcc not found, using dummy regulator [ 26.076953] at24 2-0057: GPIO lookup for consumer wp [ 26.076973] at24 2-0057: using device tree for GPIO lookup [ 26.077024] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom3@57[0]' [ 26.077049] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/cape_eeprom3@57[0]' [ 26.077065] at24 2-0057: using lookup tables for GPIO lookup [ 26.077074] at24 2-0057: No GPIO consumer wp found [ 26.230003] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer reset [ 26.230026] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup [ 26.230070] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/target-module@47400000/usb-phy@1300[0]' [ 26.230091] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/target-module@47400000/usb-phy@1300[0]' [ 26.230106] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup [ 26.230114] am335x-phy-driver 47401300.usb-phy: No GPIO consumer reset found [ 26.230122] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer vbus-detect [ 26.230129] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup [ 26.230147] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/target-module@47400000/usb-phy@1300[0]' [ 26.230165] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/target-module@47400000/usb-phy@1300[0]' [ 26.230174] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup [ 26.230181] am335x-phy-driver 47401300.usb-phy: No GPIO consumer vbus-detect found [ 26.230302] am335x-phy-driver 47401300.usb-phy: supply vcc not found, using dummy regulator [ 26.397559] usbcore: registered new interface driver usbfs [ 26.467715] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer reset [ 26.467739] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup [ 26.467781] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/target-module@47400000/usb-phy@1b00[0]' [ 26.467801] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/target-module@47400000/usb-phy@1b00[0]' [ 26.467818] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup [ 26.467827] am335x-phy-driver 47401b00.usb-phy: No GPIO consumer reset found [ 26.467835] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer vbus-detect [ 26.467841] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup [ 26.467861] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/target-module@47400000/usb-phy@1b00[0]' [ 26.467878] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/target-module@47400000/usb-phy@1b00[0]' [ 26.467887] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup [ 26.467895] am335x-phy-driver 47401b00.usb-phy: No GPIO consumer vbus-detect found [ 26.468179] am335x-phy-driver 47401b00.usb-phy: supply vcc not found, using dummy regulator [ 26.484210] usbcore: registered new interface driver hub [ 26.544309] usbcore: registered new device driver usb [ 26.811446] pvrsrvkm: loading out-of-tree module taints kernel. [ 26.894138] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 27.088239] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 27.218971] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 [ 27.227324] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 27.298403] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1 [ 27.547582] usb usb1: Product: MUSB HDRC host driver [ 27.589730] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ] [ 27.658082] usb usb1: Manufacturer: Linux 5.10.41 musb-hcd [ 27.663615] usb usb1: SerialNumber: musb-hdrc.1 [ 27.799719] hub 1-0:1.0: USB hub found [ 27.916158] hub 1-0:1.0: 1 port detected [ 31.133591] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 31.307448] omap-sham 53100000.sham: will run requests pump with realtime priority [ 31.439895] PM: bootloader does not support rtc-only! [ 31.545835] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 31.765401] omap-aes 53500000.aes: will run requests pump with realtime priority [ 39.581095] input: ti-tsc as /devices/platform/ocp/44c00000.interconnect/44c00000.interconnect:segment@200000/44e0d000.target-module/44e0d000.tscadc/TI-am335x-tsc.0.auto/input/input0 [ 40.466793] remoteproc remoteproc1: 4a334000.pru is available [ 40.588933] remoteproc remoteproc2: 4a338000.pru is available [ 1136.528565] PVR_K: User requested SGX debug info [ 1136.533280] PVR_K: SGX debug (SGX_DDK sgxddk 1.17@4948957) [ 1136.541208] PVR_K: Host Ctl flags= 00000006 [ 1136.545701] PVR_K: SGX Host control: [ 1136.550719] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001 [ 1136.557551] PVR_K: (HC-10) 0x00000000 0x00000000 0x00000014 0x00030D40 [ 1136.565884] PVR_K: (HC-20) 0x00000000 0x00000004 0x00000004 0x00000000 [ 1136.573558] PVR_K: (HC-30) 0x00000000 0x0010EABD 0xEFC7C740 0x00000000 [ 1136.581170] PVR_K: (HC-40) 0x00000000 0x00000000 0x00000004 0x00000000 [ 1136.588476] PVR_K: SGX TA/3D control: [ 1136.592189] PVR_K: (T3C-0) 0x0F003000 0x0F003140 0x0F002000 0x00000000 [ 1136.599716] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000 [ 1136.606494] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.614044] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.621289] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.628500] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.635313] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.642781] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.650211] PVR_K: (T3C-80) 0x00000000 0x00000000 0x00000000 0x0F000000 [ 1136.657029] PVR_K: (T3C-90) 0x83C07000 0x00000000 0x00000000 0x00000000 [ 1136.664514] PVR_K: (T3C-A0) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.671789] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.679022] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.685831] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000 [ 1136.693267] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x00000000 0x00000000 [ 1136.700538] PVR_K: (T3C-F0) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.707277] PVR_K: (T3C-100) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.714549] PVR_K: (T3C-110) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.721650] PVR_K: (T3C-120) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1136.728749] PVR_K: SGX Kernel CCB WO:0x2 RO:0x2 [ 1136.733309] PVR_K: Active syncs [ 1136.736467] PVR_K: SyncInfo 13: [ 1136.740277] PVR_K: Write ops (0x0d80120c): P/C = 1/0 (0x00000001/0x00000000) [ 1136.747537] PVR_K: Read ops (0x0d801214): P/C = 0/0 (0x00000000/0x00000000) [ 1136.755098] PVR_K: Read ops 2 (0x0d80121c): P/C = 0/0 (0x00000000/0x00000000) [ 1136.762699] PVR_K: SyncInfo 2: [ 1136.765859] PVR_K: Write ops (0x0d801054): P/C = 0/0 (0x00000000/0x00000000) [ 1136.773489] PVR_K: Read ops (0x0d80105c): P/C = 1/0 (0x00000001/0x00000000) [ 1136.780900] PVR_K: Read ops 2 (0x0d801064): P/C = 0/0 (0x00000000/0x00000000) [ 1136.788489] PVR_K: SyncInfo 0: [ 1136.791647] PVR_K: Write ops (0x0d801004): P/C = 1/0 (0x00000001/0x00000000) [ 1136.799408] PVR_K: Read ops (0x0d80100c): P/C = 0/0 (0x00000000/0x00000000) [ 1136.806591] PVR_K: Read ops 2 (0x0d801014): P/C = 0/0 (0x00000000/0x00000000) [ 1147.688070] PVR_K:(Error): PollForValueKM: Timeout. Expected 0x1 but found 0x0 (mask 0x1). [ 1147.696429] PVR_K:(Error): SGXCleanupRequest: Wait for uKernel to clean up (2) failed [ 1147.708085] PVR_K: SGX debug (SGX_DDK sgxddk 1.17@4948957) [ 1147.713625] PVR_K: Host Ctl flags= 00000006 [ 1147.728091] PVR_K: SGX Host control: [ 1147.731722] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000000 [ 1147.738995] PVR_K: (HC-10) 0x00000000 0x00000000 0x00000014 0x00030D40 [ 1147.745648] PVR_K: (HC-20) 0x00000000 0x00000004 0x00000006 0x00000000 [ 1147.752762] PVR_K: (HC-30) 0x00000000 0x00111650 0xEFC7C740 0x00000000 [ 1147.759727] PVR_K: (HC-40) 0x00000000 0x00000000 0x00000012 0x00000000 [ 1147.766385] PVR_K: SGX TA/3D control: [ 1147.770516] PVR_K: (T3C-0) 0x0F003000 0x0F003140 0x0F002000 0x00000000 [ 1147.777247] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000 [ 1147.784454] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.791448] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.798418] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.805162] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.818089] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.824852] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.832191] PVR_K: (T3C-80) 0x00000000 0x00000000 0x00000000 0x0F000000 [ 1147.839263] PVR_K: (T3C-90) 0x83C07000 0x0F08C000 0x00000000 0x0F09E840 [ 1147.845999] PVR_K: (T3C-A0) 0x0F00AEA0 0x0F09D684 0x0F09E840 0x00000000 [ 1147.858073] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.864818] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.872143] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000 [ 1147.879212] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000 [ 1147.885952] PVR_K: (T3C-F0) 0x00000000 0x00000164 0x00000164 0x00000000 [ 1147.898048] PVR_K: (T3C-100) 0x00000003 0x00000000 0x00000000 0x00000000 [ 1147.904882] PVR_K: (T3C-110) 0x00000000 0x00000000 0x00000000 0x00000000 [ 1147.912315] PVR_K: (T3C-120) 0x0F00AEA0 0x0F08C000 0x00000000 0x00000000 [ 1147.919474] PVR_K: SGX Kernel CCB WO:0x8 RO:0x8 [ 1147.924030] PVR_K: Active syncs [ 1147.927248] PVR_K:(Error): FreeResourceByPtr: ERROR calling FreeResource function [ 1147.938828] PVR_K:(Error): RA_TestDelete: detected resource leak! [ 1147.944970] PVR_K:(Error): RA_TestDelete: base = 0x08800000 size=0x3dd000 [ 1147.952507] PVR_K:(Error): BM_DestroyContext_AnyCb: RA_TestDelete failed [ 1147.968111] PVR_K:(Error): BM_DestroyContext: List_BM_HEAP_PVRSRV_ERROR_Any failed root@am335x-evm:~#