Other Parts Discussed in Thread: CCSTUDIO
I have a question about C6flo. (see below)
OS: 32bit Vista
CCS v3.3; OMAP L137;
I have updated my software by installing the new ones:
BIOS 5.41.10.36; C6flo 1.03; code generation 6.1.19; XDC 3.20.08.88
I thought with the new updates I can generate a code with c6flo, but it gave me the error:
[App Writer] (15:46:56.580): Application write failed! Encountered exception:
Access to the path 'C:\Program Files\Texas Instruments\C6Flo_1.03\c6_app_writer_log.txt' is denied.
I guess this is caused by an old software version.
So I uninstalled all of the old software (like BIOS 5.3, XDC 3.10) and added in Control Panel>System Properties > Advanced>Environment the Variables:
Changed the directory to the new installation directory (always used the default folders):
BIOS_INSTALL_DIR
C:\CCStudio_v3.3\bios_5_41_10_36
C6FROOT
C:\Program Files\Texas Instruments\C6Flo_1.03
CGTROOT
C:\Program Files\Texas Instruments\C6000 Code Generation Tools 6.1.9
Added:
XDCPATH
C:\Program Files\Texas Instruments\C6Flo_1.03\Blocks
XDCROOT
C:\CCStudio_v3.3\bios_5_41_10_36
In the end I tested running C6flo in Vista with Windows XP SP2 compatibility mode (no changes)
and set run as administrator, which gave me the log:
C:\Program Files\Texas Instruments\C6Flo_1.03\c6_app_writer.exe -ini="C:\Program Files\Texas Instruments\C6Flo_1.03\Temp\last_app.ini" -c6flo="C:\Program Files\Texas Instruments\C6Flo_1.03" -app="C:\Program Files\Texas Instruments\C6Flo_1.03\Examples\C6747AudioFilter" -xdc="C:\CCStudio_v3.3\bios_5_41_10_36" -cgt="C:\Program Files\Texas Instruments\C6000 Code Generation Tools 6.1.9" -v
[App Writer] (15:48:09.393): Using non-standard buffer alignment in thread0 due to block requirement(s).
[App Writer] (15:48:09.399): Writing codegen helpers...
[App Writer] (15:48:09.443): Generating CFG file...
[App Writer] (15:48:09.453): Running xdc.tools.configuro...
[App Writer] (15:48:09.453): C:/CCStudio_v3.3/bios_5_41_10_36/xs --xdcpath "C:/Program Files/Texas Instruments/C6Flo_1.03/Blocks/" xdc.tools.configuro -t ti.targets.C64P -c "C:/Program Files/Texas Instruments/C6000 Code Generation Tools 6.1.9/" -x ".*" --generationOnly "./AppWriterTemp/c6747_audio_app.cfg"
[App Writer] (15:48:09.456): Application write failed! Encountered exception:
The system cannot find the file specified
[App Writer] (15:48:09.457): Closed after 0,10 seconds.
When I open CCS 3.3 and look up the "about" it tells me "Code Generation Tools v6.1.5", but when I open the Component Manager>Build Tools>C67xx>the mark for C6000 Code Gen Tool is set for v6.1.9
It is also weird when I open DSP/BIOS Graphical Configuration Tool it says in the "about" v5.00 even though 5.41 is installed.
What do I need to change/update to be able to generate code with C6flo?
Thank you very much for you answers