Part Number: AM4379
Other Parts Discussed in Thread: TPS65218, AM4372, TLV320AIC3106
Hi,
We have a customed Am437x-gp-evm board installed ti-sdk-rt-am437x-evm-05.03.00.07, The board is work well but cann't mount SD card.
I can write it in U-boot as following, But when system boot up from NAND, there is no /dev/mmcblk0,mmblk1,...
U-Boot 2018.01-00569-gccad41e-dirty (Jun 08 2019 - 13:39:56 +0800)
CPU : AM437X-GP rev 1.2
Model: TI AM437x GP EVM
DRAM: 1 GiB
PMIC: TPS65218
NAND: 512 MiB
MMC: OMAP SD/MMC: 0
*** Warning - bad CRC, using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Hit any key to stop autoboot: 0
=> printenv partitions
partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_gpt_rootfs}
=> mmc list
OMAP SD/MMC: 0
=> gpt write mmc 0 ${partitions}
Writing GPT: success!
Please advise how to solve this. Thanks!
We check the following :
1) in the modified am437x-gp-evm.dts file:
mmc1_pins: pinmux_mmc1_pins {
pinctrl-single,pins = <
AM4372_IOPAD(0x900,PIN_INPUT_PULLUP | MUX_MODE0) /* D1:mmc0_clk.mmc0_clk */
AM4372_IOPAD(0x904,PIN_INPUT_PULLUP | MUX_MODE0) /* D2:mmc0_cmd.mmc0_cmd */
AM4372_IOPAD(0x8fc,PIN_INPUT_PULLUP | MUX_MODE0) /* C1:mmc0_dat0.mmc0_dat0 */
AM4372_IOPAD(0x8f8,PIN_INPUT_PULLUP | MUX_MODE0) /* C2:mmc0_dat1.mmc0_dat1 */
AM4372_IOPAD(0x8f4,PIN_INPUT_PULLUP | MUX_MODE0) /* B2:mmc0_dat2.mmc0_dat2 */
AM4372_IOPAD(0x8f0,PIN_INPUT_PULLUP | MUX_MODE0) /* B1:mmc0_dat3.mmc0_dat3 */
AM4372_IOPAD(0x960, PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
>;
};
&mmc1 {
status = "okay";
vmmc-supply = <&evm_v3_3d>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc1_pins>;
cd-gpios = <&gpio0 6 GPIO_ACTIVE_LOW>;
};
2) In the kernnel config:
Device Drivers --->
<*>MMC/SD/SDIO card support --->
<*> MMC block device driver
<*>TI OMAP Multimedia Card Interface support
3) the bootup log is( dmesg -k):
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.79-rt47-ga72bf1418c (root@ubuntu) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #2 PREEMPT RT Sat Jul 31 00:21:09 PDT 2021
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM437x GP EVM
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0xbd000000
[ 0.000000] On node 0 totalpages: 262144
[ 0.000000] free_area_init_node: node 0, pgdat c0d54108, node_mem_map ef6f9000
[ 0.000000] Normal zone: 1728 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 196608 pages, LIFO batch:31
[ 0.000000] HighMem zone: 65536 pages, LIFO batch:15
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM437x ES1.2 (sgx neon)
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260416
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 976228K/1048576K available (8192K kernel code, 342K rwdata, 2472K rodata, 1024K init, 273K bss, 23196K reserved, 49152K cma-reserved, 212992K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0900000 (9184 kB)
.init : 0xc0c00000 - 0xc0d00000 (1024 kB)
.data : 0xc0d00000 - 0xc0d55900 ( 343 kB)
.bss : 0xc0d55900 - 0xc0d9a024 ( 274 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] L2C: platform modifies aux control register: 0x0e030000 -> 0x3e430000
[ 0.000000] L2C: DT/platform modifies aux control register: 0x0e030000 -> 0x3e430000
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] OMAP L2C310: ROM does not support power control setting
[ 0.000000] L2C-310 dynamic clock gating disabled, standby mode disabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 256 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c9, AUX_CTRL 0x4e430000
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000012] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000022] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000027] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000156] sched_clock: 64 bits at 500MHz, resolution 2ns, wraps every 4398046511103ns
[ 0.000165] clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0xe6a171a037, max_idle_ns: 881590485102 ns
[ 0.000182] Switching to timer-based delay loop, resolution 2ns
[ 0.000552] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000555] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000976] Console: colour dummy device 80x30
[ 0.001102] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.001104] This ensures that you still see kernel messages. Please
[ 0.001106] update your kernel commandline.
[ 0.001132] Calibrating delay loop (skipped), value calculated using timer frequency.. 1000.00 BogoMIPS (lpj=5000000)
[ 0.001141] pid_max: default: 32768 minimum: 301
[ 0.001313] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001329] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.002118] CPU: Testing write buffer coherency: ok
[ 0.002167] CPU0: Spectre v2: using BPIALL workaround
[ 0.002869] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.003101] Hierarchical SRCU implementation.
[ 0.003724] EFI services will not be available.
[ 0.004635] devtmpfs: initialized
[ 0.014157] random: get_random_u32 called from bucket_table_alloc+0x124/0x27c with crng_init=0
[ 0.014580] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.014907] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.014931] futex hash table entries: 256 (order: 1, 8192 bytes)
[ 0.018208] pinctrl core: initialized pinctrl subsystem
[ 0.018897] DMI not present or invalid.
[ 0.019410] NET: Registered protocol family 16
[ 0.021155] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.098838] gpio gpiochip0: (gpio): added GPIO chardev (254:0)
[ 0.098925] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0 (gpio)
[ 0.099153] OMAP GPIO hardware version 0.1
[ 0.100059] gpio gpiochip1: (gpio): added GPIO chardev (254:1)
[ 0.100146] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip1 (gpio)
[ 0.101129] gpio gpiochip2: (gpio): added GPIO chardev (254:2)
[ 0.101217] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip2 (gpio)
[ 0.102153] gpio gpiochip3: (gpio): added GPIO chardev (254:3)
[ 0.102250] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochip3 (gpio)
[ 0.106167] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/nand_flash_x8, deferring probe
[ 0.109306] No ATAGs?
[ 0.109330] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.109343] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.123062] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.123656] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-v3_3d[0]'
[ 0.124027] of_get_named_gpiod_flags: parsed 'gpio' property of node '/fixedregulator-mmcwl[0]' - status (0)
[ 0.126991] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/i2c0_pins, deferring probe
[ 0.127050] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/i2c1_pins, deferring probe
[ 0.127165] media: Linux media interface: v0.10
[ 0.127204] Linux video capture interface: v2.00
[ 0.127309] pps_core: LinuxPPS API ver. 1 registered
[ 0.127317] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.127337] PTP clock support registered
[ 0.127370] EDAC MC: Ver: 3.0.0
[ 0.127822] dmi: Firmware registration failed.
[ 0.128176] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.128592] Advanced Linux Sound Architecture Driver Initialized.
[ 0.129700] clocksource: Switched to clocksource timer1
[ 0.137664] NET: Registered protocol family 2
[ 0.138386] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.138470] TCP bind hash table entries: 8192 (order: 5, 196608 bytes)
[ 0.138999] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.139240] UDP hash table entries: 512 (order: 3, 32768 bytes)
[ 0.139362] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
[ 0.139690] NET: Registered protocol family 1
[ 0.140384] RPC: Registered named UNIX socket transport module.
[ 0.140398] RPC: Registered udp transport module.
[ 0.140403] RPC: Registered tcp transport module.
[ 0.140408] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.140420] PCI: CLS 0 bytes, default 64
[ 0.142453] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.146586] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.147421] NFS: Registering the id_resolver key type
[ 0.147458] Key type id_resolver registered
[ 0.147464] Key type id_legacy registered
[ 0.147506] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.149557] bounce: pool size: 64 pages
[ 0.149645] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.149658] io scheduler noop registered
[ 0.149664] io scheduler deadline registered
[ 0.149983] io scheduler cfq registered (default)
[ 0.149996] io scheduler mq-deadline registered
[ 0.150002] io scheduler kyber registered
[ 0.152126] pinctrl-single 44e10800.pinmux: 199 pins at pa f9e10800 size 796
[ 0.155058] pwm-backlight backlight: GPIO lookup for consumer enable
[ 0.155069] pwm-backlight backlight: using device tree for GPIO lookup
[ 0.155082] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]'
[ 0.155088] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]'
[ 0.155093] pwm-backlight backlight: using lookup tables for GPIO lookup
[ 0.155100] pwm-backlight backlight: lookup for GPIO enable failed
[ 0.155120] pwm-backlight backlight: backlight supply power not found, using dummy regulator
[ 0.202149] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.204343] omap8250 44e09000.serial: No clock speed specified: using default: 48000000
[ 0.205033] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
[ 0.943710] console [ttyS0] enabled
[ 0.949214] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 0.956582] omapdss_dss 4832a000.dss: 4832a000.dss supply vdda_video not found, using dummy regulator
[ 0.965994] DSS: OMAP DSS rev 2.0
[ 0.970256] omapdss_dss 4832a000.dss: bound 4832a400.dispc (ops dispc_component_ops)
[ 0.979367] panel-dpi display: GPIO lookup for consumer enable
[ 0.979376] panel-dpi display: using device tree for GPIO lookup
[ 0.979388] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/display[0]'
[ 0.979395] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/display[0]'
[ 0.979399] panel-dpi display: using lookup tables for GPIO lookup
[ 0.979405] panel-dpi display: lookup for GPIO enable failed
[ 0.979411] panel-dpi display: GPIO lookup for consumer reset
[ 0.979414] panel-dpi display: using device tree for GPIO lookup
[ 0.979420] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/display[0]'
[ 0.979424] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/display[0]'
[ 0.979429] panel-dpi display: using lookup tables for GPIO lookup
[ 0.979433] panel-dpi display: lookup for GPIO reset failed
[ 0.979449] panel-dpi display: display supply vcc not found, using dummy regulator
[ 1.000182] brd: module loaded
[ 1.012000] loop: module loaded
[ 1.017842] mdio_bus fixed-0: GPIO lookup for consumer reset
[ 1.017853] mdio_bus fixed-0: using lookup tables for GPIO lookup
[ 1.017859] mdio_bus fixed-0: lookup for GPIO reset failed
[ 1.017880] libphy: Fixed MDIO Bus: probed
[ 1.037713] mdio_bus 4a101000.mdio: GPIO lookup for consumer reset
[ 1.037723] mdio_bus 4a101000.mdio: using lookup tables for GPIO lookup
[ 1.037729] mdio_bus 4a101000.mdio: lookup for GPIO reset failed
[ 1.089776] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.097477] davinci_mdio 4a101000.mdio: detected phy mask ffffffce
[ 1.106462] libphy: 4a101000.mdio: probed
[ 1.110513] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver RTL8211F Gigabit Ethernet
[ 1.120128] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver RTL8211F Gigabit Ethernet
[ 1.129748] davinci_mdio 4a101000.mdio: phy[5]: device 4a101000.mdio:05, driver RTL8211F Gigabit Ethernet
[ 1.140368] cpsw 4a100000.ethernet: Missing dual_emac_res_vlan in DT.
[ 1.146848] cpsw 4a100000.ethernet: Using 1 as Reserved VLAN for 0 slave
[ 1.153642] cpsw 4a100000.ethernet: Missing dual_emac_res_vlan in DT.
[ 1.160116] cpsw 4a100000.ethernet: Using 2 as Reserved VLAN for 1 slave
[ 1.166847] cpsw 4a100000.ethernet: Detected MACID = a8:1b:6a:c9:91:36
[ 1.173496] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.179881] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.185168] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.193082] cpsw 4a100000.ethernet: cpsw: Detected MACID = a8:1b:6a:c9:91:38
[ 1.202352] omap_rtc 44e3e000.rtc: already running
[ 1.207876] omap_rtc 44e3e000.rtc: char device (253:0)
[ 1.207989] omap_rtc 44e3e000.rtc: registered as rtc0
[ 1.213362] i2c /dev entries driver
[ 1.217285] IR NEC protocol handler initialized
[ 1.221840] IR RC5(x/sz) protocol handler initialized
[ 1.226913] IR RC6 protocol handler initialized
[ 1.231460] IR JVC protocol handler initialized
[ 1.236008] IR Sony protocol handler initialized
[ 1.240643] IR SANYO protocol handler initialized
[ 1.245365] IR Sharp protocol handler initialized
[ 1.250087] IR MCE Keyboard/mouse protocol handler initialized
[ 1.255941] IR XMP protocol handler initialized
[ 1.261481] sdhci: Secure Digital Host Controller Interface driver
[ 1.267691] sdhci: Copyright(c) Pierre Ossman
[ 1.272547] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 1.272554] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.272604] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 1.272790] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.282593] NET: Registered protocol family 10
[ 1.288327] Segment Routing with IPv6
[ 1.292097] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.298665] NET: Registered protocol family 17
[ 1.303419] Key type dns_resolver registered
[ 1.307917] omap_voltage_late_init: Voltage driver support not added
[ 1.322538] omapdrm omapdrm.0: DMM not available, disable DMM support
[ 1.329616] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.336280] [drm] No driver support for vblank timestamp query.
[ 1.416888] Console: switching to colour frame buffer device 128x48
[ 1.441106] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 1.447850] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[ 1.455568] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.460748] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.466893] gpiochip_find_base: found new base at 510
[ 1.467170] gpio gpiochip4: (omap-gpmc): added GPIO chardev (254:4)
[ 1.467255] gpiochip_setup_dev: registered GPIOs 510 to 511 on device: gpiochip4 (omap-gpmc)
[ 1.468531] omap2-nand 1000000.nand: GPIO lookup for consumer rb
[ 1.468541] omap2-nand 1000000.nand: using device tree for GPIO lookup
[ 1.468584] of_get_named_gpiod_flags: parsed 'rb-gpios' property of node '/ocp@44000000/gpmc@50000000/nand@0,0[0]' - status (0)
[ 1.468745] nand: device found, Manufacturer ID: 0x01, Chip ID: 0xdc
[ 1.475149] nand: AMD/Spansion S34ML04G2
[ 1.479093] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 128
[ 1.486880] using OMAP_ECC_BCH16_CODE_HW ECC scheme
[ 1.491869] 10 ofpart partitions found on MTD device omap2-nand.0
[ 1.497988] Creating 10 MTD partitions on "omap2-nand.0":
[ 1.503420] 0x000000000000-0x000000040000 : "NAND.SPL"
[ 1.509841] 0x000000040000-0x000000080000 : "NAND.SPL.backup1"
[ 1.516669] 0x000000080000-0x0000000c0000 : "NAND.SPL.backup2"
[ 1.523499] 0x0000000c0000-0x000000100000 : "NAND.SPL.backup3"
[ 1.530428] 0x000000100000-0x000000180000 : "NAND.u-boot-spl-os"
[ 1.537564] 0x000000180000-0x000000280000 : "NAND.u-boot"
[ 1.544390] 0x000000280000-0x0000002c0000 : "NAND.u-boot-env"
[ 1.551130] 0x0000002c0000-0x000000300000 : "NAND.u-boot-env.backup1"
[ 1.558549] 0x000000300000-0x000000a00000 : "NAND.kernel"
[ 1.568633] 0x000000a00000-0x000020000000 : "NAND.file-system"
[ 1.894701] omap_i2c 44e0b000.i2c: bus 0 rev0.12 at 100 kHz
[ 1.901741] omap_i2c 4802a000.i2c: bus 1 rev0.12 at 100 kHz
[ 1.908024] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 1.908031] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.908083] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 1.908510] ubi0: attaching mtd9
[ 3.509794] ubi0: scanning is finished
[ 3.524387] ubi0: attached mtd9 (name "NAND.file-system", size 502 MiB)
[ 3.531058] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[ 3.537964] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512
[ 3.544694] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096
[ 3.551685] ubi0: good PEBs: 4016, bad PEBs: 0, corrupted PEBs: 0
[ 3.557803] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128
[ 3.565057] ubi0: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 873692103
[ 3.574142] ubi0: available PEBs: 0, total reserved PEBs: 4016, PEBs reserved for bad PEB handling: 80
[ 3.583503] ubi0: background thread "ubi_bgt0d" started, PID 68
[ 3.589919] omap_rtc 44e3e000.rtc: setting system clock to 2021-08-05 03:11:09 UTC (1628133069)
[ 3.599319] evm_v3_3d: disabling
[ 3.602579] vmmcwl_fixed: disabling
[ 3.606095] ALSA device list:
[ 3.609070] No soundcards found.
[ 3.619894] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 70
[ 3.644920] UBIFS (ubi0:0): recovery needed
[ 3.854419] UBIFS (ubi0:0): recovery completed
[ 3.860990] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[ 3.868424] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes
[ 3.878387] UBIFS (ubi0:0): FS size: 497872896 bytes (474 MiB, 3921 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs)
[ 3.889132] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB)
[ 3.894993] UBIFS (ubi0:0): media format: w4/r0 (latest is w5/r0), UUID A1DD698B-2F5A-4EC1-AD09-57F394115CB5, small LPT model
[ 3.906894] VFS: Mounted root (ubifs filesystem) on device 0:15.
[ 3.913931] devtmpfs: mounted
[ 3.918765] Freeing unused kernel memory: 1024K
[ 5.049975] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.090104] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.120019] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.635807] cryptodev: loading out-of-tree module taints kernel.
[ 5.643800] cryptodev: driver 1.9 loaded.
[ 8.205712] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 8.206525] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.206530] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.206583] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.210946] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.210952] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.211005] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.240837] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.240844] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.240896] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.242800] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.242806] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.242853] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.275800] remoteproc remoteproc0: wkup_m3 is available
[ 8.276613] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.276619] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.276671] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.401250] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.401256] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.401309] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.401474] remoteproc remoteproc0: powering up wkup_m3
[ 8.558218] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224628
[ 8.559043] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 8.559185] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 8.674857] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@18[0]'
[ 8.692364] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.692370] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.692424] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.850816] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.850822] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.850876] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.861962] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.861968] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.862022] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 8.890631] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 8.890637] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 8.890688] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 9.150286] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 9.150293] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 9.150345] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 9.172417] omap-sham 53100000.sham: hw accel on OMAP rev 0.0
[ 9.252411] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 9.252417] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 9.252469] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 9.252844] omap-aes 53501000.aes: OMAP AES hw accel rev: 0.1
[ 9.262379] omap-aes 53501000.aes: will run requests pump with realtime priority
[ 9.293768] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 9.293774] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 9.293827] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 9.294154] omap-des 53701000.des: OMAP DES hw accel rev: 0.33
[ 9.296562] omap-des 53701000.des: will run requests pump with realtime priority
[ 9.352951] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 9.352957] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 9.353007] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 10.632331] PM: bootloader does not support rtc-only!
[ 10.702122] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 10.702132] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 10.702187] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 10.813100] of_get_named_gpiod_flags: can't parse 'simple-audio-card,hp-det-gpio' property of node '/sound0[0]'
[ 10.813311] of_get_named_gpiod_flags: can't parse 'simple-audio-card,mic-det-gpio' property of node '/sound0[0]'
[ 10.818865] asoc-simple-card sound0: tlv320aic3x-hifi <-> 4803c000.mcasp mapping ok
[ 10.865255] asoc-simple-card sound0: ASoC: no DMI vendor name!
[ 10.942300] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 10.942310] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 10.942364] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 14.595140] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 14.595153] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 14.595204] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 14.600643] input: ti-tsc as /devices/platform/44000000.ocp/44e0d000.tscadc/44e0d000.tscadc:tsc/input/input0
[ 14.678329] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 14.678341] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 14.678392] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 14.690686] pruss 54400000.pruss: creating PRU cores and other child platform devices
[ 14.778700] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 14.778713] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 14.778765] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 14.783777] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 14.783790] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 14.783838] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 14.786931] pruss 54440000.pruss: creating PRU cores and other child platform devices
[ 14.883542] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 14.883548] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 14.883601] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 14.987798] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 14.987811] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 14.987866] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.010997] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.011010] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.011065] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.026259] remoteproc remoteproc1: 54434000.pru is available
[ 15.065164] usbcore: registered new interface driver usbfs
[ 15.065559] usbcore: registered new interface driver hub
[ 15.065984] usbcore: registered new device driver usb
[ 15.156901] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[ 15.156942] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1
[ 15.168177] xhci-hcd xhci-hcd.3.auto: hcc params 0x0238f06d hci version 0x100 quirks 0x02010010
[ 15.171372] xhci-hcd xhci-hcd.3.auto: irq 95, io mem 0x483d0000
[ 15.172062] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 15.172069] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 15.172073] usb usb1: Product: xHCI Host Controller
[ 15.172077] usb usb1: Manufacturer: Linux 4.14.79-rt47-ga72bf1418c xhci-hcd
[ 15.172081] usb usb1: SerialNumber: xhci-hcd.3.auto
[ 15.184899] hub 1-0:1.0: USB hub found
[ 15.185073] hub 1-0:1.0: 1 port detected
[ 15.188814] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.188820] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.188874] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.190323] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.190330] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.190373] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.191009] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[ 15.191031] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 2
[ 15.191050] xhci-hcd xhci-hcd.3.auto: Host supports USB 3.0 SuperSpeed
[ 15.191225] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 15.191364] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[ 15.191372] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 15.191376] usb usb2: Product: xHCI Host Controller
[ 15.191380] usb usb2: Manufacturer: Linux 4.14.79-rt47-ga72bf1418c xhci-hcd
[ 15.191384] usb usb2: SerialNumber: xhci-hcd.3.auto
[ 15.193359] hub 2-0:1.0: USB hub found
[ 15.193423] hub 2-0:1.0: 1 port detected
[ 15.194352] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.194357] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.194407] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.195568] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.195574] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.195613] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.197007] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.197012] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.197057] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.197843] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 15.197877] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 3
[ 15.199270] xhci-hcd xhci-hcd.4.auto: hcc params 0x0238f06d hci version 0x100 quirks 0x02010010
[ 15.204722] xhci-hcd xhci-hcd.4.auto: irq 94, io mem 0x48390000
[ 15.204930] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002
[ 15.204936] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 15.204941] usb usb3: Product: xHCI Host Controller
[ 15.204945] usb usb3: Manufacturer: Linux 4.14.79-rt47-ga72bf1418c xhci-hcd
[ 15.204949] usb usb3: SerialNumber: xhci-hcd.4.auto
[ 15.207648] hub 3-0:1.0: USB hub found
[ 15.210089] hub 3-0:1.0: 1 port detected
[ 15.211434] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.211441] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.211493] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.213319] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.213326] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.213373] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.213975] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 15.213995] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 4
[ 15.214014] xhci-hcd xhci-hcd.4.auto: Host supports USB 3.0 SuperSpeed
[ 15.214844] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ 15.215036] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003
[ 15.215043] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 15.215047] usb usb4: Product: xHCI Host Controller
[ 15.215052] usb usb4: Manufacturer: Linux 4.14.79-rt47-ga72bf1418c xhci-hcd
[ 15.215055] usb usb4: SerialNumber: xhci-hcd.4.auto
[ 15.220706] hub 4-0:1.0: USB hub found
[ 15.220776] hub 4-0:1.0: 1 port detected
[ 15.222190] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.222195] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.222247] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.224512] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.224518] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.224567] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.230150] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.230157] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.230217] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.413511] ts init
[ 15.414015] ts probe...!!
[ 15.414072] of_get_named_gpiod_flags: parsed 'fpga-nDCLK' property of node '/FPGA_Load[0]' - status (0)
[ 15.414154] of_get_named_gpiod_flags: parsed 'fpga-DATA0' property of node '/FPGA_Load[0]' - status (0)
[ 15.414172] of_get_named_gpiod_flags: parsed 'fpga-nCONFIG' property of node '/FPGA_Load[0]' - status (0)
[ 15.414178] gpios request ok
[ 15.414321] virt_membase f6000000.....
[ 15.422396] m_ts load success!
[ 15.430753] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.430759] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.430810] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 15.433145] init success!
[ 15.550007] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 15.730082] usb 1-1: New USB device found, idVendor=0409, idProduct=005a
[ 15.730091] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 15.735516] hub 1-1:1.0: USB hub found
[ 15.736143] hub 1-1:1.0: 4 ports detected
[ 15.738172] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 15.738179] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 15.738231] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.050161] usb 1-1.3: new full-speed USB device number 3 using xhci-hcd
[ 16.124705] pru-rproc 54434000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@0/pru@34000 probed successfully
[ 16.160923] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.160936] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.160992] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.162508] remoteproc remoteproc2: 54438000.pru is available
[ 16.168373] pru-rproc 54438000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@0/pru@38000 probed successfully
[ 16.182535] usb 1-1.3: New USB device found, idVendor=0e6f, idProduct=010c
[ 16.182544] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 16.182549] usb 1-1.3: Product: PDP Audio Device
[ 16.182552] usb 1-1.3: Manufacturer: Performance Designed Products
[ 16.186709] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.186715] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.186766] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.289994] usb 1-1.4: new full-speed USB device number 4 using xhci-hcd
[ 16.386034] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.386045] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.386101] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.387535] remoteproc remoteproc3: 54474000.pru is available
[ 16.398553] pru-rproc 54474000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@40000/pru@74000 probed successfully
[ 16.408424] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.408431] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.408482] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.428669] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.428678] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.428732] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.431199] remoteproc remoteproc4: 54478000.pru is available
[ 16.437081] pru-rproc 54478000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@40000/pru@78000 probed successfully
[ 16.442357] usb 1-1.4: New USB device found, idVendor=0e6f, idProduct=010c
[ 16.442365] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 16.442370] usb 1-1.4: Product: PDP Audio Device
[ 16.442374] usb 1-1.4: Manufacturer: Performance Designed Products
[ 16.472674] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.472680] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.472733] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.484509] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.484516] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.484567] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.511647] Ethernet Channel Bonding Driver: v3.7.1 (April 27, 2011)
[ 16.511674] MII link monitoring set to 100 ms
[ 16.642098] usbcore: registered new interface driver snd-usb-audio
[ 16.647448] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.647455] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.647511] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 16.800569] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 16.800582] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 16.800636] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
[ 17.560950] IPv6: ADDRCONF(NETDEV_UP): bond0: link is not ready
[ 17.729961] net eth0: initializing cpsw version 1.15 (0)
[ 17.871502] RTL8211F Gigabit Ethernet 4a101000.mdio:04: attached PHY driver [RTL8211F Gigabit Ethernet] (mii_bus:phy_addr=4a101000.mdio:04, irq=POLL)
[ 17.906756] bond0: Enslaving eth0 as a backup interface with a down link
[ 17.969908] net eth1: initializing cpsw version 1.15 (0)
[ 18.071480] RTL8211F Gigabit Ethernet 4a101000.mdio:05: attached PHY driver [RTL8211F Gigabit Ethernet] (mii_bus:phy_addr=4a101000.mdio:05, irq=POLL)
[ 18.096516] bond0: Enslaving eth1 as a backup interface with a down link
[ 18.118184] device bond0 entered promiscuous mode
[ 18.122985] device eth0 entered promiscuous mode
[ 18.128732] device eth1 entered promiscuous mode
[ 19.931571] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 19.989855] bond0: link status definitely up for interface eth0, 100 Mbps full duplex
[ 19.997749] bond0: Warning: No 802.3ad response from the link partner for any adapters in the bond
[ 20.011804] bond0: first active interface up!
[ 20.016764] IPv6: ADDRCONF(NETDEV_CHANGE): bond0: link becomes ready
[ 24.174422] input: ts_uinput as /devices/virtual/input/input1
[ 26.621266] ts_open.....................[0]
I find there are many:
omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
Is this the case? but I define the MMC1 in the device tree file(am437x-gp-evm.dts) as shown before.
Best Regards,
Dudechao