Other Parts Discussed in Thread: DP83869, TLK105L, TLK106L
Hi,
We are planning to use the AM6442 processor from the Sitara series in our design which should support 1G Ethernet and the different industrial Ethernet protocols such as Ethernet I/P, Ether CAT, PROFINet etc. I got some documents about this from this link. In these documents, the Ethernet PHY DP83822 is recommended, which is a 10/100 Ethernet PHY, for implementing these protocols. We have purchased the evaluation board for the AM64x series TMDS64GPEVM. The PHY used in that design is DP83869HMRGZT, which supports 1G Ethernet. So, is it possible to implement the above-mentioned protocols using this PHY, or DP83822 is required? Is it possible to test these protocols using the Evaluation board?