HI,I have a problem when I develop the driver of dsp6455 basing PCI bus under Windows XP system。In the step of initialization,I want to enable the interrupt from dsp6455 to host and the interrupt from host to dsp6455.I have looked up the datasheet for dsp6455,the SOFT_INT PCI bit in PCIHINTSET register and the DSPINT bit in PCISTATSET register should be set 1,but I don't know how to access these PCI Back End Configuration Registers from host.
From the datasheet,we know that Back end registers can be programmed both from the PCI host and the DSP. Normally, the PCI host programs a part of back end registers and the DSP programs the remaining part of the registers. I hope you can give me some guidance about accessing the Back end registers from PCI host.
Waiting for your replying,thank you very much!
From xiufenchen
31 May