This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP Active Noise Cancellation Design



Dear all

I'm doing initial research on a design for an active noise cancellation system (ANC). What we want to achieve is a headphone design where we want to cancel out sound from the surrounding environment, hence there is no need to let speech etc. trough, focus is maximum attenuation.

The design will then be an Audio amplifier with integrated ANC. The  pick up microphone (noise) for the ANC will have to be placed in front of amplifier. Headphones is connected via an 5 m long extension cable. Audio source (IN) is preferably digital as this comes via a fiber optic link.

I looked at the development boards available but I did not see that they had the digital interface (S/PDIF, I2S) support. Is there other development boards available?

Second questions, does anyone have experience with what performance one can expect in regards of frequency range of ANC? The noise to be cancelled out is mainly alternating frequencies at high levels  (100+ dB) I have seen that most solutions stop at 500-800 Hz.

  • which device do you plan to use?

    There is an I2S interface on the C5515/C5505 EVM board. For details about this EVM board, please go to following web link. 

    http://support.spectrumdigital.com/boards/evm5515/revb/

     

    Regards

     

    Wen