Team,
A couple of basic questions:
a) there are several modes of operation mentionned in the datasheet - SPRS543B at page 2 like :
H264_ENC_02 , H264_ENC_04 ,etc .The doc gives ID for each mode.
The are these modes actual parameters for the CODECs (ie used directly as parameters to control the CODEC) or is it only references (for examples config used for tests) to the set of parameters mentioned in the configuration tab at page 2?
b) Still in table 1 page 2. What does SM stands for (ie SM – ON )? What parameter does it refer to?
Thanks in advance,
Anthony