Hello,
We are working on AM5728 based custom board and trying to load u-boot and kernel filesystem through eMMC.
The following steps were followed:
1. U-boot and kernel images were compiled and created for custom board
2. Boot Mode is kept at SD-Card, the above-generated images were loaded into SD Card.
3. Board is booting up perfectly and working fine through SD-CARD.
4. eMMc partitions was created successfully for both u-boot (mmc1blk1p1) and kernel ( mmc1blk1p2 )
5. Files for uboot were copied from /run/media/mmc1blk0p1/ to mmc1blk1p1 partition after mounting it.
6. Files for kernel were copied from /run/media/mmc1blk0p2 to mmc1blk1p2 after mounting it properly
7. SD Card was removed and reboot the card.
Following errors are coming while booting from eMMc.
U-Boot SPL 2019.01-g82f62fa-dirty (Aug 09 2021 - 16:52:32 +0530)
DRA752-GP ES2.0
Card did not respond to voltage select!
Firmware loading failed
Size get_effective_memsize = 7f000000 , CONFIG_MAX_MEM_MAPPED = ffffffea80000000 , ram
size = 100000000
Trying to boot from MMC2_2
env_init: Environment FAT init done (ret=-2)
env_init: Environment MMC init done (ret=-2)
Loading Environment from FAT...
*********env_fat_load() ************
Card did not respond to voltage select!
Failed (-5)
Loading Environment from MMC...
*********** env_mmc_load() env_mmc_load***********
*** Warning - bad CRC, using default environment
BAD CRC Failed (-5)
** Partition 1 not valid on device 1 **
spl_register_fat_device: fat register err - -1
spl_load_image_fat_buf: error reading image u-boot.img, err - -1
env_init: Environment FAT init done (ret=-2)
env_init: Environment MMC init done (ret=-2)
Loading Environment from FAT...
*********env_fat_load() ************
Card did not respond to voltage select!
Failed (-5)
Loading Environment from MMC...
*********** env_mmc_load() env_mmc_load***********
*** Warning - bad CRC, using default environment
BAD CRC Failed (-5)
spl: no partition table found
SPL: failed to boot from all boot devices
ERROR ### Please RESET the board ###
Regards
Sahil Kalra