This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: OpenVX single cam basic demo - img size issue

Part Number: TDA4VM

Hi,

I'm currently using the single cam app from the basic demos from vision apps, which seems to use the open VX stuff. I could see image correctly showing on my display with one sensor, and decided to create a new driver for a different sensor.

Both have been tested with TDA3 ISS and are known to be working. Also, capturing the I2C initialization sequence (deser, ser, sensor, stream on) with a logic analyzer looks like everything is ok.

When the app is running I dont see anything showing in display and I get the following messages:

786.111307 s: ISS: Initializing sensor [AR0136] ... Done !!!
read_test_image_raw : Unable to open file /opt/vision_apps/test_data/img_test.raw
app_create_viss : sensor_dcc_id = 136
Invalid DCC size for VISS. Disabling DCC
Invalid DCC size for 2A. Disabling DCC
   786.114923 s:  VX_ZONE_ERROR:[tivxAddKernelVpacMscScaleValidate:612] 'out_img[0]' width should not be larger than the input width
   786.114932 s:  VX_ZONE_ERROR:[tivxAddKernelVpacMscScaleValidate:618] 'out_img[0]' height should not be larger than the input height
   786.114939 s:  VX_ZONE_ERROR:[ownGraphNodeKernelValidate:531] node kernel validate failed for kernel com.ti.hwa.vpac_msc_multi_scale at index 3
   786.114945 s:  VX_ZONE_ERROR:[vxVerifyGraph:1930] Node kernel Validate failed
   786.114951 s:  VX_ZONE_ERROR:[vxVerifyGraph:2098] Graph verify failed
Scaler is enabled

Any idea on what could be happening?

I read registers from DS90UB960 to make sure line length and line count match my settings of 1280x960 pixels (registers 0x73 to 0x76) and they return the expected results.

Thanks,

David