Other Parts Discussed in Thread: AM1707
Hi,
I try to connect Spectrum Digital AM1707 EVM to CCS v.4 using on board JTAG emulator.
When I connect to the device OnTargetConnect( ) GEL script is executed from evmam1707.gel Version 0.61.
The script fails on those lines:
Setup_Psc_All_On( ); // Setup All Power Domains
Enable_ARM();
it never goes out of the infinitive loop:
while( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x1F) !=0x3);
while( (*(unsigned int*)(PSC1_MDSTAT+4 * LPSC_num) & 0x1F) !=0x3);
it looks like PSC0/PSC1 module does not set status bits.
If I ignore the errors, or comment out above lines the status of Device becoming - Connected.
I cam load the application to the target, but I cannot execute, or debug loaded application.
Is there any solution for this problem?
What is the reason for such failures?
Thanks.