This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 ipnc parallel input data format question in VPFE

Dear all:

    I study TMS320 SOC (VPFE) datasheet, it say that the parallel input in VPSS can use "video decoders",

so I want to using two ipnc, client ipnc can revice server ipnc's RTSP streaming and play it on client ipnc's IE browser.

Is it possible?

My step is as follow:

step 1.Setting two ipnc1(client) and ipnc2(server) in LAN (it's OK)

step 2.ipnc1 can recive ethernet packet from ipnc2 (it's OK)

step 3. I can get h.264(or mpeg4) data from ipnc2 which is using live555 openRTSP client (it's OK)

step 4. I want to use ipnc1's h.264 decoder to decode h.264 data from ipnc2 and then input it in VPSS.

 

In step4, I don't know how to do it, can anyone give me some adivse ?

Thanks a lot.