Part Number: PROCESSOR-SDK-J7200
Hi TI
We have a question about the J7200 RTOS SDK CAN related functions.
Currently, we see the can_traffic_generator demo code in the CAN-Ethernet Gateway demo and mcan demo code function in PDK.
These two are build on mcu1_0 (as below pictures). Is it possible to make these two run on mcu2_0 or 2_1?
Or ,is this a specific function that can only be run on a specific core?