Our project has the menu function which is similar to the Digital camera menu.Currently the software osd of the appro's av_capture can't satify with our requirement
I try to use the decode which be built in the dvsdk_2_10_01_18/dvsdk_demos_2_10_00_17/dm365/decode.The function is ok.
But I find it's difficult to port the code to the appro's av_capture code structure.
Can you give some suggestion?