HI!
I designed a new board for omap-l138,nandflash is K9F5608(samsung)。I use CCSV4 (XDS100V2),CODE is nand-writer-03.20.00.14。I download nand-writer.OUT to cpu(ddr),I CAN read K9F5608 ID(EC 75),but can not to write。SO I am not sure ?THE nand-writer .OUT support K9F5608 ?Does anyone use this nandflash (K9F5608)and success write to it? or rewrite the code ?
CCS Printf
Enter the image type (one of "armais" "uboot" "other")
armais
Enter the file Name
d:\ubl-nand.bin
Number of blocks needed for data: 0x1
Attempting to start write in block number 0x1.
Unprotecting blocks 0x1 through 0x1.
Erasing block 0x1 through 0x1.
Writing image data to Block 0x1, Page 0x0
NAND_readPage failed!
Verify failed. Attempting to clear page
Erasing block 0x1 through 0x1.
Attempting to start write in block number 0x2.
Unprotecting blocks 0x2 through 0x2.
Erasing block 0x2 through 0x2.