Part Number: TMDS64GPEVM
Hello E2E,
I could not to find the power source circuit for VDDSHV_SD_IO on schematic of EVM.
Where is the source of VDDSHV_SD_IO? Also, what is it?
Regards,
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The VDDSHV_SD_IO node is sourced by the AM64x CAP_VDDSHV_MMC1 pin, and is the output of an internal dual-voltage (3.3V/ 1.8V) LDO. The voltage level of the LDO is set based on the MMCSD0_POWER_CONTROL register. The MMCSD0_POWER_CONTROL register is managed by the MMC/SD Linux or RTOS drivers.
Regards,
Mike