Hi,all
I want to use spi with dma function
Is the spi dma function vaild?
I find follow configs in dts
Is there any where , can i find the dma number for each spi ?
Best regards
main_spi0: spi@2100000 {
compatible = "ti,am654-mcspi","ti,omap4-mcspi";
reg = <0x0 0x2100000 0x0 0x400>;
interrupts = <GIC_SPI 184 IRQ_TYPE_LEVEL_HIGH>;
#address-cells = <1>;
#size-cells = <0>;
clock-names = "fck";
clocks = <&k3_clks 266 1>;
power-domains = <&k3_pds 266 TI_SCI_PD_EXCLUSIVE>;
//dmas = <&main_udmap 0xc500>, <&main_udmap 0x4500>;
//dma-names = "tx0", "rx0";
};