This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3356: ftps client on AM3356 Linux

Part Number: AM3356

Dear Champs,

My customer wants to connect to FTPS server from AM3356 board and wants to know how they can connect to FTPS server.

I'm curious if they need to install ssl library to connect FTPS server from AM3356 board and if they can use below command in the AM3356 board or should use other command to connect FTPS server.

ftp-ssl <Server IP address or Server Name>

Could you please clarify how FTPS client can be used in AM3356 Linux and which components should be installed?

SW SDK is Processor Linux SDK v6.3.0.

Thanks and Best Regards,

SI.