Other Parts Discussed in Thread: OMAP-L138
The OMAP-L138 datasheet (Figure 6-6) shows OSCVss connected to an external crystal through capacitors. However, the EVM schematic shows this pin connected directly to ground.
Additionally, the footnote in section 5.2 states
"When an external crystal is used oscillator (OSC_VSS, RTC_VSS) ground must be kept separate from other grounds and connected directly to the crystal load capacitor ground. These pins are shorted to VSS on the device itself and should not be connected to VSS on the circuit board. If a crystal is not used and the clock input is driven directly, then the oscillator VSS may be connected to board ground."
Can someone clarify how an external oscillator should be connected, including OSCVss? Is the EVM incorrect and still just happens to work?
Thanks,
David