Hi:
The following are stated in section 1.4.3.2.6, steps 2 and 6 respectively, on page 27 of SPRUGH6 :
2) Set CLR_CNTL = 0 in CGCR1.
6) Set PLL_PWRDN = 0, CLR_CNTL = 1.
However, register CGCR1 of C5504 has no such bit. This was bit 15 on VC5504. Bit 15 on C5504 has to be set to 1, according to SPRUGH6.
All references to CLR_CNTL bit apply to VC5504 and to C5504. Is this correct?
Also, should the PLL be powered down in step 2 before programming multiplier and divider registers, and then powered up in step 6?
Thanks a lot!
Cheers,
Mushtaq