Hi:
Has anyone here successfully make use of dm365's internal voice codec.
The PSP I am using is linux-2.6.32.17-psp03.01.01.38. I found some patches for the voice codec from this page:
https://patchwork.kernel.org/project/linux-davinci/list/?state=*&q=voice (I got it with a filer "voice")
I am not sure which patch works for that PSP, so I applied this one, which seemed to be the latest and verified:
[5/5] DaVinci: DM365: Voice Codec support for the DM365 EVM
[4/5] DaVinci: DM365: Voice codec support for the DM365 SoC
[v2,3/5] ASoC: DaVinci: CQ93VC Voice Codec
[v2,2/5] ASoC: DaVinci: Voice Codec Interface
[v2,1/5] MFD: DaVinci Voice Codec
[v2,3/5] ASoC: DaVinci: CQ93VC Voice Codec
The kernel was compiled and built with no error, and booted up with voice codec recognized:
Advanced Linux Sound Architecture Driver Version 1.0.21.
No device for DAI tlv320aic3x
asoc: CQ93VC <-> davinci-vcif mapping ok
ALSA device list:
#0: DaVinci DM365 EVM (CQ93VC)
But no sound was heard when I took a simple test:
cat chimes.wav > /dev/audio
Any advice on this issue? Thanks.
Kevin