This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6A816x AM389x Unable to boot from SD card

I just started to work with the C6A816x EVM and have been trying to set up the board following  the SDK guide.  I set my system as directed:

Ubuntu 10.4 LTS

Code Sourcery

Serial connection set to 115200 8n1

Connected to the P10 UART

 

I ran the given setup script (${EVSDK}/setup.sh) and it looked like it was going well until it tried to use minicom to set up the board.  Minicom is unable to connect at this step in the process. 

I then tried to boot from an SD card.  I created a SD card using the steps in the SDK Guide calling the script mksdboot.sh.  That finished properly and I plugged the bard into the EVM.  I started up minicom and powered on the board and was unable to see any output from the board.  I tried the same thing with connecting through Hyper Term under Windows and got the same results.

Is there a step that needs to be considered that I have overlooked?