Part Number: TDA4VM
Dear Experts
I have referenced this thread for spi device tree, it is very clear.
but I also have one more need thing to check. (confuse)
about this property
+ main_spi6: spi@2160000 {
+ compatible = "ti,am654-mcspi","ti,omap4-mcspi";
+ reg = <0x0 0x2160000 0x0 0x400>;
+ interrupts = <GIC_SPI 190 IRQ_TYPE_LEVEL_HIGH>;
+ clocks = <&k3_clks 272 1>;
+ power-domains = <&k3_pds 272 TI_SCI_PD_EXCLUSIVE>;
+ #address-cells = <1>;
+ #size-cells = <0>;
+ };
How do I set this SPI parameter for red mark ones as below code?
+ reg = <0x0 0x2160000 0x0 0x400>;
+ interrupts = <GIC_SPI 190 IRQ_TYPE_LEVEL_HIGH>;
+ clocks = <&k3_clks 272 1>;
+ power-domains = <&k3_pds 272 TI_SCI_PD_EXCLUSIVE>;
May you give us full setting about this part for SPI0~SPI7?
Because I have no idea about these numbers
Many Thanks
Gibbs