This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AMIC110: AMIC110 Profinet

Part Number: PROCESSOR-SDK-AMIC110
Other Parts Discussed in Thread: AMIC110

I am integrating Profinet into the AMIC110 processor.  I am using the Molex Profinet stack, using the ThreadX RTOS and NetX TCP/IP stack.   I have the stack functioning with the RTOS and TCP/IP stack where it will respond to DCP requests, and read record records etc...   I was just using the TI switch PRU but I am now trying to start using the Profinet specific PRU.  As soon as I load the Profinet PRU instead of the other one, my device will not become active on the network.   It will not even respond to pings.   

The version of the PRU I am using is profinet_irt_PRU0_bin.h and profinet_irt_PRU1_bin.h with file dates of 1/14/2019.

Is there something specific I have to do to get the stack code to function with the PRU?   

I am not going to be implementing IRT, is this the correct PRU? or is there a different version somewhere?