This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: SDK 8.0 boot up error

Part Number: TDA4VM

Hi all,

I use TDA4VM and SDK 8.0
SDK 8.0 use following files.
ti-processor-sdk-linux-rt-j7-evm-08_00_00_08-Linux-x86-Install.bin
ti-processor-sdk-rtos-j721e-evm-08_00_00_12.tar.gz

I always set following command in uboot.
env default –a –f
saveenv

There are some errors when TDA4VM boot up.
I attach the boot up log in the mail.

Could you give me suggestion?

Best regards

-Jason

U-Boot SPL 2021.01-g53e79d0e89 (Aug 12 2021 - 23:27:19 +0000)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Trying to boot from MMC2
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.5(release):08.00.00.004-dirty
NOTICE:  BL31: Built : 22:19:53, Aug 12 2021

U-Boot SPL 2021.01-g53e79d0e89 (Aug 12 2021 - 22:21:49 +0000)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2


U-Boot 2021.01-g53e79d0e89 (Aug 12 2021 - 22:21:49 +0000)

SoC:   J721E SR1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM:  4 GiB
Flash: 0 Bytes
MMC:   sdhci@4f80000: 0, sdhci@4fb0000: 1
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net:   am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
eth0: ethernet@46000000
Hit any key to stop autoboot:  2  1  0 
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
483 bytes read in 7 ms (67.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
1 bytes read in 7 ms (0 Bytes/s)
Already setup.
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
2555068 bytes read in 115 ms (21.2 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 2555068 bytes: Success!
506776 bytes read in 30 ms (16.1 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 506776 bytes: Success!
Failed to load '/lib/firmware/j7-main-r5f1_0-fw'
Failed to load '/lib/firmware/j7-main-r5f1_1-fw'
1579120 bytes read in 72 ms (20.9 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 1579120 bytes: Success!
1579120 bytes read in 71 ms (21.2 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 1579120 bytes: Success!
10399672 bytes read in 187 ms (53 MiB/s)
Load Remote Processor 8 with data@addr=0x82000000 10399672 bytes: Success!
18092544 bytes read in 757 ms (22.8 MiB/s)
94312 bytes read in 12 ms (7.5 MiB/s)
Failed to load '/boot/k3-j721e-vision-apps.dtbo'
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 000000008fee5000, end 000000008fffffff ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[    0.000000] Linux version 5.10.41-rt39-g0701a5b58c (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT_RT Thu Aug 12 22:23:33 UTC 2021
[    0.000000] Machine model: Texas Instruments K3 J721E SoC
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c66-dma-memory@a6000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c66-memory@a6100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c66-dma-memory@a7000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c66-memory@a7100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c71-dma-memory@a8000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c71-memory@a8100000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008ffffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a8ffffff]
[    0.000000]   node   0: [mem 0x00000000a9000000-0x00000000a9ffffff]
[    0.000000]   node   0: [mem 0x00000000aa000000-0x00000000abbfffff]
[    0.000000]   node   0: [mem 0x00000000abc00000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[    0.000000] On node 0 totalpages: 1048576
[    0.000000]   DMA zone: 8192 pages used for memmap
[    0.000000]   DMA zone: 0 pages reserved
[    0.000000]   DMA zone: 524288 pages, LIFO batch:63
[    0.000000]   Normal zone: 8192 pages used for memmap
[    0.000000]   Normal zone: 524288 pages, LIFO batch:63
[    0.000000] cma: Reserved 24 MiB at 0x00000000fe800000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 18 pages/cpu s34752 r8192 d30784 u73728
[    0.000000] pcpu-alloc: s34752 r8192 d30784 u73728 alloc=18*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1 
[    0.000000] Detected PIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: EL2 vector hardening
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1032192
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),1m(ospi.sysfw),256k(ospi.env.backup),57344k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=a8176d3a-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: mapped [mem 0x00000000fa800000-0x00000000fe800000] (64MB)
[    0.000000] Memory: 3804808K/4194304K available (10560K kernel code, 1156K rwdata, 4092K rodata, 1728K init, 437K bss, 364920K reserved, 24576K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000] rcu: 	RCU priority boosting: priority 1 delay 500 ms.
[    0.000000] rcu: 	RCU_SOFTIRQ processing moved to rcuc kthreads.
[    0.000000] 	No expedited grace period (rcu_normal_after_boot).
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000880030000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880040000
[    0.000000] random: get_random_bytes called from start_kernel+0x330/0x4d8 with crng_init=0
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000000] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008366] Console: colour dummy device 80x25
[    0.012932] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023601] pid_max: default: 32768 minimum: 301
[    0.028358] LSM: Security Framework initializing
[    0.033108] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.040685] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.049495] rcu: Hierarchical SRCU implementation.
[    0.054623] Platform MSI: msi-controller@1820000 domain created
[    0.060857] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.070162] EFI services will not be available.
[    0.074890] smp: Bringing up secondary CPUs ...
[    0.080106] Detected PIPT I-cache on CPU1
[    0.084217] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[    0.091248] GICv3: CPU1: using allocated LPI pending table @0x0000000880050000
[    0.098656] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[    0.105378] smp: Brought up 1 node, 2 CPUs
[    0.109572] SMP: Total of 2 processors activated.
[    0.114380] CPU features: detected: 32-bit EL0 Support
[    0.119633] CPU features: detected: CRC32 instructions
[    0.133249] CPU: All CPU(s) started at EL2
[    0.137445] alternatives: patching kernel code
[    0.142456] devtmpfs: initialized
[    0.151517] KASLR disabled due to lack of seed
[    0.156152] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.166117] futex hash table entries: 512 (order: 4, 65536 bytes, linear)
[    0.173578] pinctrl core: initialized pinctrl subsystem
[    0.179151] DMI not present or invalid.
[    0.183321] NET: Registered protocol family 16
[    0.188562] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.195877] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.203943] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.212277] thermal_sys: Registered thermal governor 'step_wise'
[    0.212535] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.225629] ASID allocator initialised with 65536 entries
[    0.248432] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.255299] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.262158] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.269020] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.276404] cryptd: max_cpu_qlen set to 1000
[    0.282468] k3-chipinfo 43000014.chipid: Family:J721E rev:SR1.0 JTAGID[0x0bb6402f] Detected
[    0.291322] vsys_3v3: supplied by evm_12v0
[    0.295680] vsys_5v0: supplied by evm_12v0
[    0.300323] iommu: Default domain type: Translated 
[    0.305560] SCSI subsystem initialized
[    0.309733] mc: Linux media interface: v0.10
[    0.314114] videodev: Linux video capture interface: v2.00
[    0.319765] pps_core: LinuxPPS API ver. 1 registered
[    0.324844] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.334189] PTP clock support registered
[    0.338218] EDAC MC: Ver: 3.0.0
[    0.341985] FPGA manager framework
[    0.345512] Advanced Linux Sound Architecture Driver Initialized.
[    0.352130] clocksource: Switched to clocksource arch_sys_counter
[    0.358463] VFS: Disk quotas dquot_6.6.0
[    0.362495] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.372419] NET: Registered protocol family 2
[    0.377142] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.385744] tcp_listen_portaddr_hash hash table entries: 2048 (order: 5, 131072 bytes, linear)
[    0.394675] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.402909] TCP bind hash table entries: 32768 (order: 8, 1835008 bytes, linear)
[    0.411632] TCP: Hash tables configured (established 32768 bind 32768)
[    0.418553] UDP hash table entries: 2048 (order: 6, 262144 bytes, linear)
[    0.425747] UDP-Lite hash table entries: 2048 (order: 6, 262144 bytes, linear)
[    0.433472] NET: Registered protocol family 1
[    0.438269] RPC: Registered named UNIX socket transport module.
[    0.444334] RPC: Registered udp transport module.
[    0.449138] RPC: Registered tcp transport module.
[    0.453940] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.460523] PCI: CLS 0 bytes, default 64
[    0.464931] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[    0.475312] Initialise system trusted keyrings
[    0.479951] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[    0.488621] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.494868] NFS: Registering the id_resolver key type
[    0.500109] Key type id_resolver registered
[    0.504391] Key type id_legacy registered
[    0.508516] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.515374] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.523071] 9p: Installing v9fs 9p2000 file system support
[    0.548076] Key type asymmetric registered
[    0.552270] Asymmetric key parser 'x509' registered
[    0.557275] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[    0.564842] io scheduler mq-deadline registered
[    0.569469] io scheduler kyber registered
[    0.574716] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[    0.580937] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[    0.589246] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[    0.595529] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[    0.603486] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.611566] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf)
[    0.619849] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq
[    0.626932] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq
[    0.635622] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs
[    0.648999] brd: module loaded
[    0.656215] loop: module loaded
[    0.659839] megasas: 07.714.04.00-rc1
[    0.664851] libphy: Fixed MDIO Bus: probed
[    0.669574] tun: Universal TUN/TAP device driver, 1.6
[    0.674997] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.681419] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.687492] sky2: driver version 1.30
[    0.691756] VFIO - User Level meta-driver version: 0.3
[    0.697440] i2c /dev entries driver
[    0.701557] sdhci: Secure Digital Host Controller Interface driver
[    0.707880] sdhci: Copyright(c) Pierre Ossman
[    0.712581] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.719004] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.726194] optee: probing for conduit method.
[    0.730764] optee: revision 3.12 (3d47a131)
[    0.731003] optee: initialized driver
[    0.740355] NET: Registered protocol family 17
[    0.744986] 9pnet: Installing 9P2000 support
[    0.749382] Key type dns_resolver registered
[    0.753906] printk: bootconsole [ns16550a0]: printing thread started
[    0.753930] Loading compiled-in X.509 certificates
[    0.759494] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[    0.759587] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[    0.761601] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
[    0.781018] random: fast init done
[    0.807742] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[    0.809436] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz
[    0.809828] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz
[    0.810187] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz
[    0.810946] pca953x 3-0020: supply vcc not found, using dummy regulator
[    0.811008] pca953x 3-0020: using no AI
[    0.832954] pca953x 3-0022: supply vcc not found, using dummy regulator
[    0.833002] pca953x 3-0022: using AI
[    0.833625] gpio-481 (MCASP/TRACE_MUX_S0): hogged as output/low
[    0.833819] gpio-482 (MCASP/TRACE_MUX_S1): hogged as output/high
[    0.834180] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[    0.835070] omap_i2c 2010000.i2c: bus 4 rev0.12 at 400 kHz
[    0.835489] omap_i2c 2020000.i2c: bus 5 rev0.12 at 100 kHz
[    0.836178] pca953x 6-0020: supply vcc not found, using dummy regulator
[    0.836246] pca953x 6-0020: using no AI
[    0.860868] omap_i2c 2030000.i2c: bus 6 rev0.12 at 400 kHz
[    0.861342] omap_i2c 2040000.i2c: bus 7 rev0.12 at 100 kHz
[    0.861695] omap_i2c 2050000.i2c: bus 8 rev0.12 at 100 kHz
[    0.862362] pca953x 9-0020: supply vcc not found, using dummy regulator
[    0.862421] pca953x 9-0020: using no AI
[    0.884780] omap_i2c 2060000.i2c: bus 9 rev0.12 at 400 kHz
[    0.885579] ti-sci-intr bus@100000:bus@28380000:interrupt-controller2: Interrupt Router 137 domain created
[    0.885669] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 131 domain created
[    0.885750] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 213 domain created
[    0.886002] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[    0.898281] cdns-torrent-phy 5050000.serdes: 4 lanes, max bit rate 5.400 Gbps
[    0.898777] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[    0.898796] j721e-pcie 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
[    0.898808] j721e-pcie 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[    0.898817] j721e-pcie 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    1.900786] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[    1.900792] pci_bus 0000:00: root bus resource [bus 00-0f]
[    1.900796] pci_bus 0000:00: root bus resource [io  0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[    1.900799] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[    1.900826] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[    1.900831] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    1.900836] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    1.900861] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xe8 may corrupt adjacent RW1C bits
[    1.900866] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[    1.900879] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x92 may corrupt adjacent RW1C bits
[    1.900886] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xb2 may corrupt adjacent RW1C bits
[    1.900918] pci 0000:00:00.0: supports D1
[    1.900920] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[    1.900924] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x84 may corrupt adjacent RW1C bits
[    1.902488] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    1.902492] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[    1.902497] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[    1.902502] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[    1.903902] pci_bus 0000:01: busn_res: [bus 01-0f] end is updated to 01
[    1.903916] pci 0000:00:00.0: PCI bridge to [bus 01]
[    1.904218] pcieport 0000:00:00.0: PME: Signaling with IRQ 55
[    1.904778] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[    1.904798] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
[    1.904807] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
[    1.904817] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    2.906755] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[    2.906761] pci_bus 0001:00: root bus resource [bus 00-0f]
[    2.906765] pci_bus 0001:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[    2.906767] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[    2.906790] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[    2.906856] pci 0001:00:00.0: supports D1
[    2.906859] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[    2.908407] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    2.909796] pci_bus 0001:01: busn_res: [bus 01-0f] end is updated to 01
[    2.909809] pci 0001:00:00.0: PCI bridge to [bus 01]
[    2.910109] pcieport 0001:00:00.0: PME: Signaling with IRQ 58
[    2.910651] j721e-pcie 2920000.pcie: host bridge /bus@100000/pcie@2920000 ranges:
[    2.910670] j721e-pcie 2920000.pcie:       IO 0x4400001000..0x4400010fff -> 0x0000001000
[    2.910680] j721e-pcie 2920000.pcie:      MEM 0x4400011000..0x4407ffffff -> 0x0000011000
[    2.910689] j721e-pcie 2920000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    3.912659] j721e-pcie 2920000.pcie: PCI0host bridge to bus 0002:00
[    3.912665] pci_bus 0002:00: root bus resource [bus 00-0f]
[    3.922731] printk: console [ttyS2]: printing thread started
[    3.912669] pci_bus 0002:00: root bus resource [io  0x20000-0x2ffff] (bus address [0x1000-0x10fff])
[    3.922738] printk: console [ttyS2] enabled
[    3.922740] printk: bootconsole [ns16550a0] disabled
[    3.943244] printk: bootconsole [ns16550a0]: printing thread stopped
[    3.952594] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 34, base_baud = 3000000) is a 8250
[    3.960194] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 35, base_baud = 3000000) is a 8250
[    3.977767] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
[    3.977775] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
[    3.977778] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
[    3.977781] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
[    3.978630] scsi host0: ufshcd
[    3.997598] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[1, 1], lane[1, 1], pwr[SLOWAUTO_MODE, SLOWAUTO_MODE], rate = 0
[    4.021662] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[3, 3], lane[2, 2], pwr[FAST MODE, FAST MODE], rate = 2
[    4.021694] cdns-ufshcd 4e84000.ufs: ufshcd_find_max_sup_active_icc_level: Regulator capability was not set, actvIccLevel=0
[    4.021871] scsi 0:0:0:49488: Well-known LUN    TOSHIBA  THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[    4.022320] scsi 0:0:0:49476: Well-known LUN    TOSHIBA  THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[    4.022655] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found
[    4.025407] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    4.025417] libphy: 46000f00.mdio: probed
[    4.040948] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    4.041003] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[    4.072779] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[    4.081714] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[    4.082042] mmc1: CQHCI version 5.10
[    4.122933] mmc1: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[    4.151742] vdd_mmc1: supplied by vsys_3v3
[    4.152428] pca953x 4-0020: supply vcc not found, using dummy regulator
[    4.152489] pca953x 4-0020: using no AI
[    4.177134] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[    4.177460] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[    4.177763] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[    4.178063] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[    4.178337] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[    4.181953] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[    4.183836] ti-udma 31150000.dma-controller: Channels: 84 (tchan: 42, rchan: 42, gp-rflow: 16)
[    4.189244] spi-nor spi0.0: mt35xu512aba (65536 Kbytes)
[    4.189262] mtd: 47040000.spi.0: partitioning exceeds flash size, truncating
[    4.189264] mtd: 47040000.spi.0: skipping zero sized partition
[    4.189266] 7 cmdlinepart partitions found on MTD device 47040000.spi.0
[    4.189268] Creating 7 MTD partitions on "47040000.spi.0":
[    4.189271] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    4.189864] 0x000000080000-0x000000280000 : "ospi.tispl"
[    4.190322] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    4.190774] 0x000000680000-0x0000006c0000 : "ospi.env"
[    4.191239] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[    4.191683] 0x0000007c0000-0x000000800000 : "ospi.env.backup"
[    4.192192] 0x000000800000-0x000004000000 : "ospi.rootfs"
[    4.195163] spi-nor spi1.0: mt25qu512a (65536 Kbytes)
[    4.236136] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    4.236144] libphy: 46000f00.mdio: probed
[    4.237373] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    4.237424] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[    4.237939] mmc1: Command Queue Engine enabled
[    4.237947] mmc1: new HS400 MMC card at address 0001
[    4.238372] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    4.238488] mmcblk1: mmc1:0001 S0J56X 14.8 GiB 
[    4.238635] mmcblk1boot0: mmc1:0001 S0J56X partition 1 31.5 MiB
[    4.238753] mmcblk1boot1: mmc1:0001 S0J56X partition 2 31.5 MiB
[    4.238922] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    4.238926] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    4.239051] mmcblk1rpmb: mmc1:0001 S0J56X partition 3 4.00 MiB, chardev (237:0)
[    4.239400] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:0
[    4.245700] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[    4.246076] mmc0: CQHCI version 5.10
[    4.268239] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present!
[    4.268267] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present!
[    4.268298] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[    4.268318] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present!
[    4.272248] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    4.282318] ALSA device list:
[    4.282324]   No soundcards found.
[    5.318131] mmc0: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[    5.318391] Waiting for root device PARTUUID=a8176d3a-02...
[    5.367722] mmc0: new ultra high speed DDR50 SDXC card at address 59b4
[    5.368082] mmcblk0: mmc0:59b4 USDU1 116 GiB 
[    5.369341]  mmcblk0: p1 p2
[    5.713433] EXT4-fs (mmcblk0p2): recovery complete
[    5.714413] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    5.714457] VFS: Mounted root (ext4 filesystem) on device 179:98.
[    5.718366] devtmpfs: mounted
[    5.719178] Freeing unused kernel memory: 1728K
[    5.719264] Run /sbin/init as init process
[    5.869305] systemd[1]: System time before build time, advancing clock.
[    5.909925] NET: Registered protocol family 10
[    5.910447] Segment Routing with IPv6
[    5.924433] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[    5.924626] systemd[1]: Detected architecture arm64.

Welcome to Arago 2020.09!

[    5.968711] systemd[1]: Set hostname to <j7-evm>.
[    6.136950] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock �� /run/docker.sock; please update the unit file accordingly.
[    6.178376] random: systemd: uninitialized urandom read (16 bytes read)
[    6.178486] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[    6.178492] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[    6.180107] systemd[1]: Created slice system-getty.slice.
[  OK  ] Created slice system-getty.slice.
[  OK  ] Created slice system-serial\x2dgetty.slice.
[    6.248219] random: systemd: uninitialized urandom read (16 bytes read)
[    6.249002] systemd[1]: Created slice system-serial\x2dgetty.slice.
[    6.264213] random: systemd: uninitialized urandom read (16 bytes read)
[    6.264858] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Started Dispatch Password �Kts to Console Directory Watch.
[    6.304341] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[    6.320273] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R�Kuests to Wall Directory Watch.
[  OK  ] Reached target Paths.
[    6.352253] systemd[1]: Reached target Paths.
[    6.368205] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[  OK  ] Reached target Slices.
[    6.392192] systemd[1]: Reached target Slices.
[    6.408197] systemd[1]: Reached target Swap.
[  OK  ] Reached target Swap.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    6.436694] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Reached target RPC Port Mapper.[    6.458749] systemd[1]: Reached target RPC Port Mapper.

[  OK  ] Listening on Process Core Dump Socket.
[    6.482308] systemd[1]: Listening on Process Core Dump Socket.
[    6.496357] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on Journal Socket (/dev/log).
[    6.531486] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[    6.531873] systemd[1]: Listening on Journal Socket (/dev/log).
[    6.548484] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    6.584508] systemd[1]: Listening on Network Service Netlink Socket.
[    6.600430] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[  OK  ] Listening on udev Kernel Socket.
[    6.628334] systemd[1]: Listening on udev Kernel Socket.
[    6.646589] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
         Mounting POSIX Message Queue File System..[    6.670504] systemd[1]: Mounting POSIX Message Queue File System...
.
         Mounting Kernel Debug File System...
[    6.698521] systemd[1]: Mounting Kernel Debug File System...
         Mounting Temporary Directory (/tmp)...[    6.714920] systemd[1]: Mounting Temporary Directory (/tmp)...

         Starting Create list of st�Kodes for the curr[    6.742775] systemd[1]: Starting Create list of static device nodes for the current kernel...
ent kernel...
         Starting Start psplash boot splash screen...
[    6.770505] systemd[1]: Starting Start psplash boot splash screen...
[  OK  ] Started Hardware RNG Entropy Gather[    6.792085] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon.
er Daemon.
         Starting RPC Bind...
[    6.818610] systemd[1]: Starting RPC Bind...
         Starting Journal Service...
[    6.828339] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[    6.831222] systemd[1]: Starting Journal Service...
         Starting Load Kernel Modules...
[    6.854666] systemd[1]: Starting Load Kernel Modules...
[    6.871789] systemd[1]: Starting Remount Root and Kernel File Systems...
         Starting Remount Root and Kernel File Systems...
[    6.882365] cryptodev: loading out-of-tree module taints kernel.
         Starting udev Coldplug all Devices...[    6.889378] cryptodev: driver 1.10 loaded.

[    6.904619] systemd[1]: Starting udev Coldplug all Devices...
[  OK  ] Started RPC Bind.[    6.931350] systemd[1]: Started RPC Bind.

[  OK  ] Mounted Huge Pages File System.
[    6.953514] systemd[1]: Mounted Huge Pages File System.
[  OK  ] Mounted POSIX Message Queue File Sy[    6.958110] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
stem.
[    6.974737] systemd[1]: Mounted POSIX Message Queue File System.
[  OK  ] Mounted Kernel Debug File System.
[    7.000566] systemd[1]: Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory (/tmp) systemd[1]: Mounted Temporary Directory (/tmp).
[0m.
[  OK  ] Started Journal Service.
[    7.044635] systemd[1]: Started Journal Service.
[  OK  ] Started Create list of sta�K nodes for the current kernel.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star�Kprogress communication helper.
[  OK  ] Started Load Kernel Modules.
[  OK  ] Started Remount Root and Kernel File Systems.
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
[    7.192506] systemd-journald[200]: Received client request to flush runtime journal.
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Started Flush Journal to Persistent Storage.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started Create Static Device Nodes in /dev.
[  OK  ] Reached target Local File Systems (Pre).
         Mounting /media/ram...
         Mounting /var/volatile...
         Starting udev Kernel Device Manager...
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started udev Kernel Device Manager.
[  OK  ] Started Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Update UTMP about System Boot/Shutdown...
[  OK  ] Started udev Coldplug all Devices.
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Reached target Timers.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API.
[  OK  ] Listening on dropbear.socket.
         Starting Reboot and dump vmcore via kexec...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
[  OK  ] Started Job spooling tools.
[  OK  ] Started Periodic Command Scheduler.
[  OK  ] Started D-Bus System Message Bus.
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
[  OK  ] Started irqbalance daemon.
         Starting Telephony service...
         Starting rc.pvr.service...
         Starting Login Service...
[  OK  ] Started Reboot and dump vmcore via kexec.
[  OK  ] Started IPv6 Packet Filtering Framework.
[  OK  ] Started IPv4 Packet Filtering Framework.
[  OK  ] Reached target Network (Pre).
         Starting Network Service...
[  OK  ] Started Telephony service.
[    8.466125] Bluetooth: Core ver 2.22
[    8.466195] NET: Registered protocol family 31
[    8.466198] Bluetooth: HCI device and connection manager initialized
[    8.466210] Bluetooth: HCI socket layer initialized
[  OK  ] Started Network Service.[    8.466215] Bluetooth: L2CAP socket layer initialized

[    8.466224] Bluetooth: SCO socket layer initialized
         Starting Wait for Network to be Configured...
         Starting Network Name Resolution...
[    8.651137] PVR_K:  299: Read BVNC 22.104.208.318 from HW device registers
[  OK  ] Started Login Service.
[    8.651150] PVR_K:  299: RGX Device registered with BVNC 22.104.208.318
[    8.651701] [drm] Initialized pvr 1.13.5776728 20170530 for 4e20000000.gpu on minor 0
[    8.871337] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node c66-dma-memory@a7000000
[    8.875285] k3-dsp-rproc 4d80800000.dsp: configured DSP for IPC-only mode
[    8.875352] remoteproc remoteproc0: 4d80800000.dsp is available
[    8.875401] remoteproc remoteproc0: attaching to 4d80800000.dsp
[    8.875416] Unable to handle kernel paging request at virtual address ffff800018ffffff
[    8.910523] printk: console [ttyS2]: printing thread stopped
[    8.946730] Mem abort info:
[    8.983539] ov5640 9-003c: supply DOVDD not found, using dummy regulator
[    9.039745]   ESR = 0x96000006
[    9.115481] ov5640 9-003c: supply AVDD not found, using dummy regulator
[    9.211132]   EC = 0x25: DABT (current EL), IL = 32 bits
[    9.216506]   SET = 0, FnV = 0
[    9.219553]   EA = 0, S1PTW = 0
[    9.222696] Data abort info:
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Network.
[    9.240188] random: crng init done
[    9.247258] random: 7 urandom warning(s) missed due to ratelimiting
0;32m  OK  ] Reached target Host and Network Name L[    9.253804]   ISV = 0, ISS = 0x00000006
ookups.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting Enable and configure wl18xx bluetooth stack...
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
         Starting Simple Network Ma�Kent Protocol (SNMP) Daemon....
         Starting Permit User Sessions...
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started Getty on tty1.
[    9.337226]   CM = 0, WnR = 0
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Started Serial Getty on ttyS3.
[  OK  ] Reached target Login Prompts.
         Starting Synchronize System and HW clocks...
[  OK  ] Started Enable and configure wl18xx bluetooth stack.
[  OK  ] Started Load/Save Random Seed.
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[    9.462396] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 1
[    9.470691] tidss 4a00000.dss: [drm] Cannot find any crtc or sizes
[    9.479582] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000082e63000
[    9.515755] fbcon_init: detected unhandled fb_set_par error, error code -16
[    9.529221] Console: switching to colour frame buffer device 240x67
[    9.541783] tidss 4a00000.dss: [drm] fb0: tidssdrmfb frame buffer device
[    9.645822] ov5640 9-003c: supply DVDD not found, using dummy regulator
[    9.705749] CAN device driver interface
[    9.736468] [ffff800018ffffff] pgd=00000008fffff003, p4d=00000008fffff003, pud=00000008ffffe003, pmd=0000000887a27003, pte=0000000000000000
[  OK  ] Started Simple Network Man�Kement Protocol (SNMP) Daemon..
[    9.891420] ov5640 9-003c: ov5640_read_reg: error: reg=300a
[    9.915739] ov5640 9-003c: ov5640_check_chip_id: failed to read chip identifier
[    9.973465] Internal error: Oops: 96000006 [#1] PREEMPT_RT SMP
[    9.979292] Modules linked in: m_can_platform m_can can_dev ti_am335x_tscadc cdns_mhdp8546 pruss sa2ul sha512_generic authenc ov5640(+) v4l2_fwnode snd_soc_pcm3168a_i2c snd_soc_pcm3168a j721e_csi2rx videobuf2_dma_contig videobuf2_memops videobuf2_v4l2 ti_k3_dsp_remoteproc(+) videobuf2_common virtio_rpmsg_bus cdns_dphy pci_endpoint_test pvrsrvkm(O) bluetooth ecdh_generic ecc rfkill cdns3_ti rti_wdt sch_fq_codel rpmsg_kdrv_switch cryptodev(O) ipv6
[   10.018691] CPU: 0 PID: 225 Comm: systemd-udevd Tainted: G           O      5.10.41-rt39-g0701a5b58c #1
[   10.028064] Hardware name: Texas Instruments K3 J721E SoC (DT)
[   10.033880] pstate: 00000005 (nzcv daif -PAN -UAO -TCO BTYPE=--)
[   10.039870] pc : rproc_handle_resources.constprop.0+0x94/0x168
[   10.045699] lr : rproc_boot+0x334/0x670
[   10.049527] sp : ffff8000120437c0
[   10.052826] x29: ffff8000120437c0 x28: ffff80001119e638 
[   10.058121] x27: ffff00087f840fb0 x26: ffffffffffffffff 
[   10.063417] x25: ffff800019000000 x24: ffff800010da1b28 
[   10.068713] x23: ffff000807919038 x22: 0000000000000000 
[   10.074009] x21: ffff80001111bdf8 x20: ffff000807919000 
[   10.079304] x19: 0000000000000000 x18: 0000000000000000 
[   10.084599] x17: 0000000000000001 x16: 0000000000000019 
[   10.089895] x15: ffff00080386d880 x14: ffffffffffffffff 
[   10.095189] x13: ffffffffffffffff x12: ffffffffffffffff 
[   10.100483] x11: ffffffffffffffff x10: ffffffffffffffff 
[   10.105779] x9 : ffffffffffffffff x8 : ffffffffffffffff 
[   10.111073] x7 : ffffffffffffffff x6 : ffff00080652c400 
[   10.116367] x5 : ffff00087f7e7b28 x4 : 0000000000000000 
[   10.121662] x3 : 00000000000000fd x2 : 00000000ffffffff 
[   10.126957] x1 : ffff800019000003 x0 : ffff800019000000 
[   10.132253] Call trace:
[   10.134688]  rproc_handle_resources.constprop.0+0x94/0x168
[   10.140165]  rproc_boot+0x334/0x670
[   10.143642]  rproc_add+0x88/0x168
[   10.146944]  k3_dsp_rproc_probe+0x710/0x850 [ti_k3_dsp_remoteproc]
[   10.153116]  platform_drv_probe+0x54/0xa8
[   10.157116]  really_probe+0xe4/0x3b0
[   10.160678]  driver_probe_device+0x58/0xb8
[   10.164761]  device_driver_attach+0x74/0x80
[   10.168930]  __driver_attach+0x58/0xe0
[   10.172666]  bus_for_each_dev+0x70/0xc0
[   10.176489]  driver_attach+0x24/0x30
[   10.180052]  bus_add_driver+0x14c/0x200
[   10.183873]  driver_register+0x64/0x120
[   10.187695]  __platform_driver_register+0x48/0x58
[   10.192385]  k3_dsp_rproc_driver_init+0x20/0x1000 [ti_k3_dsp_remoteproc]
[   10.199074]  do_one_initcall+0x54/0x1b8
[   10.202901]  do_init_module+0x54/0x208
[   10.206638]  load_module+0x1f60/0x2518
[   10.210372]  __do_sys_finit_module+0xb8/0xf8
[   10.214627]  __arm64_sys_finit_module+0x20/0x30
[   10.219143]  el0_svc_common.constprop.0+0x78/0x1a0
[   10.223922]  do_el0_svc+0x24/0x90
[   10.227226]  el0_svc+0x14/0x20
[   10.230274]  el0_sync_handler+0xb0/0xb8
[   10.234097]  el0_sync+0x180/0x1c0
[   10.237405] Code: 128002b3 912bc021 97ffebee 1400002e (b87a6b20) 
[   10.243484] ---[ end trace 0000000000000002 ]---
[   10.372492] ov5640: probe of 9-003c failed with error -121
[   10.585633] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[   10.612247] platform 41000000.r5f: configured R5F for IPC-only mode
[   10.631844] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[   10.662723] remoteproc remoteproc1: 41000000.r5f is available
[   10.680228] remoteproc remoteproc1: attaching to 41000000.r5f
[   10.738148] platform 41000000.r5f: R5F core initialized in IPC-only mode
[   10.756189]  remoteproc1#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
	autoconf
	bash-dev
	bash
	bc
	binutils
	cifs-utils
	coreutils-stdbuf
	coreutils
	cpio
	cpp-symlinks
	cpp
	dosfstools
	elfutils
	g++-symlinks
	g++
	gawk
	gcc-symlinks
	gcc
	gdb
	gdbs[   10.818432] virtio_rpmsg_bus virtio0: rpmsg host is online
erver
	gettext
	glmark2
	gstreamer1.0-libav-dev
	gstreamer1.0-libav
	gzip
	less
	libasm1
	libbfd
	libdw1
	libelf1
	li[   10.832009] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
bgdbm-compat4
	libgdbm-dev
	libgdbm6
	libgettextlib
	libgett[   10.848276] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
extsrc
	libgmp-dev
	libgmp10
	libgmpxx4
	libidn2-0
	libidn2-dev
	libmpc3
	libmpfr6
	libreadline-dev
	libreadline8
	libunistring-dev
	libunistring2
	m4-dev
	m4
	make
	nettle-dev
	nettle
	parted
	python3-rfc3987
	python3-strict-rfc3339
	tar
	which
	zeromq

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
**[   10.926161]  remoteproc1#vdev0buffer: registered virtio0 (type 7)
*************************************************************
[  OK  ] Started Print notice about GPLv3 packages.
[   11.087906] remoteproc remoteproc1: remote processor 41000000.r5f is now attached
[   11.154129] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
[   11.172646] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[   11.256444] platform 5c00000.r5f: configured R5F for IPC-only mode
[   11.300601] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[   11.350295] remoteproc remoteproc2: 5c00000.r5f is available
[   11.419674] remoteproc remoteproc2: attaching to 5c00000.r5f
[   11.469952] platform 5c00000.r5f: Allocated carveout doesn't fit device address request
[   11.548225] platform 5c00000.r5f: R5F core initialized in IPC-only mode
[   11.601207]  remoteproc2#vdev0buffer: assigned reserved memory node r5f-dma-memory@a2000000
[   11.763007] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
[   11.771529] virtio_rpmsg_bus virtio1: rpmsg host is online
[   11.819663] m_can_platform 40528000.can: m_can device registered (irq=23, version=32)
[   11.831994] m_can_platform 40568000.can: m_can device registered (irq=25, version=32)
[   11.893586]  remoteproc2#vdev0buffer: registered virtio1 (type 7)
[   11.924461] remoteproc remoteproc2: remote processor 5c00000.r5f is now attached
[   12.072183] platform 5d00000.r5f: configured R5F for IPC-only mode
[   12.136332] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[   12.198347] remoteproc remoteproc3: 5d00000.r5f is available
[   12.255706] remoteproc remoteproc3: attaching to 5d00000.r5f
[   12.402387] platform 5d00000.r5f: R5F core initialized in IPC-only mode
[   12.492874] remoteproc remoteproc3: remote processor 5d00000.r5f is now attached
[   12.640312] platform 5e00000.r5f: configured R5F for remoteproc mode
[   12.676771] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000
[   12.702620] remoteproc remoteproc4: 5e00000.r5f is available
[   12.793431] remoteproc remoteproc4: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[   12.806882] remoteproc remoteproc4: powering up 5e00000.r5f
[   12.816173] remoteproc remoteproc4: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[   12.830950] remoteproc remoteproc4: request_firmware failed: -2
[   12.844505] platform 5f00000.r5f: configured R5F for remoteproc mode
[   12.880767] platform 5f00000.r5f: assigned reserved memory node r5f-dma-memory@a5000000
[   12.909091] remoteproc remoteproc5: 5f00000.r5f is available
[   12.923246] remoteproc remoteproc5: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[   12.935074] remoteproc remoteproc5: powering up 5f00000.r5f
[   12.944195] remoteproc remoteproc5: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[   12.960261] remoteproc remoteproc5: request_firmware failed: -2
[  OK  ] Created slice system-systemd\x2dfsck.slice.
[  OK  ] Listening on Load/Save RF �Kitch Status /dev/rfkill Watch.
[   14.040985] usbcore: registered new interface driver usbfs
[   14.104252] usbcore: registered new interface driver hub
[   14.150347] usbcore: registered new device driver usb
[  OK  ] Found device /dev/mmcblk0p1.
[  OK  ] Created slice system-weston.slice.
         Starting File System Check on /dev/mmcblk0p1...
[   14.445041] cdns-csi2rx 4504000.csi-bridge: Probed CSI2RX with 2/4 lanes, 4 streams, external D-PHY
[   14.640234] remoteproc remoteproc6: b034000.pru is available
[   14.726087] remoteproc remoteproc7: b004000.rtu is available
[  OK  ] Started Weston Wayland Compositor.
[  OK  ] Started rc.pvr.service.[   14.782156] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
[   14.872337] remoteproc remoteproc8: b00a000.txpru is available
[   14.982092] remoteproc remoteproc9: b038000.pru is available
[   15.009568] remoteproc remoteproc10: b006000.rtu is available
[   15.020814] remoteproc remoteproc11: b00c000.txpru is available
[   15.084807] remoteproc remoteproc12: b134000.pru is available
[   15.106929] remoteproc remoteproc13: b104000.rtu is available
[   15.124767] remoteproc remoteproc14: b10a000.txpru is available
[   15.182830] remoteproc remoteproc15: b138000.pru is available
[   15.368380] remoteproc remoteproc16: b106000.rtu is available
[   15.409242] remoteproc remoteproc17: b10c000.txpru is available
[   15.585729] PVR_K:  1046: RGX Firmware image 'rgx.fw.22.104.208.318' loaded
[   15.600170] PVR_K:(Error):  1046: RGXGetFWImageAllocSize: FW page size mismatch (expected: 4096, found: 65536) [105]
[   15.624154] PVR_K:(Error):  1046: InitFirmware: RGXGetFWImageAllocSize failed [833]
[   15.631817] PVR_K:(Error):  1046: RGXInit: InitFirmware failed (3) [1366]
[   15.654165] PVR_K:(Error):  1046: RGXInit() failed (PVRSRV_ERROR_INVALID_PARAMS) in PVRSRVCommonDeviceInitialise() [2343]
[   15.680154] PVR_K:(Error):  1046: PVRSRVDeviceFinalise() failed (PVRSRV_ERROR_NOT_INITIALISED) in PVRSRVCommonDeviceInitialise() [2352]
[   15.700600] PVR_K:(Error):  1046: PVRSRVDeviceOpen: Failed to initialise device (PVRSRV_ERROR_NOT_INITIALISED) [461]
[   15.717345] detected fb_set_par error, error code: -16

 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project http://arago-project.org j7-evm ttyS2

Arago 2020.09 j7-evm ttyS2

j7-evm login: [   16.226240] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[   16.272723] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
[   16.288558] xhci-hcd xhci-hcd.2.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000010010
[   16.319365] xhci-hcd xhci-hcd.2.auto: irq 619, io mem 0x06410000
[   16.332937] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[   16.348399] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   16.364142] usb usb1: Product: xHCI Host Controller
[   16.372134] usb usb1: Manufacturer: Linux 5.10.41-rt39-g0701a5b58c xhci-hcd
[   16.388130] usb usb1: SerialNumber: xhci-hcd.2.auto
[   16.396310] hub 1-0:1.0: USB hub found
[   16.404139] hub 1-0:1.0: 1 port detected
[   16.414574] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[   16.424147] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
[   16.432155] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
[   16.444147] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[   16.452270] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[   16.468130] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   16.475337] usb usb2: Product: xHCI Host Controller
[   16.488129] usb usb2: Manufacturer: Linux 5.10.41-rt39-g0701a5b58c xhci-hcd
[   16.495074] usb usb2: SerialNumber: xhci-hcd.2.auto
[   16.504606] hub 2-0:1.0: USB hub found
[   16.508369] hub 2-0:1.0: 1 port detected
[   16.752137] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[   16.912431] usb 1-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00
[   16.924149] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
[   16.931269] usb 1-1: SerialNumber: BE0100597885
[   16.944550] hub 1-1:1.0: USB hub found
[   16.948322] hub 1-1:1.0: 4 ports detected
[   17.244137] usb 1-1.3: new high-speed USB device number 3 using xhci-hcd
[   17.357686] usb 1-1.3: New USB device found, idVendor=058f, idProduct=0510, bcdDevice= 1.00
[   17.368137] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[   17.375430] usb 1-1.3: Product: RUFD 4GB
[   17.388130] usb 1-1.3: Manufacturer: IND
[   17.392037] usb 1-1.3: SerialNumber: R0UPZDF3
[   17.477656] usb-storage 1-1.3:1.0: USB Mass Storage device detected
[   17.500208] scsi host1: usb-storage 1-1.3:1.0
[   17.505805] usbcore: registered new interface driver usb-storage
[   18.528788] scsi 1:0:0:0: Direct-Access     IND      RUFD 4GB         8.07 PQ: 0 ANSI: 2
[   18.541085] sd 1:0:0:0: [sda] 7970816 512-byte logical blocks: (4.08 GB/3.80 GiB)
[   18.551422] sd 1:0:0:0: [sda] Write Protect is off
[   18.560178] sd 1:0:0:0: [sda] Mode Sense: 03 00 00 00
[   18.568359] sd 1:0:0:0: [sda] No Caching mode page found
[   18.576139] sd 1:0:0:0: [sda] Assuming drive cache: write through
[   19.757850]  sda: sda1
[   19.761603] sd 1:0:0:0: [sda] Attached SCSI removable disk
root
Last login: Thu Aug 12 22:10:05 UTC 2021
root@j7-evm:~# cd /opt/vision_apps/
root@j7-evm:/opt/vision_apps# cat uEnv.txt
psdk_setup_file=.psdk_setup
check_psdk_setup=load mmc 1:1 ${loadaddr} ${psdk_setup_file}

# Reset to the default environment
do_psdk_setup=env default -f -a; saveenv

# If not previously configured, then configure the environment and indicate this by writing a file
uenvcmd=if run check_psdk_setup; then echo "Already setup."; else run do_psdk_setup; mw.b ${loadaddr} 0 1; fatwrite mmc 1:1 ${loadaddr} .psdk_setup 1; reset; fi

dorprocboot=1
name_overlays=k3-j721e-vision-apps.dtbo

root@j7-evm:/opt/vision_apps# source ./vision_apps_init.sh 
root@j7-evm:/opt/vision_apps# APP_LOG: ERROR: Unable to map memory @ 0xb2000000 of size 262144 bytes !!!