Hello,
i work with EVM C6474 and i want to use 4 port SRIO as output in the AMC.
the default configuration is Port 0 of each DSP is connected with AMC,but Port 1 of each DSP connected inside the EVM.
I want to redirect port 1 SRIO to AMC ,so i should change the Crows Foot (CF) (capacity of 1 µF and Resistor of 1 ohm )
so this operation is easy or not ?