Other Parts Discussed in Thread: DP83867IR, DP83867E
Hello,
We are experiencing some difficulties when trying to establish Ethernet connection from TDA4x to outside world (PC, router).
So we have a custom board based on a TDA4x SoC where DP83867 ethernet phy is connected to MCU domain cpsw. (Using RGMII)

When we try to use Ethernet from u-boot this is the message we get:

For our Uboot DTS we are using same configuration you did for EVM board where very similar Ethernet Phy is being used. We use DP83867IR and on EVM board its DP83867E.
DTS info related to cpsw:
mcu_cpsw_pins_default: mcu_cpsw_pins_default {
pinctrl-single,pins = <
J721E_WKUP_IOPAD(0x0058, PIN_OUTPUT, 0) /* (B27) MCU_RGMII1_TX_CTL */
J721E_WKUP_IOPAD(0x005c, PIN_INPUT, 0) /* (C25) MCU_RGMII1_RX_CTL */
J721E_WKUP_IOPAD(0x0060, PIN_OUTPUT, 0) /* (A28) MCU_RGMII1_TD3 */
J721E_WKUP_IOPAD(0x0064, PIN_OUTPUT, 0) /* (A27) MCU_RGMII1_TD2 */
J721E_WKUP_IOPAD(0x0068, PIN_OUTPUT, 0) /* (A26) MCU_RGMII1_TD1 */
J721E_WKUP_IOPAD(0x006c, PIN_OUTPUT, 0) /* (B25) MCU_RGMII1_TD0 */
J721E_WKUP_IOPAD(0x0078, PIN_INPUT, 0) /* (A25) MCU_RGMII1_RD3 */
J721E_WKUP_IOPAD(0x007c, PIN_INPUT, 0) /* (D24) MCU_RGMII1_RD2 */
J721E_WKUP_IOPAD(0x0080, PIN_INPUT, 0) /* (A24) MCU_RGMII1_RD1 */
J721E_WKUP_IOPAD(0x0084, PIN_INPUT, 0) /* (B24) MCU_RGMII1_RD0 */
J721E_WKUP_IOPAD(0x0070, PIN_INPUT, 0) /* (B26) MCU_RGMII1_TXC */
J721E_WKUP_IOPAD(0x0074, PIN_INPUT, 0) /* (C24) MCU_RGMII1_RXC */
>;
};
&mcu_cpsw {
pinctrl-names = "default";
pinctrl-0 = <&mcu_cpsw_pins_default &mcu_mdio_pins_default>;
};
&davinci_mdio {
phy0: ethernet-phy@0 {
reg = <0>;
ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
};
};
&cpsw_port1 {
phy-mode = "rgmii-rxid";
phy-handle = <&phy0>;
};
&mcu_cpsw {
reg = <0x0 0x46000000 0x0 0x200000>,
<0x0 0x40f00200 0x0 0x2>;
reg-names = "cpsw_nuss", "mac_efuse";
/delete-property/ ranges;
cpsw-phy-sel@40f04040 {
compatible = "ti,am654-cpsw-phy-sel";
reg= <0x0 0x40f04040 0x0 0x4>;
reg-names = "gmii-sel";
};
};
We are trying different RX and TX skew parameters where on EVM this is ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS> but no success.
Any help would be appreciated regarding this issue, we can also provide register values from PHY with mii dump command in uboot if necessary.
Best regards,
Ogi