Other Parts Discussed in Thread: AM1802
I'm looking at the Am1802 SDRAM interface on EMIFA and not clear on a couple items. We are currently working with an Atmel AT91SAM9260 which has a 32bit SDRAM data bus which we use to connect (2) 256MBit x 16 SDRAMs for a total of 256MBit x 32 memory. The SDRAM bus is running at 100MHz. My goal is a similar setup with an AM1802.
- EMIF is only 16 bits - does this mean I will have half the performance of an equivalent bus speed 32-bit (2 chip) system such as our current system?
- How would one use (2) SDRAM x16 parts to get to 512Mbit? I have only found one SDRAM CS (CS0) and single chip diagrams.
- Presumably one 512Mbitx16 is an option, but very costly with few available chips.
Thanks
christopher