Part Number: AM6442
Other Parts Discussed in Thread: SYSCONFIG
Hello TI supporter,
I have AM64xx-evm.
I use the TI SysConfig tool to generate the PIN MUX source as below:
&main_pmx0 {
myuart3_pins_default: myuart3_pins_default {
pinctrl-single,pins = <
AM64x_IOPAD(0x0248, PIN_INPUT, 4) /* (D16) UART1_CTSn.UART3_RXD */
AM64x_IOPAD(0x024c, PIN_OUTPUT, 4) /* (E16) UART1_RTSn.UART3_TXD */
>;
};
};
the function AM64x_IOPAD in Linux devicetree.dts is the leter "x" is upper-cased
so that, It must be AM64X_IOPAD
Thanks