Part Number: TDA4VM
Hello, there.
I use PSDK RTOS and PSDK QNX. And I added my TIOVX custom kernels to ${PSDK_RTOS_PATH}/vision_apps/kernels using PyTIOVX as follows:
from tiovx import *
code = KernelExportCode("my_custom_kernel", "r5f", "CUSTOM_APPLICATION_PATH")
code.setCoreDirectory("r5f")
kernel = Kernel("my_custom_kernel")
kernel.setParameter(Type.USER_DATA_OBJECT, Direction.INPUT, ParamState.REQUIRED, "configuration", ['my_custom_kernel_input_t'])
kernel.setParameter(Type.USER_DATA_OBJECT, Direction.OUTPUT, ParamState.REQUIRED, "recognition_result", ['my_custom_kernel_output_t'])
kernel.setTarget(Target.IPU2)
code.export(kernel)
How can I increase available malloc size in TIOVX User Kernels (R5F)?
I already tried the following two ways, but both failed.
1. Modify ${PSDK_RTOS}/vision_apps/apps/basic_demos/app_tirtos/bios_cfg/bios_common.cfg.
a) Modify: Memory.defaultHeapSize = 10*768*1024; (origin: 768*1024)
b) Build -> Build error
"/home/user/ti-processor-sdk-rtos-j721e-evm-07_01_00_11/vision_apps/apps/basic_demos/app_tirtos/tirtos_qnx/mcu3_0/linker.cmd", line 23: error:
program will not fit into available memory, or the section contains a call
site that requires a trampoline that can't be generated for this section.
run placement with alignment fails for section ".bss" size 0xb07448.
Available memory ranges:
DDR_MCU3_0 size: 0x6ffc00 unused: 0x5470c0 max hole: 0x545400
error: errors encountered during linking;
"/home/user/ti-processor-sdk-rtos-j721e-evm-07_01_00_11/vision_apps/out/J7/R5F/SYSBIOS/release/vx_app_tirtos_qnx_mcu3_0.out" not built
concerto/finale.mak:208: recipe for target '/home/user/ti-processor-sdk-rtos-j721e-evm-07_01_00_11/vision_apps/out/J7/R5F/SYSBIOS/release/vx_app_tirtos_qnx_mcu3_0.out' failed
2. Modify ${PSDK_RTOS}/vision_apps/apps/basic_demos/app_tirtos/tirtos_qnx/gen_linker_mem_map.py.
a) Modify: mcu3_0_ddr_local_heap_size = 16*MB; (origin: 2MB)
b) Run: gen_linker_mem_map.py
c) Build
d) It didn't work. Still available around 670KB.
Please answer about my question.