Question: Is version 0.6.0 of the Jacinto7 DDRSS Register Configuration Tool compatible with older SDKs (prior to SDK8.0)?
Answer: Yes, version 0.6.0 of the Jacinto7 DDRSS Register Configuration Tool is backwards compatible with older SDKs. However, version 0.6.0 or later must be used with SDK8.0 or later. This requirement is because a new parameter was introduced in v0.6.0 of the XLS tool that is utilized by the DDR driver included in SDK8.0. If using version 0.6.0 of the tool with older SDKs, the new parameter will not be used. If using version 0.5.0 or earlier of the tool with SDK8.0, then the source code will not compile due to the missing parameter in the output file of the tool.
Note: Default inputs may change between revisions of the Jacinto7 DDRSS Register Configuration tool. If experiencing issues where v0.6.0 does not work on a custom PCB design using TDA4VM and v0.5.0 of the tool does work, please first verify that the inputs into the tool match exactly. If still experiencing issues, please contact TI for further assistance.