This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: DDR section of IBIS model does not have required inputs.

Part Number: 66AK2G12

Is there any other IBIS model for 66AK2G12 processor for DDR3L.

  • Currently I am referring to IBIS model within sprm705.zip (https://www.ti.com/lit/zip/sprm705)

    The Data Models have not  defined Receiver Threshold section  (AC and DC thresholds) as well as Vmeas.

  • Pl refer the section with details on each specific model. For e.g. for the below model I have highlighted the portion where this information is located.

    regards,

    -Shriram

    |************************************************************************
    | Model PDDRIO_D3FP3L_34
    |************************************************************************
    |
    [Model] PDDRIO_D3FP3L_34
    |
    Model_type I/O
    |
    Polarity Non-Inverting
    |
    Enable Active-High
    |
    C_comp 3.244pF 3.179pF 3.327pF
    C_comp_pullup 525.014fF 499.307fF 553.259fF
    C_comp_pulldown 2.714pF 2.675pF 2.768pF
    |
    Vinh = 810.000mV
    Vinl = 540.000mV
    |
    Vmeas = 675.000mV
    |
    Vref = 675.000mV
    |
    Rref = 50Ohms
    |
    Cref = 0pF

    [Model Spec]
    |
    Vinh 810.000mV 777.000mV 860.000mV
    Vinl 540.000mV 507.000mV 590.000mV
    |
    Vmeas 675.000mV 642.000mV 725.000mV
    |
    Vref 675.000mV 642.000mV 725.000mV