Hi,
We are using the DM6446 EVM with our own drivers and middle ware support for the TI EMAC ethernet controller. While testing for maximum TCP throughput, we have encountered a problem where out throughout drops to a very low value after a certain amount of time. Our tests run fine for almost 10 minutes on average with reasonable throughput (around 60 Mbps) but then the throughput suddenly drops down to less than 1 Mbps. We have spent quite a lot of time finding out the cause of the problem and just want to know whether this issue has something to do with hardware and has been observed before on Linux or some other platform?
Regards,
Awais