This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: QT GUI application in latest SDK

Part Number: AM3358


Hello Team,

I have some custom boards of AM3358 and they are working fine with SDKs up-to ti-processor-sdk-linux-am335x-evm-06.03.00.106.

Recently I have downloaded the latest version ti-processor-sdk-linux-am335x-evm-07.03.00.005 and started using it. I found that my QT GUI applications are not running and throwing errors related to Wayland etc.

Are there any major changes between these two SDKs with respect to WAyland, PVR ?

Kindly help me in full migration from 06.03.00.106 to 07.03.00.005 where I could be able to run my QT GUI Applications.

The main reason for my up-gradation from stable 06.03.00.106 to unknown 07.03.00.005  is that 07.03.00.005 has progress bar update in the psplash which is one the major and pending requirements for me.

Regards

Mad_hu