This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: NDK EMAC RxCRCErros e RxAlignCodeErros errors

Part Number: AM4378


What could cause EMAC RxCRCErros e RxAlignCodeErros errors?

These errors appear once in a while when we perform load tests.

The tests consists in sending and receiving a short message every 25ms, which is not high.

The network configuration is 100Mbps full duplex.

The pdk version in 1_0_10.

Thanks in advance.