Other Parts Discussed in Thread: OMAP-L138
My customer ran into a problem with the TI OMAP-L138 development system. They are trying to install v4.2.0 from a DVD supplied with the TI OMAP-L138 development system and can’t get code composer program to install on their system. It gets about ¾ through the install then it seems to just hang there until end the task, which windows says is “not responding”.
Their PC has 1.95GB of RAM, 2.26 GHz processor, and 100GB of free disk space so it doesnt seem to be a memory problem. And they see the same issue on multiple PCs. They are running on XP pro SP3.
I had them zip the whole InstallJammer Registry directory and can send it if that helps.
thanks,
Lynne