Part Number: SK-AM64
Just beginning development with the SK-AM64. Got by the "smart" USB-C power supply and cable hurdle and now the board is powering up with the correct LEDs lit.
Followed all the Quick Start and User Guide instructions. Created an SD using the latest linux downloads. Used Balena Etcher to create a 64 GB SD. (Using a Sandisk Ultra SDXC). Balena Etcher flashed the SD and verified it without error. I've tried both the LINUX and LINUX-RT downloads with the same result. SW2 and SW3 are set as described in the guides.
I have connectivity on the UART port. The Output is:
U-Boot SPL 2021.01-g53e79d0e89 (Aug 10 2021 - 21:47:42 +0000)
EEPROM not available at 80, trying to read at 81
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
SPL initial stack usage: 13392 bytes
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.5(release):08.00.00.004-dirty
NOTICE: BL31: Built : 21:46:29, Aug 10 2021
U-Boot SPL 2021.01-g53e79d0e89 (Aug 10 2021 - 21:47:02 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Trying to boot from MMC2
Error reading cluster
** Unable to read file u-boot.img **
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
Did I miss a step?? I verified that the SD contains the U-Boot image. Why its it trying to boot from MMC2? I'll keep looking for an answer.
Thanks in advance,
dave