We are trying to set shared memory between the C6472 cores.
One issue that is coming up, is the cashing of the SL2RAM
memory.
in Bios5, the L2CFG mode is set to "0k" i.e. the
size of the L2 cash is set to 0.
But when I read and write to the SL2RAM [ base = 0x002BF000,
length = 0x1000], I can clearly see that the memory is being cashed.
My question:
How can I disable the cashing of the SL2RAM all together so
I don't have to invalidate the cash lines every time.
khaled.