This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: ENABLE_ETHFW will affect MCAN

Genius 13655 points
Part Number: TDA4VM


Hello Champs,

HW: smart car driving system with tda4
SW: SDK7.3.0.

After enabling ENABLE_ETHFW, it will affect the sending of MCAN, causing the MCAN of the MAIN domain to fail to send messages. When ENABLE_ETHFW is not enabled, the MCAN transmission of the MAIN domain is normal, and the display effect is as shown below. 


this is the new one ,but I disable ENABLE_ETHFW,the CAN can send messge!



Thanks.
Rgds
Shine