Part Number: TMDS64GPEVM
Our customer is using processor SDK Linux 08.00.00.21 and sometimes fails to mount the root file system on SD card boot.
Attached are the logs for success and failure:
In case of success:
U-Boot SPL 2021.01 (Aug 27 2021 - 04:35:24 +0900)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
SPL initial stack usage: 13392 bytes
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.5(release):08.00.00.004-dirty
NOTICE: BL31: Built : 21:46:29, Aug 10 2021
U-Boot SPL 2021.01 (Aug 27 2021 - 04:38:29 +0900)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Trying to boot from MMC2
U-Boot 2021.01 (Aug 27 2021 - 04:38:29 +0900)
SoC: AM64X SR1.0
Model: Texas Instruments AM642 EVM
Board: AM64-GPEVM rev A
DRAM: 2 GiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Net: eth0: ethernet@8000000
Hit any key to stop autoboot: 0
## Error: "boot_rprocs" not defined
19137024 bytes read in 797 ms (22.9 MiB/s)
53223 bytes read in 5 ms (10.2 MiB/s)
Moving Image from 0x80080000 to 0x80200000, end=81550000
## Flattened Device Tree blob at 82000000
Booting using the fdt blob at 0x82000000
Loading Device Tree to 000000008feef000, end 000000008fffffff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.41-ti-am6442evm-g4c2eade9f7 (user01@ubuntu) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Sat Aug 21 05:47:01 JST 2021
[ 0.000000] Machine model: Texas Instruments AM642 EVM
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a3ffffff]
[ 0.000000] node 0: [mem 0x00000000a4000000-0x00000000a4ffffff]
[ 0.000000] node 0: [mem 0x00000000a5000000-0x00000000a57fffff]
[ 0.000000] node 0: [mem 0x00000000a5800000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 2 pages/cpu s49880 r8192 d73000 u131072
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Built 1 zonelists, mobility grouping off. Total pages: 32736
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16500a,mmio32,0x02800000 mtdparts=fc40000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern) root=/dev/mmcblk1p5 rw roottypefs=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 262144 (order: 5, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 4, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1448832K/2097152K available (10816K kernel code, 1344K rwdata, 4288K rodata, 1856K init, 758K bss, 124032K reserved, 524288K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @a4000000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000000a58c0000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000000a58d0000
[ 0.000000] random: get_random_bytes called from start_kernel+0x32c/0x4d4 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000004] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.000318] Console: colour dummy device 80x25
[ 0.000378] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.000395] pid_max: default: 32768 minimum: 301
[ 0.000484] LSM: Security Framework initializing
[ 0.000579] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.000619] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.002959] rcu: Hierarchical SRCU implementation.
[ 0.003257] Platform MSI: msi-controller@1820000 domain created
[ 0.003543] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.003660] EFI services will not be available.
[ 0.004108] smp: Bringing up secondary CPUs ...
[ 0.004859] Detected VIPT I-cache on CPU1
[ 0.004898] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
[ 0.004912] GICv3: CPU1: using allocated LPI pending table @0x00000000a58e0000
[ 0.004978] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.005111] smp: Brought up 1 node, 2 CPUs
[ 0.005133] SMP: Total of 2 processors activated.
[ 0.005143] CPU features: detected: 32-bit EL0 Support
[ 0.005152] CPU features: detected: CRC32 instructions
[ 0.013235] CPU: All CPU(s) started at EL2
[ 0.013265] alternatives: patching kernel code
[ 0.014492] devtmpfs: initialized
[ 0.022513] KASLR disabled due to lack of seed
[ 0.022803] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.022821] futex hash table entries: 512 (order: -1, 32768 bytes, linear)
[ 0.024951] pinctrl core: initialized pinctrl subsystem
[ 0.025562] DMI not present or invalid.
[ 0.026244] NET: Registered protocol family 16
[ 0.034053] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.034527] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.034638] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.035278] thermal_sys: Registered thermal governor 'step_wise'
[ 0.035285] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.035797] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.035904] ASID allocator initialised with 65536 entries
[ 0.064451] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages
[ 0.064472] HugeTLB registered 512 MiB page size, pre-allocated 0 pages
[ 0.064480] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.066448] cryptd: max_cpu_qlen set to 1000
[ 0.070218] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR1.0 JTAGID[0x0bb3802f] Detected
[ 0.070848] vsys_5v0: supplied by evm_12v0
[ 0.071174] vsys_3v3: supplied by evm_12v0
[ 0.071557] vddb_3v3_display: supplied by vsys_3v3
[ 0.072594] iommu: Default domain type: Translated
[ 0.073043] SCSI subsystem initialized
[ 0.073780] mc: Linux media interface: v0.10
[ 0.073816] videodev: Linux video capture interface: v2.00
[ 0.073912] pps_core: LinuxPPS API ver. 1 registered
[ 0.073919] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.073938] PTP clock support registered
[ 0.073977] EDAC MC: Ver: 3.0.0
[ 0.074813] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[ 0.075022] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
[ 0.075155] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
[ 0.075926] FPGA manager framework
[ 0.076038] Advanced Linux Sound Architecture Driver Initialized.
[ 0.077256] clocksource: Switched to clocksource arch_sys_counter
[ 0.077762] VFS: Disk quotas dquot_6.6.0
[ 0.077877] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes)
[ 0.084150] NET: Registered protocol family 2
[ 0.084399] IP idents hash table entries: 32768 (order: 2, 262144 bytes, linear)
[ 0.085909] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear)
[ 0.086017] TCP established hash table entries: 16384 (order: 1, 131072 bytes, linear)
[ 0.086145] TCP bind hash table entries: 16384 (order: 2, 262144 bytes, linear)
[ 0.086377] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.086560] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.086658] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.086903] NET: Registered protocol family 1
[ 0.087549] RPC: Registered named UNIX socket transport module.
[ 0.087565] RPC: Registered udp transport module.
[ 0.087571] RPC: Registered tcp transport module.
[ 0.087578] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.087595] PCI: CLS 0 bytes, default 64
[ 0.088394] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.093126] Initialise system trusted keyrings
[ 0.093458] workingset: timestamp_bits=46 max_order=15 bucket_order=0
[ 0.098469] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.099189] NFS: Registering the id_resolver key type
[ 0.099231] Key type id_resolver registered
[ 0.099237] Key type id_legacy registered
[ 0.099311] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.099320] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.099544] 9p: Installing v9fs 9p2000 file system support
[ 0.144106] Key type asymmetric registered
[ 0.144131] Asymmetric key parser 'x509' registered
[ 0.144200] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.144211] io scheduler mq-deadline registered
[ 0.144218] io scheduler kyber registered
[ 0.146820] pinctrl-single f4000.pinctrl: 180 pins, size 720
[ 0.147921] pinctrl-single a40000.timesync-router: 512 pins, size 2048
[ 0.157612] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.174353] brd: module loaded
[ 0.182522] loop: module loaded
[ 0.183341] megasas: 07.714.04.00-rc1
[ 0.186349] libphy: Fixed MDIO Bus: probed
[ 0.187786] tun: Universal TUN/TAP device driver, 1.6
[ 0.188524] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.188534] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.188588] sky2: driver version 1.30
[ 0.189897] VFIO - User Level meta-driver version: 0.3
[ 0.190979] i2c /dev entries driver
[ 0.192111] sdhci: Secure Digital Host Controller Interface driver
[ 0.192121] sdhci: Copyright(c) Pierre Ossman
[ 0.192474] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.193751] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.194179] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.195497] optee: probing for conduit method.
[ 0.195538] optee: revision 3.12 (3d47a131)
[ 0.196169] optee: initialized driver
[ 0.198725] NET: Registered protocol family 17
[ 0.198891] 9pnet: Installing 9P2000 support
[ 0.198959] Key type dns_resolver registered
[ 0.199203] Loading compiled-in X.509 certificates
[ 0.213431] ti-sci 44043000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
[ 0.247192] random: fast init done
[ 0.251888] omap_i2c 20000000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.253925] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 0.254074] pca953x 1-0022: using AI
[ 0.306886] Console: switching to mono frame buffer device 12x2
[ 0.335683] ssd1307fb 1-003c: fb0: Solomon SSD1307 framebuffer device registered, using 192 bytes of video memory
[ 0.335915] omap_i2c 20010000.i2c: bus 1 rev0.12 at 400 kHz
[ 0.337158] omap_i2c 20020000.i2c: bus 2 rev0.12 at 100 kHz
[ 0.338344] omap_i2c 20030000.i2c: bus 3 rev0.12 at 100 kHz
[ 0.338739] ti-sci-intr bus@f4000:bus@4000000:interrupt-controller1: Interrupt Router 5 domain created
[ 0.338890] ti-sci-intr bus@f4000:interrupt-controller0: Interrupt Router 3 domain created
[ 0.339131] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 0.349514] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[ 0.349572] j721e-pcie f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000
[ 0.349596] j721e-pcie f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000
[ 0.349620] j721e-pcie f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[ 1.362101] j721e-pcie f102000.pcie: PCI host bridge to bus 0000:00
[ 1.362122] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.362133] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x68001000-0x68010fff])
[ 1.362142] pci_bus 0000:00: root bus resource [mem 0x68011000-0x6fffffff]
[ 1.362194] pci 0000:00:00.0: [104c:b010] type 01 class 0x060400
[ 1.362217] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0xfffffffff 64bit pref]
[ 1.362306] pci 0000:00:00.0: supports D1
[ 1.362315] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 1.364932] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 1.367346] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[ 1.367391] pci 0000:00:00.0: BAR 0: no space for [mem size 0x1000000000 64bit pref]
[ 1.367400] pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x1000000000 64bit pref]
[ 1.367412] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.367972] pcieport 0000:00:00.0: PME: Signaling with IRQ 42
[ 1.368761] ti-bcdma 485c0100.dma-controller: Number of rings: 68
[ 1.370119] ti-bcdma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
[ 1.371965] ti-pktdma 485c0000.dma-controller: Number of rings: 288
[ 1.379456] ti-pktdma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
[ 1.383023] printk: console [ttyS2] disabled
[ 1.383114] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 16, base_baud = 3000000) is a 8250
[ 2.774086] printk: console [ttyS2] enabled
[ 2.781751] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[ 2.786799] 7 cmdlinepart partitions found on MTD device fc40000.spi.0
[ 2.793319] Creating 7 MTD partitions on "fc40000.spi.0":
[ 2.798716] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 2.805655] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 2.812269] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 2.818941] 0x000000680000-0x0000006c0000 : "ospi.env"
[ 2.825451] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[ 2.832390] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[ 2.839033] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[ 2.901266] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.908865] libphy: 8000f00.mdio: probed
[ 2.915044] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[ 2.923286] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000002
[ 2.936553] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
[ 2.943327] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
[ 2.950474] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 2.957050] pps pps0: new PPS source ptp0
[ 2.961481] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[ 2.973992] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[ 2.984040] mmc0: CQHCI version 5.10
[ 2.985451] gpio-mux mux-controller: 2-way mux-controller registered
[ 3.002303] vdd_mmc1: supplied by vsys_3v3
[ 3.007562] libphy: mdio_mux: probed
[ 3.019632] mmc1: CQHCI version 5.10
[ 3.019789] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present!
[ 3.030651] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 3.043502] ALSA device list:
[ 3.046489] No soundcards found.
[ 3.069868] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 3.078159] Waiting for root device /dev/mmcblk1p5...
[ 3.131037] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.137789] mmc0: Command Queue Engine enabled
[ 3.142241] mmc0: new HS400 MMC card at address 0001
[ 3.148143] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[ 3.149782] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[ 3.150002] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[ 3.150231] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[ 3.150487] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (237:0)
[ 3.156084] mmcblk1: p1 p2 p3 p4 < p5 >
[ 3.207029] EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: (null)
[ 3.215267] VFS: Mounted root (ext4 filesystem) on device 179:5.
[ 3.227144] devtmpfs: mounted
[ 3.231103] Freeing unused kernel memory: 1856K
[ 3.235675] Run /sbin/init as init process
[ 3.492498] systemd[1]: System time before build time, advancing clock.
[ 3.567393] NET: Registered protocol family 10
[ 3.573200] Segment Routing with IPv6
[ 3.599689] systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
[ 3.626091] systemd[1]: Detected architecture arm64.
Welcome to Debian GNU/Linux 10 (buster)!
[ 3.673027] systemd[1]: Set hostname to <am6442evm>.
[ 4.043272] systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[ 4.060346] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[ 4.303299] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.319384] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.326447] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 4.349463] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.359267] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 4.382423] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.402802] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.418055] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password �cts to Console Directory Watch.
[ OK ] Created slice User and Session Slice.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Listening on udev Kernel Socket.
[ OK ] Listening on Syslog Socket.
Starting Journal Service...
Starting Create list of re�codes for the current kernel...
Mounting POSIX Message Queue File System...
Mounting Huge Pages File System...
Starting Set the console keyboard layout...
[ OK ] Listening on udev Control Socket.
Starting udev Coldplug all Devices...
[ OK ] Listening on fsck to fsckd communication Socket.
Starting Remount Root and Kernel File Systems...
[ OK ] Reached target Remote File Systems.
[ OK ] Reached target Slices.
[ OK ] Created slice system-getty.slice.
Starting Load Kernel Modules...
[ OK ] Started Forward Password R�cuests to Wall Directory Watch.
[ 4.798214] EXT4-fs (mmcblk1p5): re-mounted. Opts: errors=remount-ro
[ OK ] Reached target Paths.
[ OK ] Reached target Local Encrypted Volumes.
[ OK ] Started Journal Service.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Started Create list of req�c nodes for the current kernel.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Huge Pages File System.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Load Kernel Modules.
Mounting Kernel Configuration File System...
Starting Apply Kernel Variables...
Starting Create System Users...
Starting Load/Save Random Seed...
Starting Flush Journal to Persistent Storage...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Started Load/Save Random Seed.
[ 5.326078] systemd-journald[147]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create Static Device Nodes in /dev.
Starting udev Kernel Device Manager...
[ OK ] Started Set the console keyboard layout.
[ OK ] Reached target Local File Systems (Pre).
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
Starting Set console font and keymap...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Set console font and keymap.
[ OK ] Started Create Volatile Files and Directories.
[ OK ] Started udev Coldplug all Devices.
Starting Helper to synchronize boot up for ifupdown...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Helper to synchronize boot up for ifupdown.
Starting Raise network interfaces...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Raise network interfaces.
[ OK ] Reached target Network.
[ OK ] Reached target Network is Online.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ 6.272144] 93xx46 spi1.0: 16-bit eeprom
[ 6.289361] CAN device driver interface
[ OK ] Created slice system-systemd\x2dbacklight.slice.
Starting Load/Save Screen �cess of backlight:ssd1307fb0...
[ OK ] Found device /dev/ttyS2.
[ OK ] Started Load/Save Screen B�ctness of backlight:ssd1307fb0.
[ 6.509382] davinci_mdio 300b2400.mdio: davinci mdio revision 1.7, bus freq 1000000
[ 6.536723] libphy: 300b2400.mdio: probed
[ 6.592681] davinci_mdio 300b2400.mdio: phy[15]: device 300b2400.mdio:0f, driver TI DP83869
[ 6.617573] platform 78000000.r5f: configured R5F for remoteproc mode
[ 6.633229] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[ 6.643029] rti-wdt bus@f4000:watchdog@e000000: invalid resource
[ 6.661349] rti-wdt: probe of bus@f4000:watchdog@e000000 failed with error -22
[ 6.669153] remoteproc remoteproc0: 78000000.r5f is available
[ 6.696343] remoteproc remoteproc0: Direct firmware load for am64-main-r5f0_0-fw failed with error -2
[ 6.711473] remoteproc remoteproc0: powering up 78000000.r5f
[ 6.720774] remoteproc remoteproc0: Direct firmware load for am64-main-r5f0_0-fw failed with error -2
[ 6.731458] remoteproc remoteproc0: request_firmware failed: -2
[ 6.737575] rti-wdt bus@f4000:watchdog@e010000: invalid resource
[ 6.747400] platform 78200000.r5f: configured R5F for remoteproc mode
[ 6.757566] rti-wdt: probe of bus@f4000:watchdog@e010000 failed with error -22
[ 6.758086] m_can_platform 20701000.can: m_can device registered (irq=36, version=32)
[ 6.765051] platform 78200000.r5f: assigned reserved memory node r5f-dma-memory@a1000000
[ 6.798242] m_can_platform 20711000.can: m_can device registered (irq=38, version=32)
[ 6.819048] remoteproc remoteproc1: 78200000.r5f is available
[ 6.819349] remoteproc remoteproc1: Direct firmware load for am64-main-r5f0_1-fw failed with error -2
[ 6.819362] remoteproc remoteproc1: powering up 78200000.r5f
[ 6.819396] remoteproc remoteproc1: Direct firmware load for am64-main-r5f0_1-fw failed with error -2
[ 6.819403] remoteproc remoteproc1: request_firmware failed: -2
[ 6.870817] platform 78400000.r5f: configured R5F for remoteproc mode
[ 6.872095] platform 78400000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[ 6.872440] remoteproc remoteproc2: 78400000.r5f is available
[ 6.872754] remoteproc remoteproc2: Direct firmware load for am64-main-r5f1_0-fw failed with error -2
[ 6.872767] remoteproc remoteproc2: powering up 78400000.r5f
[ 6.872802] remoteproc remoteproc2: Direct firmware load for am64-main-r5f1_0-fw failed with error -2
[ 6.872809] remoteproc remoteproc2: request_firmware failed: -2
[ 6.891722] platform 78600000.r5f: configured R5F for remoteproc mode
[ 6.892484] platform 78600000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[ 6.902207] remoteproc remoteproc3: 78600000.r5f is available
[ 6.902451] remoteproc remoteproc3: Direct firmware load for am64-main-r5f1_1-fw failed with error -2
[ 6.902464] remoteproc remoteproc3: powering up 78600000.r5f
[ 6.902500] remoteproc remoteproc3: Direct firmware load for am64-main-r5f1_1-fw failed with error -2
[ 6.902507] remoteproc remoteproc3: request_firmware failed: -2
[ 7.252386] remoteproc remoteproc4: 30034000.pru is available
[ 7.290061] remoteproc remoteproc5: 30004000.rtu is available
[ 7.341653] remoteproc remoteproc6: 3000a000.txpru is available
[ 7.363098] remoteproc remoteproc7: 30038000.pru is available
[ 7.383084] remoteproc remoteproc8: 30006000.rtu is available
[ 7.417955] remoteproc remoteproc9: 3000c000.txpru is available
[ 7.457615] remoteproc remoteproc10: 300b4000.pru is available
[ OK ] Found device /dev/mmcblk1p3.[ 7.486403] remoteproc remoteproc11: 30084000.rtu is available
[ 7.537807] remoteproc remoteproc12: 3008a000.txpru is available
[ 7.595368] remoteproc remoteproc13: 300b8000.pru is available
[ 7.631623] remoteproc remoteproc14: 30086000.rtu is available
[ 7.681901] remoteproc remoteproc15: 3008c000.txpru is available
[ 7.951320] icssg-prueth icssg1-eth: TI PRU ethernet driver initialized: single EMAC mode
[ 8.097512] random: crng init done
[ 8.100938] random: 7 urandom warning(s) missed due to ratelimiting
[ 8.107360] omap_rng 40910000.rng: Random Number Generator ver. 241b34c
[ 8.263109] usbcore: registered new interface driver usbfs
[ 8.333541] usbcore: registered new interface driver hub
[ 8.363750] usbcore: registered new device driver usb
Activating swap /dev/mmcblk1p3...
[ OK ] Started ifup for eth0.
[ 8.593474] Adding 524224k swap on /dev/mmcblk1p3. Priority:-2 extents:1 across:524224k SS
[ 8.635423] TI DP83867 8000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=8000f00.mdio:00, irq=POLL)
[ 8.655235] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
[ OK ] Activated swap /dev/mmcblk1p3.
[ OK ] Reached target Swap.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily apt download activities.
[ OK ] Started Daily apt upgrade and clean activities.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Started Daily man-db regeneration.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Basic System.
Starting Login Service...
Starting OpenBSD Secure Shell server...
[ OK ] Started D-Bus System Message Bus.
Starting System Logging Service...
Starting Permit User Sessions...
[ OK ] Started Regular background program processing daemon.
Starting LSB: Starts ProFTPD daemon...
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
Starting The Apache HTTP Server...
[ OK ] Started System Logging Service.
[ OK ] Started Permit User Sessions.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Started Getty on tty1.
[ OK ] Reached target Login Prompts.
[ OK ] Started OpenBSD Secure Shell server.
[ OK ] Started Login Service.
[ OK ] Started The Apache HTTP Server.
[ 12.766802] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 12.775314] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Debian GNU/Linux 10 am6442evm ttyS2
am6442evm login:
In case of failure:
U-Boot SPL 2021.01 (Aug 27 2021 - 04:35:24 +0900) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam') SPL initial stack usage: 13392 bytes Trying to boot from MMC2 Starting ATF on ARM64 core... NOTICE: BL31: v2.5(release):08.00.00.004-dirty NOTICE: BL31: Built : 21:46:29, Aug 10 2021 U-Boot SPL 2021.01 (Aug 27 2021 - 04:38:29 +0900) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam') Trying to boot from MMC2 U-Boot 2021.01 (Aug 27 2021 - 04:38:29 +0900) SoC: AM64X SR1.0 Model: Texas Instruments AM642 EVM Board: AM64-GPEVM rev A DRAM: 2 GiB MMC: mmc@fa10000: 0, mmc@fa00000: 1 In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: ethernet@8000000 Hit any key to stop autoboot: 0 ## Error: "boot_rprocs" not defined 19137024 bytes read in 797 ms (22.9 MiB/s) 53223 bytes read in 5 ms (10.2 MiB/s) Moving Image from 0x80080000 to 0x80200000, end=81550000 ## Flattened Device Tree blob at 82000000 Booting using the fdt blob at 0x82000000 Loading Device Tree to 000000008feef000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.10.41-ti-am6442evm-g4c2eade9f7 (user01@ubuntu) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Sat Aug 21 05:47:01 JST 2021 [ 0.000000] Machine model: Texas Instruments AM642 EVM [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a3ffffff] [ 0.000000] node 0: [mem 0x00000000a4000000-0x00000000a4ffffff] [ 0.000000] node 0: [mem 0x00000000a5000000-0x00000000a57fffff] [ 0.000000] node 0: [mem 0x00000000a5800000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 2 pages/cpu s49880 r8192 d73000 u131072 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Built 1 zonelists, mobility grouping off. Total pages: 32736 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16500a,mmio32,0x02800000 mtdparts=fc40000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern) root=/dev/mmcblk1p5 rw roottypefs=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 5, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 4, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1448832K/2097152K available (10816K kernel code, 1344K rwdata, 4288K rodata, 1856K init, 758K bss, 124032K reserved, 524288K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @a4000000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x00000000a58c0000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000000a58d0000 [ 0.000000] random: get_random_bytes called from start_kernel+0x32c/0x4d4 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000004] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.000316] Console: colour dummy device 80x25 [ 0.000375] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.000391] pid_max: default: 32768 minimum: 301 [ 0.000480] LSM: Security Framework initializing [ 0.000575] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear) [ 0.000614] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear) [ 0.002968] rcu: Hierarchical SRCU implementation. [ 0.003270] Platform MSI: msi-controller@1820000 domain created [ 0.003550] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.003664] EFI services will not be available. [ 0.004126] smp: Bringing up secondary CPUs ... [ 0.004878] Detected VIPT I-cache on CPU1 [ 0.004918] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000 [ 0.004933] GICv3: CPU1: using allocated LPI pending table @0x00000000a58e0000 [ 0.005000] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.005131] smp: Brought up 1 node, 2 CPUs [ 0.005152] SMP: Total of 2 processors activated. [ 0.005162] CPU features: detected: 32-bit EL0 Support [ 0.005171] CPU features: detected: CRC32 instructions [ 0.013260] CPU: All CPU(s) started at EL2 [ 0.013288] alternatives: patching kernel code [ 0.014582] devtmpfs: initialized [ 0.022618] KASLR disabled due to lack of seed [ 0.022908] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.022926] futex hash table entries: 512 (order: -1, 32768 bytes, linear) [ 0.025101] pinctrl core: initialized pinctrl subsystem [ 0.025713] DMI not present or invalid. [ 0.026385] NET: Registered protocol family 16 [ 0.034315] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.034792] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.034901] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.035543] thermal_sys: Registered thermal governor 'step_wise' [ 0.035549] thermal_sys: Registered thermal governor 'power_allocator' [ 0.036062] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.036168] ASID allocator initialised with 65536 entries [ 0.064796] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages [ 0.064818] HugeTLB registered 512 MiB page size, pre-allocated 0 pages [ 0.064826] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.066774] cryptd: max_cpu_qlen set to 1000 [ 0.070557] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR1.0 JTAGID[0x0bb3802f] Detected [ 0.071189] vsys_5v0: supplied by evm_12v0 [ 0.071515] vsys_3v3: supplied by evm_12v0 [ 0.071897] vddb_3v3_display: supplied by vsys_3v3 [ 0.072958] iommu: Default domain type: Translated [ 0.073390] SCSI subsystem initialized [ 0.074053] mc: Linux media interface: v0.10 [ 0.074087] videodev: Linux video capture interface: v2.00 [ 0.074182] pps_core: LinuxPPS API ver. 1 registered [ 0.074190] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.074208] PTP clock support registered [ 0.074247] EDAC MC: Ver: 3.0.0 [ 0.075107] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100 [ 0.075316] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100 [ 0.075448] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100 [ 0.076224] FPGA manager framework [ 0.076335] Advanced Linux Sound Architecture Driver Initialized. [ 0.077715] clocksource: Switched to clocksource arch_sys_counter [ 0.078226] VFS: Disk quotas dquot_6.6.0 [ 0.078332] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes) [ 0.084945] NET: Registered protocol family 2 [ 0.085195] IP idents hash table entries: 32768 (order: 2, 262144 bytes, linear) [ 0.086952] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear) [ 0.087106] TCP established hash table entries: 16384 (order: 1, 131072 bytes, linear) [ 0.087233] TCP bind hash table entries: 16384 (order: 2, 262144 bytes, linear) [ 0.087468] TCP: Hash tables configured (established 16384 bind 16384) [ 0.087645] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear) [ 0.087740] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear) [ 0.087982] NET: Registered protocol family 1 [ 0.088634] RPC: Registered named UNIX socket transport module. [ 0.088650] RPC: Registered udp transport module. [ 0.088656] RPC: Registered tcp transport module. [ 0.088662] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.088679] PCI: CLS 0 bytes, default 64 [ 0.089474] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.094343] Initialise system trusted keyrings [ 0.094629] workingset: timestamp_bits=46 max_order=15 bucket_order=0 [ 0.099606] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.100327] NFS: Registering the id_resolver key type [ 0.100368] Key type id_resolver registered [ 0.100374] Key type id_legacy registered [ 0.100449] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.100457] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.100681] 9p: Installing v9fs 9p2000 file system support [ 0.144816] Key type asymmetric registered [ 0.144840] Asymmetric key parser 'x509' registered [ 0.144910] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243) [ 0.144921] io scheduler mq-deadline registered [ 0.144927] io scheduler kyber registered [ 0.147584] pinctrl-single f4000.pinctrl: 180 pins, size 720 [ 0.148690] pinctrl-single a40000.timesync-router: 512 pins, size 2048 [ 0.158568] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.175676] brd: module loaded [ 0.183719] loop: module loaded [ 0.184535] megasas: 07.714.04.00-rc1 [ 0.187551] libphy: Fixed MDIO Bus: probed [ 0.188998] tun: Universal TUN/TAP device driver, 1.6 [ 0.189841] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 0.189856] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.189916] sky2: driver version 1.30 [ 0.191119] VFIO - User Level meta-driver version: 0.3 [ 0.192216] i2c /dev entries driver [ 0.193347] sdhci: Secure Digital Host Controller Interface driver [ 0.193356] sdhci: Copyright(c) Pierre Ossman [ 0.194100] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.195413] ledtrig-cpu: registered to indicate activity on CPUs [ 0.195831] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.197138] optee: probing for conduit method. [ 0.197180] optee: revision 3.12 (3d47a131) [ 0.197893] optee: initialized driver [ 0.200538] NET: Registered protocol family 17 [ 0.200702] 9pnet: Installing 9P2000 support [ 0.200768] Key type dns_resolver registered [ 0.201014] Loading compiled-in X.509 certificates [ 0.215707] ti-sci 44043000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam') [ 0.249829] random: fast init done [ 0.254348] omap_i2c 20000000.i2c: bus 0 rev0.12 at 100 kHz [ 0.256334] pca953x 1-0022: supply vcc not found, using dummy regulator [ 0.256483] pca953x 1-0022: using AI [ 0.307347] Console: switching to mono frame buffer device 12x2 [ 0.336150] ssd1307fb 1-003c: fb0: Solomon SSD1307 framebuffer device registered, using 192 bytes of video memory [ 0.336386] omap_i2c 20010000.i2c: bus 1 rev0.12 at 400 kHz [ 0.337648] omap_i2c 20020000.i2c: bus 2 rev0.12 at 100 kHz [ 0.338830] omap_i2c 20030000.i2c: bus 3 rev0.12 at 100 kHz [ 0.339232] ti-sci-intr bus@f4000:bus@4000000:interrupt-controller1: Interrupt Router 5 domain created [ 0.339387] ti-sci-intr bus@f4000:interrupt-controller0: Interrupt Router 3 domain created [ 0.339630] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created [ 0.350008] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges: [ 0.350065] j721e-pcie f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000 [ 0.350089] j721e-pcie f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000 [ 0.350115] j721e-pcie f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000 [ 1.362602] j721e-pcie f102000.pcie: PCI host bridge to bus 0000:00 [ 1.362623] pci_bus 0000:00: root bus resource [bus 00-ff] [ 1.362635] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x68001000-0x68010fff]) [ 1.362644] pci_bus 0000:00: root bus resource [mem 0x68011000-0x6fffffff] [ 1.362695] pci 0000:00:00.0: [104c:b010] type 01 class 0x060400 [ 1.362719] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0xfffffffff 64bit pref] [ 1.362805] pci 0000:00:00.0: supports D1 [ 1.362814] pci 0000:00:00.0: PME# supported from D0 D1 D3hot [ 1.365436] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 1.367855] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01 [ 1.367901] pci 0000:00:00.0: BAR 0: no space for [mem size 0x1000000000 64bit pref] [ 1.367910] pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x1000000000 64bit pref] [ 1.367922] pci 0000:00:00.0: PCI bridge to [bus 01] [ 1.368476] pcieport 0000:00:00.0: PME: Signaling with IRQ 42 [ 1.369268] ti-bcdma 485c0100.dma-controller: Number of rings: 68 [ 1.370581] ti-bcdma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6) [ 1.372458] ti-pktdma 485c0000.dma-controller: Number of rings: 288 [ 1.380021] ti-pktdma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15) [ 1.383566] printk: console [ttyS2] disabled [ 1.383657] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 16, base_baud = 3000000) is a 8250 [ 2.774690] printk: console [ttyS2] enabled [ 2.782355] spi-nor spi0.0: s28hs512t (65536 Kbytes) [ 2.787374] 7 cmdlinepart partitions found on MTD device fc40000.spi.0 [ 2.793895] Creating 7 MTD partitions on "fc40000.spi.0": [ 2.799292] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 2.806209] 0x000000080000-0x000000280000 : "ospi.tispl" [ 2.812771] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 2.819517] 0x000000680000-0x0000006c0000 : "ospi.env" [ 2.825937] 0x0000006c0000-0x000000700000 : "ospi.env.backup" [ 2.832971] 0x000000800000-0x000003fc0000 : "ospi.rootfs" [ 2.839658] 0x000003fc0000-0x000004000000 : "ospi.phypattern" [ 2.901722] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 2.909322] libphy: 8000f00.mdio: probed [ 2.915727] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867 [ 2.923966] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000002 [ 2.937199] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16 [ 2.944210] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4 [ 2.944217] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512 [ 2.944860] pps pps0: new PPS source ptp0 [ 2.945229] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1 [ 2.961951] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0 [ 2.985824] mmc1: CQHCI version 5.10 [ 2.986508] gpio-mux mux-controller: 2-way mux-controller registered [ 3.004068] vdd_mmc1: supplied by vsys_3v3 [ 3.009356] libphy: mdio_mux: probed [ 3.021635] mmc0: CQHCI version 5.10 [ 3.021927] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present! [ 3.025756] mmc1: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit [ 3.045372] ALSA device list: [ 3.048359] No soundcards found. [ 3.065725] mmc0: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit [ 3.074216] Waiting for root device /dev/mmcblk1p5... [ 3.131259] mmc0: new ultra high speed SDR104 SDHC card at address aaaa [ 3.131326] mmc1: Command Queue Engine enabled [ 3.142570] mmc1: new HS400 MMC card at address 0001 [ 3.142925] mmcblk0: mmc0:aaaa SC16G 14.8 GiB [ 3.148281] mmcblk1: mmc1:0001 S0J56X 14.8 GiB [ 3.156853] mmcblk1boot0: mmc1:0001 S0J56X partition 1 31.5 MiB [ 3.163107] mmcblk1boot1: mmc1:0001 S0J56X partition 2 31.5 MiB [ 3.169438] mmcblk1rpmb: mmc1:0001 S0J56X partition 3 4.00 MiB, chardev (237:0) [ 3.176838] mmcblk0: p1 p2 p3 p4 < p5 > [ 3.190025] VFS: Cannot open root device "mmcblk1p5" or unknown-block(179,37): error -6 [ 3.198072] Please append a correct "root=" boot option; here are the available partitions: [ 3.206448] 0100 4096 ram0 [ 3.206451] (driver?) [ 3.212557] 0101 4096 ram1 [ 3.212560] (driver?) [ 3.218666] 0102 4096 ram2 [ 3.218669] (driver?) [ 3.224765] 0103 4096 ram3 [ 3.224768] (driver?) [ 3.230868] 0104 4096 ram4 [ 3.230871] (driver?) [ 3.236964] 0105 4096 ram5 [ 3.236968] (driver?) [ 3.243068] 0106 4096 ram6 [ 3.243071] (driver?) [ 3.249166] 0107 4096 ram7 [ 3.249169] (driver?) [ 3.255276] 0108 4096 ram8 [ 3.255279] (driver?) [ 3.261373] 0109 4096 ram9 [ 3.261377] (driver?) [ 3.267477] 010a 4096 ram10 [ 3.267481] (driver?) [ 3.273662] 010b 4096 ram11 [ 3.273665] (driver?) [ 3.279851] 010c 4096 ram12 [ 3.279854] (driver?) [ 3.286041] 010d 4096 ram13 [ 3.286044] (driver?) [ 3.292223] 010e 4096 ram14 [ 3.292225] (driver?) [ 3.298411] 010f 4096 ram15 [ 3.298414] (driver?) [ 3.304599] 1f00 512 mtdblock0 [ 3.304602] (driver?) [ 3.311142] 1f01 2048 mtdblock1 [ 3.311146] (driver?) [ 3.317676] 1f02 4096 mtdblock2 [ 3.317679] (driver?) [ 3.324213] 1f03 256 mtdblock3 [ 3.324216] (driver?) [ 3.330782] 1f04 256 mtdblock4 [ 3.330785] (driver?) [ 3.337314] 1f05 57088 mtdblock5 [ 3.337317] (driver?) [ 3.343852] 1f06 256 mtdblock6 [ 3.343855] (driver?) [ 3.350388] b300 15558144 mmcblk0 [ 3.350392] driver: mmcblk [ 3.357181] b301 65536 mmcblk0p1 33d0c7ad-01 [ 3.357184] [ 3.363972] b302 65536 mmcblk0p2 33d0c7ad-02 [ 3.363975] [ 3.370775] b303 524288 mmcblk0p3 33d0c7ad-03 [ 3.370778] [ 3.377566] b304 1 mmcblk0p4 [ 3.377569] [ 3.383403] b305 14900736 mmcblk0p5 33d0c7ad-05 [ 3.383405] [ 3.390199] b320 15540224 mmcblk1 [ 3.390203] driver: mmcblk [ 3.396995] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,37) [ 3.405504] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.10.41-ti-am6442evm-g4c2eade9f7 #1 [ 3.413662] Hardware name: Texas Instruments AM642 EVM (DT) [ 3.419220] Call trace: [ 3.421671] dump_backtrace+0x0/0x1a0 [ 3.425325] show_stack+0x18/0x68 [ 3.428634] dump_stack+0xd0/0x12c [ 3.432027] panic+0x16c/0x334 [ 3.435076] mount_block_root+0x1c4/0x254 [ 3.439074] mount_root+0x10c/0x140 [ 3.442552] prepare_namespace+0x130/0x170 [ 3.446637] kernel_init_freeable+0x210/0x23c [ 3.450984] kernel_init+0x14/0x114 [ 3.454463] ret_from_fork+0x10/0x34 [ 3.458034] SMP: stopping secondary CPUs [ 3.461955] Kernel Offset: disabled [ 3.465434] CPU features: 0x0040002,2000200c [ 3.469689] Memory Limit: none [ 3.472744] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,37) ]---
The root file system is located on the "mmcblk1p5" partition, but in case of failure, the partition cannot be opened.
[ 3.190025] VFS: Cannot open root device "mmcblk1p5" or unknown-block(179,37): error -6
The order of the mounted MMC devices seems to be different between success and failure.
In case of success:
[ 3.148143] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[ 3.149782] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
In case of failure:
[ 3.142925] mmcblk0: mmc0:aaaa SC16G 14.8 GiB
[ 3.148281] mmcblk1: mmc1:0001 S0J56X 14.8 GiB
Why does it fail to mount the root file system?
Best regards,
Daisuke