This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v3.3 with OMAp-L137 EVM board,

Other Parts Discussed in Thread: OMAP-L137

Dear Sir / Madam,

I am working with CCS v3.3 and Spectrum Digital OMAP-L137 EVM board. I am using SPI-Flash as boot flash and i am using Code Sourcery G++ for application development.

With CCS and SPI Writer, i am trying to program UBL and the application. I am able to do it successfully till today. All of sudden i am facing the below problem, can you please suggest me for soving this.

I am able to connect the L137 EVM board with the CCS and load the SPI writer program successfully, then after supplying the UBL file name, the following error is coming.

******CCS popup window************************

Can't Run Target CPU:

Error 0x00000026/-1060

Error during: Memory, Register, Execution,

An unknown error prevented the emulator from accessing the processor in a timely fashion.

It is recommended to RESET EMULATOR.  This will disconnect each target from the emulator.  The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.

 


******CCS output window*************************

Can't Run Target CPU: Error 0x00000026/-1060 Error during: Memory, Register, Execution, An unknown error prevented the emulator from accessing the processor in a timely fashion. It is recommended to RESET EMULATOR.  This will disconnect each target from the emulator.  The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. 

Trouble Reading PC Register: Error 0x00000004/-1060 Error during: Register, An unknown error prevented the emulator from accessing the processor in a timely fashion. It is recommended to RESET EMULATOR.  This will disconnect each target from the emulator.  The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. 

Thanks and Regards,

Venkata Ramana