Part Number: AM5728
Hello Champs,
HW: Customer own AM5728 board
SW: ti-processor-sdk-android-am57xx-evm-06.03.00.106 Kernel:4.19
PCIe is connected to FPGA on customer own board, AM5728 is configured to RC mode. When using android5.1.1+linux3.14, everything is ok.
But when upgrading to the new 4.19 version. The PCIe can't work. It can detect the PCI device, but it prompted below error message when reading BAR0. The value is all 0xffff ffff。
omap_l3_noc 44000000.ocp: L3 application error: target 5 mod:1 (unclearable)
omap_l3_noc 44000000.ocp: L3 debug error: target 5 mod:1 (unclearable)
Below is the log of PCIe:
console:/ # dmesg | grep pci
[ 0.905083] usm-controller usm_controller: GPIO lookup for consumer pcie_rst
[ 0.905111] of_get_named_gpiod_flags: parsed 'pcie_rst-gpios' property of node '/usm_controller[0]' - status (0)
[ 0.905145] no flags found for pcie_rst
[ 2.877261] ehci-pci: EHCI PCI platform driver
[ 3.454369] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.3
[ 3.462209] dra7-pcie 51000000.pcie: GPIO lookup for consumer (null)
[ 3.462213] dra7-pcie 51000000.pcie: using device tree for GPIO lookup
[ 3.462226] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/ocp/axi@0/pcie@51000000[0]'
[ 3.462236] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/ocp/axi@0/pcie@51000000[0]'
[ 3.462242] dra7-pcie 51000000.pcie: using lookup tables for GPIO lookup
[ 3.462247] dra7-pcie 51000000.pcie: No GPIO consumer (null) found
[ 3.462398] dra7-pcie 51000000.pcie: host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 3.469927] dra7-pcie 51000000.pcie: Parsing ranges property...
[ 3.469949] dra7-pcie 51000000.pcie: IO 0x20003000..0x20012fff -> 0x00000000
[ 3.477310] dra7-pcie 51000000.pcie: MEM 0x20013000..0x2fffffff -> 0x20013000
[ 3.584771] dra7-pcie 51000000.pcie: Link up
[ 3.589199] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 3.595497] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 3.610258] pci_bus 0000:00: root bus resource [io 0x1000-0x10000]
[ 3.616570] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 3.623545] pci_bus 0000:00: scanning bus
[ 3.623623] pci 0000:00:00.0: [104c:8888] type 01 class 0x060400
[ 3.623650] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]
[ 3.623679] pci 0000:00:00.0: reg 0x14: [mem 0x00000000-0x0000ffff]
[ 3.623733] pci 0000:00:00.0: supports D1
[ 3.623740] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 3.623760] pci 0000:00:00.0: PME# disabled
[ 3.628460] pci_bus 0000:00: fixups for bus
[ 3.634066] pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0
[ 3.634136] pci_bus 0000:01: scanning bus
[ 3.634197] pci 0000:01:00.0: [10ee:7024] type 00 class 0x058000
[ 3.634289] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x00ffffff 64bit pref]
[ 3.634316] pci 0000:01:00.0: reg 0x18: [mem 0x00000000-0x00007fff]
[ 3.634587] pci 0000:01:00.0: PME# supported from D0 D1 D2 D3hot
[ 3.634601] pci 0000:01:00.0: PME# disabled
[ 3.634652] pci 0000:01:00.0: 4.000 Gb/s available PCIe bandwidth, limited by 5 GT/s x1 link at 0000:00:00.0 (capable of 8.000 Gb/s with 5 GT/s x2 l
ink)
[ 3.653130] pci_bus 0000:01: fixups for bus
[ 3.658767] pci_bus 0000:01: bus scan returning with max=01
[ 3.658776] pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 1
[ 3.658784] pci_bus 0000:00: bus scan returning with max=01
[ 3.658804] pci 0000:00:00.0: BAR 9: assigned [mem 0x21000000-0x21ffffff pref]
[ 3.666057] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 3.672909] pci 0000:00:00.0: BAR 8: assigned [mem 0x20200000-0x202fffff]
[ 3.679739] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 3.686560] pci 0000:01:00.0: BAR 0: assigned [mem 0x21000000-0x21ffffff 64bit pref]
[ 3.694393] pci 0000:01:00.0: BAR 2: assigned [mem 0x20200000-0x20207fff]
[ 3.701231] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 3.706217] pci 0000:00:00.0: bridge window [mem 0x20200000-0x202fffff]
[ 3.713043] pci 0000:00:00.0: bridge window [mem 0x21000000-0x21ffffff pref]
The log of spci -v :
00:00.0 Class 0604: Device 104c:8888 (rev 01)
Flags: bus master, fast devsel, latency 0
Memory at 20100000 (32-bit, non-prefetchable)
[Result] flg:537919488 pciaddr_t a : 0x20100000
[size=1M]
Memory at 20020000 (32-bit, non-prefetchable)
[Result] flg:537001984 pciaddr_t a : 0x20020000
[size=64K]
Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
Memory behind bridge: 20200000-202fffff
Prefetchable memory behind bridge: 21000000-21ffffff
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/1 Maskable- 64bit+
Capabilities: [70] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
01:00.0 Class 0580: Device 10ee:7024
Subsystem: Device 10ee:0007
Flags: bus master, fast devsel, latency 0, IRQ 215
Memory at 21000000 (64-bit, prefetchable)
[Result] flg:553648140 pciaddr_t a : 0x21000000
[size=16M]
Memory at 20200000 (32-bit, non-prefetchable)
[Result] flg:538968064 pciaddr_t a : 0x20200000
[size=32K]
Capabilities: [40] Power Management version 3
Capabilities: [48] MSI: Enable- Count=1/1 Maskable- 64bit+
Capabilities: [60] Express Legacy Endpoint, MSI 00
Capabilities: [100] Device Serial Number 00-00-00-01-01-00-0a-35
Kernel driver in use: E5PCIeDriver
Thanks.
Rgds
Shine