Hi Team,
What is the working current of the HDMI module of TDA2SG, and what is the static current when the SATA\PCIE module is not used? The LDO3_OUT of TPS659039 supplies power to SATA, PCIE, and HDMI, and the two modules SATA and PCIE are not used. If the 1.8V generated by LDO3_OUT is used to power SATA, PCIE, HDMI, and DS90UB914. According to the manual, the maximum 1.8V current of DS90UB914 is 110mA, the normal is 60+mA, and the LDO3_OUT capacity is 200mA. Is there a problem with this use?